I am using ti-ezsdk_dm816x-evm_5_00_00_11 and trying to bring up a board with a 8168 PG2.0 (TMX320DM8168BCYG2)
The kernel gives this error during boot up
Could not init clock framework - unknown CPU
I see this comes from arch/arm/mach-omap2/io.c
Is there some guidance you can give me to migrate from the PG1.1 (my current chip) and PG2.0?
Is there a new SDK that supports the PG2.0?
Thanks
Joe