Other Parts Discussed in Thread: MSP430BT5190
I'm using: CCSv4.2.4, SYS/BIOS 6.32.04.49, IPC 1.23.04.36, XDCtools 3.22.03.41 on Windows XP. I have a MSP430BT5190 connected to my computer through a MSP-FET430UIF.
When I enable RTA, I can no longer debug my msp430 code. I cannot run or halt the program.
The reproduce the problem is easy:
1. New->CCS Project, project name "test", project type: MSP430, Project Templates: SYS/BIOS->MSP430 Examples->Task Example
2. Open task.cfg, in the Available Products tab SYS/BIOS->Realtime Analysis->Agent and check "Add Agent to my configuration". Save
3. Build Active Project: No errors.
4. Debug Active Project: "Source not found." with the file name 0 c_int00_noargs() at boot_3.3.c:129 0x06196, and the console displays:
out of memory: heap=0x0, size=28
xdc.runtime.Error.raise: terminating execution