Tool/software:
Hi!
The TIAM64x board I am working on, suddenly stops working.
With the AC adapter plugged in, I can confirm that the LED6 and LED24 are lit up.
when I connect the UART and JTAG to the board, LED20 and LED21 are also lit up .
But, when I switch the power on, the other LEDs do not light up.
I have tried to recover the board by following the set up guide below without any success.
I think that the board is now broken, but I wonder if anyone can help me recover the board.
Thanks in advance!
Kind regards,
Ryota