Part Number: TDA4AP-Q1
Tool/software:
Hi TI Experts,
Customer is working on TDA4AP SDK9.2.
As we could find on the register manual for the register 0x03702010, only bit 0 and bit 1 are used, and the rest of the other bits are reserved.

However, inside our Linux SDK, these reserved bits are set by DDS_QOS with value 0.



Hence, customer is wondering why we should set these reserved bits to 0? If they do not set these reserved bits to 0, would there be any problem?
Thanks,
Kevin