This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VC Demo on 814x

Hi.

 We are using VC Demo on 814x.

One problem we are observing, After loading the .xv5t the video and vpss module is loaded correctly.

But we are seeing a white screen on the output connected to Tx HDMI port.. the Rx HDMI port is connected to Blu-Ray player.

(Checked with both 720p and 1080p input to off chip HDMI)

Please let us know your input on this..

 

Logs:

Wait for VM3 to to create the server first
Entering : OMX_HDVPSS_MicroChain_Test
You could Connect CCS Now:: Press any key to continue:
VFCC:0
VFDC:0
VFPC_DEI:0
VFPC_SCWB:0

 Encode: got the component handle
OMX_IndexParamVideoProfileLevelCurrent Getparam done for enc!!
OMX_IndexParamVideoProfileLevelCurrent Setparam done for enc!!
OMX_TI_IndexParamVideoBitStreamFormatSelect Getparam done for enc!!
OMX_TI_IndexParamVideoBitStreamFormatSelect Setparam done for enc!!
OMX_TI_IndexParamVideoEncoderPreset Getparam done for enc!!
OMX_TI_IndexParamVideoEncoderPreset Setparam done for enc!!
OMX_TI_IndexParamVideoFrameDataContentSettings Getparam done for enc!!
OMX_TI_IndexParamVideoFrameDataContentSettings Setparam done for enc!!
OMX_TI_IndexParamVideoTransformBlockSize Getparam done for enc!!
OMX_TI_IndexParamVideoTransformBlockSize Setparam done for enc!!
Entering H264ENC_SetParamsFromInitialDynamicParams!!
Exited H264ENC_SetParamsFromInitialDynamicParams!!
VFPC_VENC_H264:0
VFPC_VDEC_H264:0

 VFCC Component Transitioned to Idle state
 CTRLTVP Component Transitioned to Idle state
 VFPCDEI_0 Component Transitioned to Idle state
 VENC_0 Component Transitioned to Idle state
 VDEC_0 Component Transitioned to Idle state
 INDTXSC Component Transitioned to Idle state
 CTRLDC_0 Component Transitioned to Idle state
 VFDC_0 Component Transitioned to Idle state
 CTRLDC_0 Component Transitioned to Executing state
 VFDC_0 Component Transitioned to Executing state
 INDTXSC Component Transitioned to Executing state
 VDEC_0 Component Transitioned to Executing state
 VENC_0 Component Transitioned to Executing state
 VFPCDEI_0 Component Transitioned to Executing state
 CTRLTVP Component Transitioned to Executing state
 VFCC Component Transitioned to Executing state

 

Regards,

Sudeep