This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517 usage of USBOTG_SELINPUTCLKFREQ bits

Hello,

The current SDK is setting "6" (reserved) instead of "7" (sys_clk) for USBOTG_SELINPUTCLKFREQ bit in CONTROL_DEVCONF2 register.  These bit are set for USB PHY PLL reference clock frequency. 
Does this device allow this setting?  (The setting "6" is described as "reserved" in the latest TRM (Literature Number: SPRUGR0B)).

Thank you
Regards
Takasugi