Other Parts Discussed in Thread: TDA4VM-Q1, , TDA4VL, TDA4VM, AM68A
Tool/software:
Hi Ti,
I am making processor selection of the TDA4 series, mainly between TDA4VL-Q1 and TDA4VM-Q1. Please clarify some performance parameters for me, Thanks.
For CPU part:
1. I found TDA4VL and TDA4VM both have different speed grades, can I identify that same frequency has same DMIPS performance? for example, according to the 2 tables(left represent 4VL, right represent 4VM), can I get same DMIPS score between T grade of 4VL and TDA4VMxT of 4VM ?


2. If the answer is positive, do 4VL and 4VM have the same thermal design and power design? I am afraid that TDA4VMxE and TDA4VLT has huge DMIPS score difference even if they have similar frequency.
3. I searched on the web and got an 18.8KDMIPS score of 2000MHz grade. Is it right? Can I estimate another grade linearly? (for example: kDIMPS of H= 2/1.2*18.8 )
For GPU part:
1. 4VL has tw0 C71 cores running @500MHz frequency, while 4VMxE has 1 C71 core and two C66 cores running @750MHz&1GHz, how can I calculate the TOPs parameters? Do you have some measurement or benchmark data could share? Thanks.