Part Number: PROCESSOR-SDK-AM64X
Tool/software:
Hello Ti,
I'm using the latest TI SDK release Image + firmware:
https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-RT-AM64X
=> 09.02.01.10 (30 May 2024)
I observe some duplicated packets on hsr0 interface on 100 Mbps for "high throughput" on 100 Mbps.
Here is our set up :
We have 2 EVMs
eth1 <-> eth2
eth2 <-> eth2
First we set the boards in u_boot, as DUAL EMAC mode
setenv name_overlays 'k3-am642-evm-icssg1-dualemac.dtbo' run bootcmd
and once it's boot, we disable network on EVM1 and EVM2:
systemctl disable dhcpcd.service systemctl disable NetworkManager.service systemctl disable systemd-resolved.service systemctl disable systemd-networkd.service sync reboot
Also, we set up the board EVM1 to 100Mbps link speed
ethtool -s eth1 speed 100 duplex full ethtool -s eth2 speed 100 duplex full
We up interfaces for EVM1 and EVM2 :
ip link set dev eth1 up ip link set dev eth2 up
And we enable HSR offload solution on both boards.
TEST1 :Send packets with ping
We observe some duplicated packets on HSR interface with our applications.
The application basically is sending message every 1ms et wait the receive of a message before re-sending it again. Since we cannot share this application, we tried to use an open source application : ping
ping 192.168.100.5 -s 400 -i 0.001
root@am64xx-evm:~# ping 192.168.100.5 -s 400 -i 0.005
PING 192.168.100.5 (192.168.100.5): 400 data bytes
408 bytes from 192.168.100.5: seq=0 ttl=64 time=0.565 ms
408 bytes from 192.168.100.5: seq=1 ttl=64 time=0.397 ms
408 bytes from 192.168.100.5: seq=2 ttl=64 time=0.301 ms
408 bytes from 192.168.100.5: seq=3 ttl=64 time=0.301 ms
408 bytes from 192.168.100.5: seq=4 ttl=64 time=0.287 ms
(...)
408 bytes from 192.168.100.5: seq=170 ttl=64 time=72.846 ms
408 bytes from 192.168.100.5: seq=175 ttl=64 time=72.879 ms
408 bytes from 192.168.100.5: seq=180 ttl=64 time=72.891 ms
408 bytes from 192.168.100.5: seq=185 ttl=64 time=72.893 ms
408 bytes from 192.168.100.5: seq=190 ttl=64 time=72.881 ms
408 bytes from 192.168.100.5: seq=195 ttl=64 time=72.824 ms
408 bytes from 192.168.100.5: seq=201 ttl=64 time=66.246 ms
408 bytes from 192.168.100.5: seq=206 ttl=64 time=66.207 ms
408 bytes from 192.168.100.5: seq=211 ttl=64 time=66.270 ms
408 bytes from 192.168.100.5: seq=216 ttl=64 time=66.271 ms
408 bytes from 192.168.100.5: seq=221 ttl=64 time=66.330 ms
408 bytes from 192.168.100.5: seq=226 ttl=64 time=67.387 ms
408 bytes from 192.168.100.5: seq=231 ttl=64 time=67.386 ms
408 bytes from 192.168.100.5: seq=236 ttl=64 time=67.394 ms
408 bytes from 192.168.100.5: seq=241 ttl=64 time=67.454 ms
408 bytes from 192.168.100.5: seq=246 ttl=64 time=67.389 ms
408 bytes from 192.168.100.5: seq=251 ttl=64 time=67.412 ms
408 bytes from 192.168.100.5: seq=256 ttl=64 time=67.376 ms
408 bytes from 192.168.100.5: seq=261 ttl=64 time=67.377 ms
408 bytes from 192.168.100.5: seq=262 ttl=64 time=71.744 ms
408 bytes from 192.168.100.5: seq=266 ttl=64 time=72.865 ms
408 bytes from 192.168.100.5: seq=266 ttl=64 time=78.379 ms (DUP!)
408 bytes from 192.168.100.5: seq=276 ttl=64 time=72.784 ms
408 bytes from 192.168.100.5: seq=281 ttl=64 time=72.775 ms
408 bytes from 192.168.100.5: seq=287 ttl=64 time=71.716 ms
408 bytes from 192.168.100.5: seq=292 ttl=64 time=71.861 ms
408 bytes from 192.168.100.5: seq=297 ttl=64 time=71.867 ms
408 bytes from 192.168.100.5: seq=302 ttl=64 time=71.893 ms
408 bytes from 192.168.100.5: seq=307 ttl=64 time=71.911 ms
408 bytes from 192.168.100.5: seq=312 ttl=64 time=71.921 ms
408 bytes from 192.168.100.5: seq=317 ttl=64 time=66.460 ms
408 bytes from 192.168.100.5: seq=322 ttl=64 time=66.487 ms
408 bytes from 192.168.100.5: seq=327 ttl=64 time=66.595 ms
408 bytes from 192.168.100.5: seq=332 ttl=64 time=66.597 ms
408 bytes from 192.168.100.5: seq=337 ttl=64 time=66.618 ms
408 bytes from 192.168.100.5: seq=342 ttl=64 time=67.827 ms
408 bytes from 192.168.100.5: seq=342 ttl=64 time=73.238 ms (DUP!)
408 bytes from 192.168.100.5: seq=352 ttl=64 time=67.672 ms
408 bytes from 192.168.100.5: seq=352 ttl=64 time=73.202 ms (DUP!)
408 bytes from 192.168.100.5: seq=362 ttl=64 time=67.557 ms
408 bytes from 192.168.100.5: seq=362 ttl=64 time=73.031 ms (DUP!)
408 bytes from 192.168.100.5: seq=372 ttl=64 time=67.519 ms
408 bytes from 192.168.100.5: seq=377 ttl=64 time=67.478 ms
408 bytes from 192.168.100.5: seq=378 ttl=64 time=71.889 ms
408 bytes from 192.168.100.5: seq=378 ttl=64 time=77.416 ms (DUP!)
408 bytes from 192.168.100.5: seq=387 ttl=64 time=72.881 ms
408 bytes from 192.168.100.5: seq=387 ttl=64 time=78.399 ms (DUP!)
408 bytes from 192.168.100.5: seq=397 ttl=64 time=72.858 ms
408 bytes from 192.168.100.5: seq=403 ttl=64 time=71.761 ms
408 bytes from 192.168.100.5: seq=403 ttl=64 time=77.266 ms (DUP!)
408 bytes from 192.168.100.5: seq=413 ttl=64 time=71.761 ms
408 bytes from 192.168.100.5: seq=418 ttl=64 time=71.806 ms
408 bytes from 192.168.100.5: seq=423 ttl=64 time=71.895 ms
408 bytes from 192.168.100.5: seq=428 ttl=64 time=71.917 ms
408 bytes from 192.168.100.5: seq=433 ttl=64 time=73.019 ms
408 bytes from 192.168.100.5: seq=438 ttl=64 time=73.015 ms
408 bytes from 192.168.100.5: seq=443 ttl=64 time=73.056 ms
408 bytes from 192.168.100.5: seq=448 ttl=64 time=72.988 ms
408 bytes from 192.168.100.5: seq=453 ttl=64 time=73.097 ms
408 bytes from 192.168.100.5: seq=453 ttl=64 time=78.526 ms (DUP!)
408 bytes from 192.168.100.5: seq=463 ttl=64 time=73.046 ms
408 bytes from 192.168.100.5: seq=468 ttl=64 time=73.018 ms
408 bytes from 192.168.100.5: seq=473 ttl=64 time=73.032 ms
408 bytes from 192.168.100.5: seq=478 ttl=64 time=72.986 ms
408 bytes from 192.168.100.5: seq=483 ttl=64 time=72.960 ms
408 bytes from 192.168.100.5: seq=488 ttl=64 time=72.877 ms
408 bytes from 192.168.100.5: seq=493 ttl=64 time=72.837 ms
408 bytes from 192.168.100.5: seq=499 ttl=64 time=71.699 ms
408 bytes from 192.168.100.5: seq=504 ttl=64 time=66.191 ms
408 bytes from 192.168.100.5: seq=509 ttl=64 time=66.153 ms
408 bytes from 192.168.100.5: seq=509 ttl=64 time=71.691 ms (DUP!)
408 bytes from 192.168.100.5: seq=519 ttl=64 time=66.164 ms
408 bytes from 192.168.100.5: seq=524 ttl=64 time=67.229 ms
408 bytes from 192.168.100.5: seq=529 ttl=64 time=67.182 ms
408 bytes from 192.168.100.5: seq=534 ttl=64 time=67.163 ms
408 bytes from 192.168.100.5: seq=539 ttl=64 time=67.169 ms
408 bytes from 192.168.100.5: seq=544 ttl=64 time=67.198 ms
408 bytes from 192.168.100.5: seq=549 ttl=64 time=67.250 ms
408 bytes from 192.168.100.5: seq=554 ttl=64 time=67.256 ms
408 bytes from 192.168.100.5: seq=559 ttl=64 time=67.251 ms
408 bytes from 192.168.100.5: seq=564 ttl=64 time=67.241 ms
408 bytes from 192.168.100.5: seq=565 ttl=64 time=71.658 ms
408 bytes from 192.168.100.5: seq=569 ttl=64 time=72.754 ms
408 bytes from 192.168.100.5: seq=574 ttl=64 time=72.745 ms
408 bytes from 192.168.100.5: seq=579 ttl=64 time=72.834 ms
408 bytes from 192.168.100.5: seq=585 ttl=64 time=71.735 ms
408 bytes from 192.168.100.5: seq=590 ttl=64 time=71.712 ms
408 bytes from 192.168.100.5: seq=595 ttl=64 time=71.731 ms
408 bytes from 192.168.100.5: seq=600 ttl=64 time=71.834 ms
408 bytes from 192.168.100.5: seq=605 ttl=64 time=71.886 ms
408 bytes from 192.168.100.5: seq=610 ttl=64 time=72.933 ms
408 bytes from 192.168.100.5: seq=615 ttl=64 time=67.448 ms
408 bytes from 192.168.100.5: seq=620 ttl=64 time=67.457 ms
408 bytes from 192.168.100.5: seq=625 ttl=64 time=67.526 ms
408 bytes from 192.168.100.5: seq=630 ttl=64 time=67.444 ms
408 bytes from 192.168.100.5: seq=635 ttl=64 time=67.449 ms
408 bytes from 192.168.100.5: seq=640 ttl=64 time=67.495 ms
408 bytes from 192.168.100.5: seq=645 ttl=64 time=67.403 ms
408 bytes from 192.168.100.5: seq=650 ttl=64 time=67.412 ms
408 bytes from 192.168.100.5: seq=655 ttl=64 time=67.396 ms
408 bytes from 192.168.100.5: seq=660 ttl=64 time=67.416 ms
408 bytes from 192.168.100.5: seq=665 ttl=64 time=67.427 ms
408 bytes from 192.168.100.5: seq=670 ttl=64 time=67.302 ms
408 bytes from 192.168.100.5: seq=676 ttl=64 time=66.176 ms
408 bytes from 192.168.100.5: seq=677 ttl=64 time=70.632 ms
408 bytes from 192.168.100.5: seq=681 ttl=64 time=71.692 ms
408 bytes from 192.168.100.5: seq=686 ttl=64 time=71.697 ms
As you can see, according to ping, we have some duplicated packets. We was wondering if this is coming from the PRU firmware.
Here the speed is 408B every 1ms
=> throughput = 408kB/s
By assuming the device needs to handle Rx and Tx, so it can handle ~ 816kB/s ~ 1Mbit/s << 100 Mbps
is it possible to reproduce on your side this issue ?
Tianyi