Tool/software:
Hi ti experts, I have tested the I2C communication between TDAV4M and the camera and found that there was about 15,000 times of I2C communication failure (NACK_ERR) in the camera. The following is the I2C3 register value that we captured in turn 50ms after the normal operation of the power on and abnormal. Can these registers be queried for specific exceptions。