This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

프로세서-SDK-J721S2:How do i use the RTOS + QNX SPI_Slave function?

Part Number: PROCESSOR-SDK-J721S2


Tool/software:

Hello, my name is Maengho Lee.
I am using ti-processor-sdk-rtos SDK and QNX OS.
The relevant version is 09_01_00_06 and the QNX version is also the same.
PDK version is 09_01_00_22.
After checking other inquiries, we confirmed that there is a SPI-SLAVE Driver and Test Code that can be used in R Core.
As a result of checking the PDK, it was confirmed that SPI-related code exists.
I would like to build and test, but it seems that the SPI_Slave code cannot be built using the makefile inside the PDK. Accordingly, I would like to inquire about the overall implementation of related content.
The contents below are a summary of the inquiries.
1.How to build and test SPI_Slave inside PDK
2. How to test on j721s2 EVM board
3. How to port SPI-SLAVE Driver to A72 core