This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Porting DVSDK 4.01 on Beagleboard-xM Rev B/C

Other Parts Discussed in Thread: DM3730

Hello to all,

We have ported DVSDK-4.01 onto Beagleboard-xM Rev B/C and uploaded the Source file in Sourceforge,

For more details please go through the link provided below,

http://sourceforge.net/projects/dvsdkbbxm/files/DVSDK-4.01%20for%20BeagleBoard/

 

Thank-you.

  • Hi Naveen,

    Thanks for uploads..

    I have problem on making sd card

    ************************************************************
    * THIS WILL DELETE ALL THE DATA ON /dev/sdc *
    * *
    * WARNING! Make sure your computer does not go *
    * in to idle mode while this script is *
    * running. The script will complete, *
    * but your SD card may be corrupted. *
    * *
    * Press <ENTER> to confirm.... *
    ************************************************************

    unmounting device '/dev/sdc1'
    1024+0 records in
    1024+0 records out
    1048576 bytes (1.0 MB) copied, 0.4498 s, 2.3 MB/s
    Disk /dev/sdc doesn't contain a valid partition table
    Checking that no-one is using this disk right now ...
    OK

    Disk /dev/sdc: 501 cylinders, 255 heads, 63 sectors/track

    sfdisk: ERROR: sector 0 does not have an msdos signature
    /dev/sdc: unrecognized partition table type
    Old situation:
    No partitions found
    New situation:
    Units = cylinders of 8225280 bytes, blocks of 1024 bytes, counting from 0

    Device Boot Start End #cyls #blocks Id System
    /dev/sdc1 * 0+ 4 5- 40131 c W95 FAT32 (LBA)
    /dev/sdc2 5 500 496 3984120 83 Linux
    /dev/sdc3 0 - 0 0 0 Empty
    /dev/sdc4 0 - 0 0 0 Empty
    Successfully wrote the new partition table

    Re-reading the partition table ...

    If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
    to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
    (See fdisk(8).)
    Formating /dev/sdc1 ...
    Formating /dev/sdc2 ...
    mke2fs 1.41.11 (14-Mar-2010)
    Image Name: Execute uImage.bin
    Created: Sun May 13 01:00:15 2012
    Image Type: ARM Linux Script (uncompressed)
    Data Size: 238 Bytes = 0.23 kB = 0.00 MB
    Load Address: 0x00000000
    Entry Point: 0x00000000
    Contents:
    Image 0: 230 Bytes = 0 kB = 0 MB
    Image Name: Execute uImage.bin
    Created: Sun May 13 01:00:15 2012
    Image Type: ARM Linux Script (uncompressed)
    Data Size: 289 Bytes = 0.28 kB = 0.00 MB
    Load Address: 0x00000000
    Entry Point: 0x00000000
    Contents:
    Image 0: 281 Bytes = 0 kB = 0 MB
    Select Primary display output:
    1: LCD
    2: DVI

    Copying u-boot/mlo/uImage on /dev/sdc1
    unmounting /dev/sdc1
    Extracting filesystem on /dev/sdc2 ...
    Creating matrix-gui-e symbolic link...done
    unmounting /dev/sdc2
    completed!
    Updating FS with modified beagleboard-xM files
    Makefile:927: warning: overriding commands for target `depmod_install'
    Makefile:922: warning: ignoring old commands for target `depmod_install'
    Makefile:932: warning: overriding commands for target `depmod_install'
    Makefile:927: warning: ignoring old commands for target `depmod_install'
    Makefile:937: warning: overriding commands for target `depmod_install'
    Makefile:932: warning: ignoring old commands for target `depmod_install'
    Makefile:942: warning: overriding commands for target `depmod_install'
    Makefile:937: warning: ignoring old commands for target `depmod_install'
    unmounting /dev/sdc2
    Done
    Updating FS with modified beagleboard-xM files
    Makefile:927: warning: overriding commands for target `depmod_install'
    Makefile:922: warning: ignoring old commands for target `depmod_install'
    Makefile:932: warning: overriding commands for target `depmod_install'
    Makefile:927: warning: ignoring old commands for target `depmod_install'
    Makefile:937: warning: overriding commands for target `depmod_install'
    Makefile:932: warning: ignoring old commands for target `depmod_install'
    Makefile:942: warning: overriding commands for target `depmod_install'
    Makefile:937: warning: ignoring old commands for target `depmod_install'
    install: writing `/tmp/sdk/5333/usr/share/ti/ti-dmai-apps/image_decode_io1_dm3730.x470MV': Read-only file system
    make[3]: *** [doinstall] Error 1
    make[2]: *** [image_decode_io1/.install] Error 2
    make[1]: *** [install] Error 2
    make: *** [dmai_install] Error 2

    ERROR: executing make depmod_install

  • Hi Naveen ,

    I am facing an issue in porting , 

    I have run the dvsdk_dm365-evm_4_00_00_22_setuplinux binary , 

    The resulting directory contains the kernel version linux-2.6.32-rc2-psp03.01.0037 

    In the setup-dvsdk-4-01-beaglexm.sh script it is linux-2.6.32-psp03.00.01.06 

    this version change is causing issue in running the script , 

    It will be great full if you give me any links for  resolving this issue.

    Regards,

    Dibin