This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB on DSK6455



Hello, I'm using a DSK6455 board and CCS v4. I need to write my own application with visual C++ and communicate DSK6455 via USB with PC, but I don't find any documentation about this. Could anybody say me how work with usb port of DSK6455.

Regards.

Manuel

  • Manuel,

    The USB connector on the DSK6455 is for JTAG emulation and communication with the CCSv4 program. You may want to check on the Code Composer forum to see if there is any communication method supported through this JTAG interface that you could use. Please post a link here to your new thread, if you choose to do that.

    There may be EMIF daughtercards available for the DSK6455 that can give you USB functionality. Or perhaps you can use another communications port, such as Ethernet.

    Regards,
    RandyP

     

    If you need more help, please reply back. If this answers the question, please click  Verify Answer  , below.