Hi everyone,
I am trying to debug an ARM+DSP application on DM8148 where in the ARM application loads a BIOS 6 based excutable on the DSP. The debugging steps and setup is as mentioned in the wiki mentioned below.
http://processors.wiki.ti.com/index.php/Debugging_the_DSP_side_of_a_CE_application_using_CCS
The code on the DSP side uses framework components to allocate and manage EDMA resources using IRES interface. To debug the application I have enabled the logging and debuging in framework components using
http://processors.wiki.ti.com/index.php/Trace_in_Framework_Components#Framework_Components_3.20
The code on the DSP uses log_print statements to create a debug log which I need to be able to see in the RTA tool in CCS. However when I load the symbols from the executable after halting the ARM side application, CCS does not allow me to open the RTA window after I connect to the DSP. This prevents me from collecting all the debug log information that is being obtained from the DSP side of the application. Has any body tried this debug setup? Are there other ways of collecting trace.
I have posted a similar question in the CCS forums but I am not sure they have tried this debug environment in their test setup.
Regards,
Rahul