This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 Framebuffer/DSS Field Order

Hi,

I am looking at capturing video using the Camera ISP and Video4Linux 2 - I am currently following one of the examples supplied in the PSP. I am noticing that after capturing a frame of PAL video, the fields appear to be swapped when replaying the frame on the output. Looking at the available IOCTLs V4L2 provides, there is a way to set the interlacing method (INTERLACED_TB or INTERLACED_BT) for capture.

As the output is supplied a full frame, the DSS must interlace this to produce the output video. Is there a way to tell the DSS to output fields in a different order?

Thanks,

 

Andy

  • It appears that it is not possible to set the field order of the DSS output video. I am now looking to change the capture side (ISP and CCDC) to support V4L2_FIELD_INTERLACED_TB or V4L2_FIELD_INTERLACED_BT as they don't appear to be supported. Are there any examples of this?

    Any help would be appreciated.

     

    Andy