Part Number: AM6442
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM6442
Tool/software:
Hi,
You need to power on the board, and run a few commands to verify CAN communication on AM64x. However, you need to have a setup, i.e. the transmitting and receiving end.
Please go though the documentation: https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/09_02_01_10/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/MCAN.html
Regards,
Aparna
Hi Aparna Patra,
Now I have Kit AM64x SK, I know this Kit does not have CAN transceiver. But I want to configure to enable Main_can1 in linux kernel so that I can test with loopback or I will test with external transceiver, so help me fix the .dts file or something.
Thanks!
Hi Cong Pham,
I know this Kit does not have CAN transceiver
AM64x does have an external transceiver, hence you don't need to connect an external one. Using the AM64x CAN node which is present on-board you can either sent or receive CAN messages. So, regarding the hardware setup, you will need another CAN node, i.e. another AM64 EVM, or a CAN tool such as the CANoe or PCAN module. This will complete the setup required to test CAN.
For the software requirements, you can download the SDK: https://www.ti.com/tool/PROCESSOR-SDK-AM64X
Then, flash the wic image onto the SD card for the same site: https://www.ti.com/tool/PROCESSOR-SDK-AM64X
Put the boot switches to SD card boot mode, and boot into Linux.
Then you can follow the previously shared documentation link to test CAN.
Instruction to get started and boot Linux: https://dev.ti.com/tirex/explore/node?node=A__AJmDBSOwjLb1yKNiksusLQ__am64x-devtools__FUz-xrs__LATEST
Regards,
Aparna
Hi Cong Pham,
The Linux driver support for CAN is already present.
I'm using Am64x Starter Kit, not AM64x-GPVM
Apologies for the misunderstanding.
I could find that main domain CAN pins are realised in SOC_MAIN_UART4 and SOC_MAIN_UART5. Check below:

However, only SOC_MAIN_UART5 is drawn out on the user expansion header:

You can connect to this pin, check pinmux configuration of the same.
Regarding connection of an external transceiver, you are right. AM64 SK doesnot have a MCAN transceiver on the board. You can connect preferably TCAN1042D to the above shared MCAN pins. This together will make a CAN node which can act as TX or RX. For the other enc, you will either need the same setup, or a CAN tool such as CANoe or PCAN.
Additionally, you also need to apply the overlay file at the U-boot prompt. Let me check internally regarding this, as I cannot find an overlay file present for AM64x. You might have to re-use nodes from AM62x MCAN overlay file.
Regards,
Aparna
// SPDX-License-Identifier: GPL-2.0
/*
* Copyright (C) 2021 Texas Instruments Incorporated - https://www.ti.com/
*/
/dts-v1/;
#include <dt-bindings/mux/ti-serdes.h>
#include <dt-bindings/phy/phy.h>
#include <dt-bindings/gpio/gpio.h>
#include <dt-bindings/net/ti-dp83867.h>
#include <dt-bindings/leds/common.h>
#include "k3-am642.dtsi"
/ {
compatible = "ti,am642-sk", "ti,am642";
model = "Texas Instruments AM642 SK V04";
chosen {
stdout-path = "serial2:115200n8";
bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000";
};
memory@80000000 {
device_type = "memory";
/* 2G RAM */
reg = <0x00000000 0x80000000 0x00000000 0x80000000>;
};
reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;
secure_ddr: optee@9e800000 {
reg = <0x00 0x9e800000 0x00 0x01800000>; /* for OP-TEE */
alignment = <0x1000>;
no-map;
};
main_r5fss0_core0_dma_memory_region: r5f-dma-memory@a0000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa0000000 0x00 0x100000>;
no-map;
};
main_r5fss0_core0_memory_region: r5f-memory@a0100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa0100000 0x00 0xf00000>;
no-map;
};
main_r5fss0_core1_dma_memory_region: r5f-dma-memory@a1000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa1000000 0x00 0x100000>;
no-map;
};
main_r5fss0_core1_memory_region: r5f-memory@a1100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa1100000 0x00 0xf00000>;
no-map;
};
main_r5fss1_core0_dma_memory_region: r5f-dma-memory@a2000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa2000000 0x00 0x100000>;
no-map;
};
main_r5fss1_core0_memory_region: r5f-memory@a2100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa2100000 0x00 0xf00000>;
no-map;
};
main_r5fss1_core1_dma_memory_region: r5f-dma-memory@a3000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa3000000 0x00 0x100000>;
no-map;
};
main_r5fss1_core1_memory_region: r5f-memory@a3100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa3100000 0x00 0xf00000>;
no-map;
};
mcu_m4fss_dma_memory_region: m4f-dma-memory@a4000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa4000000 0x00 0x100000>;
no-map;
};
mcu_m4fss_memory_region: m4f-memory@a4100000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa4100000 0x00 0xf00000>;
no-map;
};
rtos_ipc_memory_region: ipc-memories@a5000000 {
reg = <0x00 0xa5000000 0x00 0x00800000>;
alignment = <0x1000>;
no-map;
};
};
vusb_main: fixed-regulator-vusb-main5v0 {
/* USB MAIN INPUT 5V DC */
compatible = "regulator-fixed";
regulator-name = "vusb_main5v0";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
regulator-always-on;
regulator-boot-on;
};
vcc_3v3_sys: fixedregulator-vcc-3v3-sys {
/* output of LP8733xx */
compatible = "regulator-fixed";
regulator-name = "vcc_3v3_sys";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
vin-supply = <&vusb_main>;
regulator-always-on;
regulator-boot-on;
};
transceiver1: can-phy0 {
compatible = "ti,tcan1042";
#phy-cells = <0>;
max-bitrate = <5000000>;
};
transceiver2: can-phy1 {
compatible = "ti,tcan1042";
#phy-cells = <0>;
max-bitrate = <5000000>;
};
vdd_mmc1: fixed-regulator-sd {
/* TPS2051BD */
compatible = "regulator-fixed";
regulator-name = "vdd_mmc1";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-boot-on;
enable-active-high;
vin-supply = <&vcc_3v3_sys>;
gpio = <&exp1 3 GPIO_ACTIVE_HIGH>;
};
com8_ls_en: regulator-1 {
compatible = "regulator-fixed";
regulator-name = "com8_ls_en";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
regulator-boot-on;
pinctrl-0 = <&main_com8_ls_en_pins_default>;
pinctrl-names = "default";
gpio = <&main_gpio0 62 GPIO_ACTIVE_LOW>;
};
wlan_en: regulator-2 {
/* output of SN74AVC4T245RSVR */
compatible = "regulator-fixed";
regulator-name = "wlan_en";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
enable-active-high;
pinctrl-0 = <&main_wlan_en_pins_default>;
pinctrl-names = "default";
vin-supply = <&com8_ls_en>;
gpio = <&main_gpio0 48 GPIO_ACTIVE_HIGH>;
};
led-controller {
compatible = "gpio-leds";
led-0 {
color = <LED_COLOR_ID_GREEN>;
function = LED_FUNCTION_INDICATOR;
function-enumerator = <1>;
gpios = <&exp2 0 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-1 {
color = <LED_COLOR_ID_RED>;
function = LED_FUNCTION_INDICATOR;
function-enumerator = <2>;
gpios = <&exp2 1 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-2 {
color = <LED_COLOR_ID_GREEN>;
function = LED_FUNCTION_INDICATOR;
function-enumerator = <3>;
gpios = <&exp2 2 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-3 {
color = <LED_COLOR_ID_AMBER>;
function = LED_FUNCTION_INDICATOR;
function-enumerator = <4>;
gpios = <&exp2 3 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-4 {
color = <LED_COLOR_ID_GREEN>;
function = LED_FUNCTION_INDICATOR;
function-enumerator = <5>;
gpios = <&exp2 4 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-5 {
color = <LED_COLOR_ID_RED>;
function = LED_FUNCTION_INDICATOR;
function-enumerator = <6>;
gpios = <&exp2 5 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-6 {
color = <LED_COLOR_ID_GREEN>;
function = LED_FUNCTION_INDICATOR;
function-enumerator = <7>;
gpios = <&exp2 6 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-7 {
color = <LED_COLOR_ID_AMBER>;
function = LED_FUNCTION_HEARTBEAT;
function-enumerator = <8>;
linux,default-trigger = "heartbeat";
gpios = <&exp2 7 GPIO_ACTIVE_HIGH>;
};
};
};
&main_pmx0 {
main_mmc1_pins_default: main-mmc1-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0294, PIN_INPUT, 0) /* (J19) MMC1_CMD */
AM64X_IOPAD(0x0290, PIN_INPUT, 0) /* (#N/A) MMC1_CLKLB */
AM64X_IOPAD(0x028c, PIN_INPUT, 0) /* (L20) MMC1_CLK */
AM64X_IOPAD(0x0288, PIN_INPUT, 0) /* (K21) MMC1_DAT0 */
AM64X_IOPAD(0x0284, PIN_INPUT, 0) /* (L21) MMC1_DAT1 */
AM64X_IOPAD(0x0280, PIN_INPUT, 0) /* (K19) MMC1_DAT2 */
AM64X_IOPAD(0x027c, PIN_INPUT, 0) /* (K18) MMC1_DAT3 */
AM64X_IOPAD(0x0298, PIN_INPUT, 0) /* (D19) MMC1_SDCD */
>;
};
main_uart0_pins_default: main-uart0-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0238, PIN_INPUT, 0) /* (B16) UART0_CTSn */
AM64X_IOPAD(0x023c, PIN_OUTPUT, 0) /* (A16) UART0_RTSn */
AM64X_IOPAD(0x0230, PIN_INPUT, 0) /* (D15) UART0_RXD */
AM64X_IOPAD(0x0234, PIN_OUTPUT, 0) /* (C16) UART0_TXD */
>;
};
main_uart1_pins_default: main-uart1-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0248, PIN_INPUT, 0) /* UART1_CTSn */
AM64X_IOPAD(0x024c, PIN_OUTPUT, 0) /* UART1_RTSn */
AM64X_IOPAD(0x0240, PIN_INPUT, 0) /* (E15) UART1_RXD */
AM64X_IOPAD(0x0244, PIN_OUTPUT, 0) /* (E14) UART1_TXD */
>;
};
main_usb0_pins_default: main-usb0-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x02a8, PIN_OUTPUT, 0) /* (E19) USB0_DRVVBUS */
>;
};
main_i2c1_pins_default: main-i2c1-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0268, PIN_INPUT_PULLUP, 0) /* (C18) I2C1_SCL */
AM64X_IOPAD(0x026c, PIN_INPUT_PULLUP, 0) /* (B19) I2C1_SDA */
>;
};
mdio1_pins_default: mdio1-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x01fc, PIN_OUTPUT, 4) /* (R2) PRG0_PRU1_GPO19.MDIO0_MDC */
AM64X_IOPAD(0x01f8, PIN_INPUT, 4) /* (P5) PRG0_PRU1_GPO18.MDIO0_MDIO */
>;
};
rgmii1_pins_default: rgmii1-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x011c, PIN_INPUT, 4) /* (AA13) PRG1_PRU1_GPO5.RGMII1_RD0 */
AM64X_IOPAD(0x0128, PIN_INPUT, 4) /* (U12) PRG1_PRU1_GPO8.RGMII1_RD1 */
AM64X_IOPAD(0x0150, PIN_INPUT, 4) /* (Y13) PRG1_PRU1_GPO18.RGMII1_RD2 */
AM64X_IOPAD(0x0154, PIN_INPUT, 4) /* (V12) PRG1_PRU1_GPO19.RGMII1_RD3 */
AM64X_IOPAD(0x00d8, PIN_INPUT, 4) /* (W13) PRG1_PRU0_GPO8.RGMII1_RXC */
AM64X_IOPAD(0x00cc, PIN_INPUT, 4) /* (V13) PRG1_PRU0_GPO5.RGMII1_RX_CTL */
AM64X_IOPAD(0x0124, PIN_OUTPUT, 4) /* (V15) PRG1_PRU1_GPO7.RGMII1_TD0 */
AM64X_IOPAD(0x012c, PIN_OUTPUT, 4) /* (V14) PRG1_PRU1_GPO9.RGMII1_TD1 */
AM64X_IOPAD(0x0130, PIN_OUTPUT, 4) /* (W14) PRG1_PRU1_GPO10.RGMII1_TD2 */
AM64X_IOPAD(0x014c, PIN_OUTPUT, 4) /* (AA14) PRG1_PRU1_GPO17.RGMII1_TD3 */
AM64X_IOPAD(0x00e0, PIN_OUTPUT, 4) /* (U14) PRG1_PRU0_GPO10.RGMII1_TXC */
AM64X_IOPAD(0x00dc, PIN_OUTPUT, 4) /* (U15) PRG1_PRU0_GPO9.RGMII1_TX_CTL */
>;
};
rgmii2_pins_default: rgmii2-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0108, PIN_INPUT, 4) /* (W11) PRG1_PRU1_GPO0.RGMII2_RD0 */
AM64X_IOPAD(0x010c, PIN_INPUT, 4) /* (V11) PRG1_PRU1_GPO1.RGMII2_RD1 */
AM64X_IOPAD(0x0110, PIN_INPUT, 4) /* (AA12) PRG1_PRU1_GPO2.RGMII2_RD2 */
AM64X_IOPAD(0x0114, PIN_INPUT, 4) /* (Y12) PRG1_PRU1_GPO3.RGMII2_RD3 */
AM64X_IOPAD(0x0120, PIN_INPUT, 4) /* (U11) PRG1_PRU1_GPO6.RGMII2_RXC */
AM64X_IOPAD(0x0118, PIN_INPUT, 4) /* (W12) PRG1_PRU1_GPO4.RGMII2_RX_CTL */
AM64X_IOPAD(0x0134, PIN_OUTPUT, 4) /* (AA10) PRG1_PRU1_GPO11.RGMII2_TD0 */
AM64X_IOPAD(0x0138, PIN_OUTPUT, 4) /* (V10) PRG1_PRU1_GPO12.RGMII2_TD1 */
AM64X_IOPAD(0x013c, PIN_OUTPUT, 4) /* (U10) PRG1_PRU1_GPO13.RGMII2_TD2 */
AM64X_IOPAD(0x0140, PIN_OUTPUT, 4) /* (AA11) PRG1_PRU1_GPO14.RGMII2_TD3 */
AM64X_IOPAD(0x0148, PIN_OUTPUT, 4) /* (Y10) PRG1_PRU1_GPO16.RGMII2_TXC */
AM64X_IOPAD(0x0144, PIN_OUTPUT, 4) /* (Y11) PRG1_PRU1_GPO15.RGMII2_TX_CTL */
>;
};
ospi0_pins_default: ospi0-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0000, PIN_OUTPUT, 0) /* (N20) OSPI0_CLK */
AM64X_IOPAD(0x002c, PIN_OUTPUT, 0) /* (L19) OSPI0_CSn0 */
AM64X_IOPAD(0x000c, PIN_INPUT, 0) /* (M19) OSPI0_D0 */
AM64X_IOPAD(0x0010, PIN_INPUT, 0) /* (M18) OSPI0_D1 */
AM64X_IOPAD(0x0014, PIN_INPUT, 0) /* (M20) OSPI0_D2 */
AM64X_IOPAD(0x0018, PIN_INPUT, 0) /* (M21) OSPI0_D3 */
AM64X_IOPAD(0x001c, PIN_INPUT, 0) /* (P21) OSPI0_D4 */
AM64X_IOPAD(0x0020, PIN_INPUT, 0) /* (P20) OSPI0_D5 */
AM64X_IOPAD(0x0024, PIN_INPUT, 0) /* (N18) OSPI0_D6 */
AM64X_IOPAD(0x0028, PIN_INPUT, 0) /* (M17) OSPI0_D7 */
AM64X_IOPAD(0x0008, PIN_INPUT, 0) /* (N19) OSPI0_DQS */
>;
};
main_ecap0_pins_default: main-ecap0-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0270, PIN_INPUT, 0) /* (D18) ECAP0_IN_APWM_OUT */
>;
};
main_gpio_pins_default: main-gpio-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x00F4, PIN_OUTPUT, 7) /* (Y9) GPIO0_60 */
>;
};
main_mcan0_pins_default: main-mcan0-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0254, PIN_INPUT, 0) /* (B17) MCAN0_RX */
AM64X_IOPAD(0x0250, PIN_OUTPUT, 0) /* (A17) MCAN0_TX */
>;
};
main_mcan1_pins_default: main-mcan1-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x025C, PIN_INPUT, 0) /* (D17) MCAN0_RX */
AM64X_IOPAD(0x0258, PIN_OUTPUT, 0) /* (C17) MCAN0_TX */
>;
};
main_wlan_en_pins_default: main-wlan-en-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x00c4, PIN_OUTPUT_PULLUP, 7) /* (V8) GPIO0_48 */
>;
};
main_com8_ls_en_pins_default: main-com8-ls-en-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x00fc, PIN_OUTPUT, 7) /* (U7) PRG1_PRU0_GPO17.GPIO0_62 */
>;
};
main_wlan_pins_default: main-wlan-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x00bc, PIN_INPUT, 7) /* (U8) GPIO0_46 */
>;
};
main_eqep0_pins_default: main-eqep0-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x00a0, PIN_INPUT, 3) /* (N16) GPMC0_WPn.EQEP0_A */
AM64X_IOPAD(0x00a4, PIN_INPUT, 3) /* (N17) GPMC0_DIR.EQEP0_B */
AM64X_IOPAD(0x00ac, PIN_INPUT, 3) /* (R20) GPMC0_CSn1.EQEP0_I */
AM64X_IOPAD(0x00a8, PIN_INPUT, 3) /* (R19) GPMC0_CSn0.EQEP0_S */
>;
};
};
&main_mcan1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_mcan1_pins_default>;
phys = <&transceiver2>;
};
/*&main_mcan0 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_mcan0_pins_default>;
phys = <&transceiver1>;
};
*/
&main_gpio0 {
pinctrl-names = "default";
pinctrl-0 = <&main_gpio_pins_default>;
status = "okay";
};
&main_uart0 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_uart0_pins_default>;
};
&main_uart1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_uart1_pins_default>;
};
&main_i2c1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_i2c1_pins_default>;
clock-frequency = <400000>;
exp1: gpio@70 {
compatible = "nxp,pca9538";
reg = <0x70>;
gpio-controller;
#gpio-cells = <2>;
gpio-line-names = "GPIO_CPSW2_RST", "GPIO_CPSW1_RST",
"PRU_DETECT", "MMC1_SD_EN",
"VPP_LDO_EN", "RPI_PS_3V3_En",
"RPI_PS_5V0_En", "RPI_HAT_DETECT";
};
exp2: gpio@60 {
compatible = "ti,tpic2810";
reg = <0x60>;
gpio-controller;
#gpio-cells = <2>;
gpio-line-names = "LED1","LED2","LED3","LED4","LED5","LED6","LED7","LED8";
};
};
/* mcu_gpio0 and mcu_gpio_intr are reserved for mcu firmware usage */
&mcu_gpio0 {
status = "reserved";
};
&mcu_gpio_intr {
status = "reserved";
};
&sdhci0 {
status = "okay";
vmmc-supply = <&wlan_en>;
bus-width = <4>;
non-removable;
cap-power-off-card;
keep-power-in-suspend;
ti,driver-strength-ohm = <50>;
#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@2 {
compatible = "ti,wl1837";
reg = <2>;
pinctrl-0 = <&main_wlan_pins_default>;
pinctrl-names = "default";
interrupt-parent = <&main_gpio0>;
interrupts = <46 IRQ_TYPE_EDGE_FALLING>;
};
};
&sdhci1 {
/* SD/MMC */
status = "okay";
vmmc-supply = <&vdd_mmc1>;
pinctrl-names = "default";
pinctrl-0 = <&main_mmc1_pins_default>;
disable-wp;
};
&serdes_ln_ctrl {
idle-states = <AM64_SERDES0_LANE0_USB>;
};
&serdes0 {
serdes0_usb_link: phy@0 {
reg = <0>;
cdns,num-lanes = <1>;
#phy-cells = <0>;
cdns,phy-type = <PHY_TYPE_USB3>;
resets = <&serdes_wiz0 1>;
};
};
&usbss0 {
ti,vbus-divider;
};
&usb0 {
dr_mode = "host";
maximum-speed = "super-speed";
pinctrl-names = "default";
pinctrl-0 = <&main_usb0_pins_default>;
phys = <&serdes0_usb_link>;
phy-names = "cdns3,usb3-phy";
};
&cpsw3g {
pinctrl-names = "default";
pinctrl-0 = <&rgmii1_pins_default
&rgmii2_pins_default>;
/* Map HW8_TS_PUSH to GENF1 */
cpts@3d000 {
ti,pps = <7 1>;
};
};
&cpsw_port1 {
phy-mode = "rgmii-rxid";
phy-handle = <&cpsw3g_phy0>;
};
&cpsw_port2 {
phy-mode = "rgmii-rxid";
phy-handle = <&cpsw3g_phy1>;
};
&cpsw3g_mdio {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&mdio1_pins_default>;
cpsw3g_phy0: ethernet-phy@0 {
reg = <0>;
ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
};
cpsw3g_phy1: ethernet-phy@1 {
reg = <1>;
ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
};
};
&tscadc0 {
status = "okay";
adc {
ti,adc-channels = <0 1 2 3 4 5 6 7>;
};
};
&ospi0 {
pinctrl-names = "default";
pinctrl-0 = <&ospi0_pins_default>;
flash@0 {
compatible = "jedec,spi-nor";
reg = <0x0>;
spi-tx-bus-width = <8>;
spi-rx-bus-width = <8>;
spi-max-frequency = <25000000>;
cdns,tshsl-ns = <60>;
cdns,tsd2d-ns = <60>;
cdns,tchsh-ns = <60>;
cdns,tslch-ns = <60>;
cdns,read-delay = <4>;
partitions {
compatible = "fixed-partitions";
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "ospi.tiboot3";
reg = <0x0 0x100000>;
};
partition@100000 {
label = "ospi.tispl";
reg = <0x100000 0x200000>;
};
partition@300000 {
label = "ospi.u-boot";
reg = <0x300000 0x400000>;
};
partition@700000 {
label = "ospi.env";
reg = <0x700000 0x40000>;
};
partition@740000 {
label = "ospi.env.backup";
reg = <0x740000 0x40000>;
};
partition@800000 {
label = "ospi.rootfs";
reg = <0x800000 0x37c0000>;
};
partition@3fc0000 {
label = "ospi.phypattern";
reg = <0x3fc0000 0x40000>;
};
};
};
};
&mailbox0_cluster2 {
mbox_main_r5fss0_core0: mbox-main-r5fss0-core0 {
ti,mbox-rx = <0 0 2>;
ti,mbox-tx = <1 0 2>;
};
mbox_main_r5fss0_core1: mbox-main-r5fss0-core1 {
ti,mbox-rx = <2 0 2>;
ti,mbox-tx = <3 0 2>;
};
};
&mailbox0_cluster3 {
status = "disabled";
};
&mailbox0_cluster4 {
mbox_main_r5fss1_core0: mbox-main-r5fss1-core0 {
ti,mbox-rx = <0 0 2>;
ti,mbox-tx = <1 0 2>;
};
mbox_main_r5fss1_core1: mbox-main-r5fss1-core1 {
ti,mbox-rx = <2 0 2>;
ti,mbox-tx = <3 0 2>;
};
};
&mailbox0_cluster5 {
status = "disabled";
};
&mailbox0_cluster6 {
mbox_m4_0: mbox-m4-0 {
ti,mbox-rx = <0 0 2>;
ti,mbox-tx = <1 0 2>;
};
};
&mailbox0_cluster7 {
status = "disabled";
};
&main_r5fss0_core0 {
mboxes = <&mailbox0_cluster2 &mbox_main_r5fss0_core0>;
memory-region = <&main_r5fss0_core0_dma_memory_region>,
<&main_r5fss0_core0_memory_region>;
};
&main_r5fss0_core1 {
mboxes = <&mailbox0_cluster2 &mbox_main_r5fss0_core1>;
memory-region = <&main_r5fss0_core1_dma_memory_region>,
<&main_r5fss0_core1_memory_region>;
};
&main_r5fss1_core0 {
mboxes = <&mailbox0_cluster4 &mbox_main_r5fss1_core0>;
memory-region = <&main_r5fss1_core0_dma_memory_region>,
<&main_r5fss1_core0_memory_region>;
};
&main_r5fss1_core1 {
mboxes = <&mailbox0_cluster4 &mbox_main_r5fss1_core1>;
memory-region = <&main_r5fss1_core1_dma_memory_region>,
<&main_r5fss1_core1_memory_region>;
};
&mcu_m4fss {
mboxes = <&mailbox0_cluster6 &mbox_m4_0>;
memory-region = <&mcu_m4fss_dma_memory_region>,
<&mcu_m4fss_memory_region>;
};
&ecap0 {
status = "okay";
/* PWM is available on Pin 1 of header J3 */
pinctrl-names = "default";
pinctrl-0 = <&main_ecap0_pins_default>;
};
&eqep0 {
/* EQEP0_A is available on Pin 18 of header J4 */
/* EQEP0_B is available on Pin 22 of header J4 */
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_eqep0_pins_default>;
};
#define TS_OFFSET(pa, val) (0x4+(pa)*4) (0x10000 | val)
×ync_router {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&cpsw_cpts_pps>;
/*
* Use Time Sync Router to map GENF1 input to HW8_TS_PUSH output as well
* as the PRU ICSSG0 SYNC1 output.
*/
cpsw_cpts_pps: cpsw-cpts-pps {
pinctrl-single,pins = <
/* pps [cpts genf1] in22 -> out37 [cpts hw8_push] */
TS_OFFSET(37, 22)
/* pps [cpts genf1] in22 -> out26 [SYNC1_OUT pin] */
TS_OFFSET(26, 22)
>;
};
};