Tool/software:
1. Hardware : TDA4 (TI EVM)
2. SDK: 0902
3. u-boot, linux image, rootfs all use 0902 prebuild
4. MCU1_0 bootapp use the following path:pdk_jacinto_09_02_00_30/packages/ti/boot/sbl/example/boot_app
5. sbl uses the command to compile
make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_mmcsd_img -sj
6. For adding u-boot, please refer to the following link
e2e.ti.com/.../faq-tda4vm-how-to-load-main-core-images-from-emmc-with-boot_app

The current problem is that starting the Kernel will report an error

The complete log is as follows
Welcome to minicom 2.7.1
OPTIONS: I18n
Compiled on Dec 23 2019, 02:06:26.
Port /dev/ttyUSB2, 18:19:20
Press CTRL-A Z for help on special keys
root@j721e-evm:~# NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
NOTICE: BL31: Built : 16:09:05, Feb 9 2024
ERROR: GTC_CNTFID0 is 0! Assuming 200000000 Hz. Fix Bootloader
I/TC:
I/TC: OP-TEE version: 4.1.0-51-g012cdca49 (gcc version 11.4.0 (GCC)) #1 Tue Jan 30 10:48:03 UTC 2024 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot
U-Boot SPL 2023.04-dirty (Jul 31 2024 - 14:51:01 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)')
ti_i2c_eeprom_am6_parse_record: Ignoring record id 17
Detected: J7X-BASE-CPB rev A
spl_boot_device: hack to boot from SD card
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
U-Boot 2023.04-ti-gf9b966c67473 (Mar 19 2024 - 20:31:40 +0000)
SoC: J721E SR1.1 GP
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev A
DRAM: 2 GiB (effective 4 GiB)
Core: 126 devices, 35 uclasses, devicetree: separate
Flash: 0 Bytes
MMC: mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from nowhere... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Detected: J7X-BASE-CPB rev A
phy-j721e-wiz wiz@5000000: SERDES already configured
Sierra init failed:-16
Net: eth0: ethernet@46000000port@1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
723 bytes read in 29 ms (23.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
1 bytes read in 30 ms (0 Bytes/s)
Already setup.
gpio: pin gpio@22_17 (gpio 281) value is 1
gpio: pin gpio@22_16 (gpio 280) value is 0
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
Failed to load '/lib/firmware/j7-mcu-r5f0_1-fw'
1572544 bytes read in 71 ms (21.1 MiB/s)
Load Remote Processor 2 with data@addr=0x82000000 1572544 bytes: Success!
322804 bytes read in 44 ms (7 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 322804 bytes: Success!
Failed to load '/lib/firmware/j7-main-r5f1_0-fw'
Failed to load '/lib/firmware/j7-main-r5f1_1-fw'
1002288 bytes read in 57 ms (16.8 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 1002288 bytes: Success!
1002288 bytes read in 58 ms (16.5 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 1002288 bytes: Success!
13504656 bytes read in 318 ms (40.5 MiB/s)
Load Remote Processor 8 with data@addr=0x82000000 13504656 bytes: Success!
19376640 bytes read in 437 ms (42.3 MiB/s)
114992 bytes read in 36 ms (3 MiB/s)
Working FDT set to 88000000
3589 bytes read in 34 ms (102.5 KiB/s)
11541 bytes read in 34 ms (331.1 KiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
ERROR: reserving fdt memory region failed (addr=880000000 size=27000000 flags=4)
Loading Device Tree to 000000008fee0000, end 000000008fffffff ... OK
Working FDT set to 8fee0000
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 6.1.80-ti-g2e423244f8c0 (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP4
[ 0.000000] Machine model: Texas Instruments J721e EVM
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000008e0000000, size 512 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a8100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a9000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a9100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 96 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@ac000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@b2000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b2100000, size 95 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71-memory@b2100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000d8000000, size 192 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@d8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e4000000, size 8 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-queues@e4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e4800000, size 24 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-buffers@e4800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 624 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8000000-0x00000000d7ffffff]
[ 0.000000] node 0: [mem 0x00000000d8000000-0x00000000e5ffffff]
[ 0.000000] node 0: [mem 0x00000000e6000000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008a6ffffff]
[ 0.000000] node 0: [mem 0x00000008a7000000-0x00000008ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.4
[ 0.000000] percpu: Embedded 20 pages/cpu s41064 r8192 d32664 u81920
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Spectre-v3a
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] CPU features: detected: ARM erratum 1742098
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=e9206496-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 2.
[ 0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
[ 0.000000] Memory: 1695672K/4194304K available (11712K kernel code, 1258K rwdata, 3812K rodata, 1984K init, 438K bss, 1974344K reserved, 524288K c)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8a7800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x00000008a7030000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008a7040000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008435] Console: colour dummy device 80x25
[ 0.013004] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023675] pid_max: default: 32768 minimum: 301
[ 0.028411] LSM: Security Framework initializing
[ 0.033190] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.040763] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.049555] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.056952] cblist_init_generic: Setting shift to 1 and lim to 1.
[ 0.063214] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.070601] cblist_init_generic: Setting shift to 1 and lim to 1.
[ 0.076904] rcu: Hierarchical SRCU implementation.
[ 0.081802] rcu: Max phase no-delay instances is 1000.
[ 0.087325] Platform MSI: msi-controller@1820000 domain created
[ 0.093603] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.103088] EFI services will not be available.
[ 0.107831] smp: Bringing up secondary CPUs ...
ERROR: GTC_CNTFID0 is 0! Assuming 200000000 Hz. Fix Bootloader
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[ 0.126808] Detected PIPT I-cache on CPU1
[ 0.126870] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.126882] GICv3: CPU1: using allocated LPI pending table @0x00000008a7050000
[ 0.126912] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.126957] smp: Brought up 1 node, 2 CPUs
[ 0.156299] SMP: Total of 2 processors activated.
[ 0.161103] CPU features: detected: 32-bit EL0 Support
[ 0.166355] CPU features: detected: CRC32 instructions
[ 0.171632] CPU: All CPU(s) started at EL2
[ 0.175813] alternatives: applying system-wide alternatives
[ 0.182380] devtmpfs: initialized
[ 0.192790] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.202774] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.218747] pinctrl core: initialized pinctrl subsystem
[ 0.224422] DMI not present or invalid.
[ 0.228676] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.235312] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.242630] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.250638] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.258764] audit: initializing netlink subsys (disabled)
[ 0.264382] audit: type=2000 audit(0.172:1): state=initialized audit_enabled=0 res=1
[ 0.264613] thermal_sys: Registered thermal governor 'step_wise'
[ 0.272301] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.278506] cpuidle: using governor menu
[ 0.289258] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.296218] ASID allocator initialised with 65536 entries
[ 0.310988] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@100000/pinctrl@a40000/mcu-cpsw-cpts
[ 0.322575] KASLR disabled due to lack of seed
[ 0.329902] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.336845] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.343247] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.350180] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.356581] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.363514] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.369915] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.376848] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.383964] k3-chipinfo 43000014.chipid: Family:J721E rev:SR2.0 JTAGID[0x1bb6402f] Detected
[ 0.393293] iommu: Default domain type: Translated
[ 0.398281] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.404794] SCSI subsystem initialized
[ 0.408779] usbcore: registered new interface driver usbfs
[ 0.414398] usbcore: registered new interface driver hub
[ 0.419834] usbcore: registered new device driver usb
[ 0.425209] pps_core: LinuxPPS API ver. 1 registered
[ 0.430280] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.439617] PTP clock support registered
[ 0.443700] EDAC MC: Ver: 3.0.0
[ 0.447399] FPGA manager framework
[ 0.450912] Advanced Linux Sound Architecture Driver Initialized.
[ 0.457518] clocksource: Switched to clocksource arch_sys_counter
[ 0.463859] VFS: Disk quotas dquot_6.6.0
[ 0.467890] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.477833] Carveout Heap: Exported 512 MiB at 0x00000000b8000000
[ 0.484125] NET: Registered PF_INET protocol family
[ 0.489291] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.498320] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.507081] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.515005] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.523210] TCP bind hash table entries: 32768 (order: 8, 1048576 bytes, linear)
[ 0.531821] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.538606] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.545522] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.552972] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.559050] RPC: Registered named UNIX socket transport module.
[ 0.565111] RPC: Registered udp transport module.
[ 0.569913] RPC: Registered tcp transport module.
[ 0.574716] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.581298] NET: Registered PF_XDP protocol family
[ 0.586206] PCI: CLS 0 bytes, default 64
[ 0.590584] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.599759] Initialise system trusted keyrings
[ 0.604423] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[ 0.612972] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.619208] NFS: Registering the id_resolver key type
[ 0.624387] Key type id_resolver registered
[ 0.628659] Key type id_legacy registered
[ 0.632776] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.639624] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.666925] Key type asymmetric registered
[ 0.671109] Asymmetric key parser 'x509' registered
[ 0.676115] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.683752] io scheduler mq-deadline registered
[ 0.688382] io scheduler kyber registered
[ 0.694765] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[ 0.701182] pinctrl-single 11c000.pinctrl: 173 pins, size 692
[ 0.707738] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[ 0.717199] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[ 0.725583] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00001faf)
[ 0.733795] arm-smmu-v3 36600000.iommu: allocated 65536 entries for cmdq
[ 0.740947] arm-smmu-v3 36600000.iommu: allocated 32768 entries for evtq
[ 0.748909] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs
[ 0.759861] loop: module loaded
[ 0.763809] megasas: 07.719.03.00-rc1
[ 0.769106] tun: Universal TUN/TAP device driver, 1.6
[ 0.774691] VFIO - User Level meta-driver version: 0.3
[ 0.780341] usbcore: registered new interface driver usb-storage
[ 0.786806] i2c_dev: i2c /dev entries driver
[ 0.791736] sdhci: Secure Digital Host Controller Interface driver
[ 0.798057] sdhci: Copyright(c) Pierre Ossman
[ 0.802655] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.808783] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.815015] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.821756] usbcore: registered new interface driver usbhid
[ 0.827449] usbhid: USB HID core driver
[ 0.831867] optee: probing for conduit method.
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[ 0.836426] optee: revision 4.1 (012cdca4)
[ 0.852847] optee: dynamic shared memory is enabled
[ 0.862230] optee: initialized driver
[ 0.867258] Initializing XFRM netlink socket
[ 0.871645] NET: Registered PF_PACKET protocol family
[ 0.876845] Key type dns_resolver registered
[ 0.881384] registered taskstats version 1
[ 0.885582] Loading compiled-in X.509 certificates
[ 0.896254] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)')
[ 0.954350] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.960666] pca953x 1-0020: supply vcc not found, using dummy regulator
[ 0.967498] pca953x 1-0020: using no AI
[ 0.994196] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 1.001000] pca953x 1-0022: using AI
[ 1.005268] gpio-480 (CTRL_PM_I2C_OE): hogged as output/high
[ 1.011244] gpio-481 (MCASP/TRACE_MUX_S0): hogged as output/low
[ 1.017484] gpio-482 (MCASP/TRACE_MUX_S1): hogged as output/high
[ 1.023983] omap_i2c 2000000.i2c: bus 1 rev0.12 at 400 kHz
[ 1.030704] omap_i2c 2020000.i2c: bus 2 rev0.12 at 400 kHz
[ 1.036847] pca953x 3-0020: supply vcc not found, using dummy regulator
[ 1.043677] pca953x 3-0020: using no AI
[ 1.069976] omap_i2c 2030000.i2c: bus 3 rev0.12 at 400 kHz
[ 1.075845] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 137 domain created
[ 1.084377] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 131 domain created
[ 1.093702] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 213 domain created
[ 1.102297] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[ 1.116203] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[ 1.126098] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 1.132859] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 1.141946] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211
[ 1.152093] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 1.158851] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 1.166767] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 192, base_baud = 6000000) is a 8250
[ 1.176237] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 193, base_baud = 3000000) is a 8250
[ 1.185089] printk: console [ttyS2] enabled
[ 1.185089] printk: console [ttyS2] enabled
[ 1.193531] printk: bootconsole [ns16550a0] disabled
[ 1.193531] printk: bootconsole [ns16550a0] disabled
[ 1.203925] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 194, base_baud = 3000000) is a 8250
[ 1.212886] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 195, base_baud = 3000000) is a 8250
[ 1.222853] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 1.269521] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.278186] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 1.286457] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[ 1.299270] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 1.306478] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 1.312642] pps pps0: new PPS source ptp0
[ 1.316768] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:1
[ 1.327038] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[ 1.335797] mmc0: CQHCI version 5.10
[ 1.378092] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[ 1.467242] mmc0: Command Queue Engine enabled
[ 1.471696] mmc0: new HS200 MMC card at address 0001
[ 1.477104] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[ 1.484459] mmcblk0: p1
[ 1.487390] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB
[ 1.493139] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB
[ 1.498785] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (240:0)
[ 1.666247] tps6594-rtc tps6594-rtc.4.auto: registered as rtc0
[ 1.672208] tps6594-rtc tps6594-rtc.4.auto: hctosys: unable to read the hardware clock
[ 1.938389] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[ 1.945181] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[ 1.951952] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[ 1.958723] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[ 1.965493] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[ 1.978223] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[ 1.988828] ti-udma 31150000.dma-controller: Channels: 122 (tchan: 61, rchan: 61, gp-rflow: 16)
[ 2.002199] spi-nor spi0.0: mt35xu512aba (65536 Kbytes)
[ 2.007487] 8 fixed-partitions partitions found on MTD device 47040000.spi.0
[ 2.014523] Creating 8 MTD partitions on "47040000.spi.0":
[ 2.020001] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 2.026025] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 2.031777] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 2.037605] 0x000000680000-0x0000006a0000 : "ospi.env"
[ 2.043143] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup"
[ 2.049296] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[ 2.055017] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[ 2.060838] 0x000003fe0000-0x000004000000 : "ospi.phypattern"
[ 2.071663] spi-nor spi1.0: mt25qu512a (65536 Kbytes)
[ 2.076753] 8 fixed-partitions partitions found on MTD device 47050000.spi.0
[ 2.083793] Creating 8 MTD partitions on "47050000.spi.0":
[ 2.089265] 0x000000000000-0x000000080000 : "qspi.tiboot3"
[ 2.095221] 0x000000080000-0x000000280000 : "qspi.tispl"
[ 2.100953] 0x000000280000-0x000000680000 : "qspi.u-boot"
[ 2.106741] 0x000000680000-0x0000006a0000 : "qspi.env"
[ 2.112287] 0x0000006a0000-0x0000006c0000 : "qspi.env.backup"
[ 2.118437] 0x0000006c0000-0x0000007c0000 : "qspi.sysfw"
[ 2.124162] 0x000000800000-0x000003fc0000 : "qspi.rootfs"
[ 2.129999] 0x000003fe0000-0x000004000000 : "qspi.phypattern"
[ 2.136694] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 2.181530] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.190238] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 2.198509] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[ 2.211319] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 2.218526] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 2.224665] pps pps0: new PPS source ptp1
[ 2.228800] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:1
[ 2.238944] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 2.247193] mmc1: CQHCI version 5.10
[ 2.253778] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 2.268826] ALSA device list:
[ 2.271805] No soundcards found.
[ 2.291072] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[ 2.298702] Waiting for root device PARTUUID=e9206496-02...
[ 2.853170] mmc1: new ultra high speed DDR50 SDHC card at address 59b4
[ 2.860070] mmcblk1: mmc1:59b4 SD3.0 30.3 GiB
[ 2.866248] mmcblk1: p1 p2
[ 4.006354] EXT4-fs (mmcblk1p2): recovery complete
[ 4.017041] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
[ 4.025587] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 4.037877] devtmpfs: mounted
[ 4.041798] Freeing unused kernel memory: 1984K
[ 4.046398] Run /sbin/init as init process
[ 4.374572] systemd[1]: System time before build time, advancing clock.
[ 4.446856] NET: Registered PF_INET6 protocol family
[ 4.452329] Segment Routing with IPv6
[ 4.456003] In-situ OAM (IOAM) with IPv6
[ 4.505534] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +B)
[ 4.536911] systemd[1]: Detected architecture arm64.
Welcome to Arago 2023.10!
[ 4.592570] systemd[1]: Hostname set to <j721e-evm>.
[ 4.719798] systemd-sysv-generator[148]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a .
[ 4.947692] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please.
[ 5.005665] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Ple.
[ 5.067464] systemd[1]: Queued start job for default target Graphical Interface.
[ 5.107421] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 5.130899] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 5.154834] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 5.178541] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 5.201725] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password �…ts to Console Directory Watch.
[ 5.225645] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R�…uests to Wall Directory Watch.
[ 5.249707] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 5.265575] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 5.285566] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 5.301579] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 5.351784] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 5.373647] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 5.398767] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 5.421742] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 5.445905] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 5.465792] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 5.485819] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 5.501888] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 5.525872] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 5.545753] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 5.565776] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 5.605845] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 5.623999] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 5.661826] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 5.681789] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[ 5.699735] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 5.738002] systemd[1]: Starting Create List of Static Device Nodes...
Starting Create List of Static Device Nodes...
[ 5.764031] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 5.787927] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 5.812056] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 5.828172] fuse: init (API version 7.37)
[ 5.839719] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 5.893999] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 5.913753] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[ 5.929762] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 5.982081] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 6.000382] systemd[1]: Starting Generate network units from Kernel command line...
Starting Generate network �…ts from Kernel command line...
[ 6.020050] cryptodev: loading out-of-tree module taints kernel.
[ 6.026943] cryptodev: driver 1.12 loaded.
[ 6.028964] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 6.046813] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
[ 6.070050] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 6.094079] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 6.114054] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Create List of Static Device Nodes.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star�…progress communication helper.
[ OK ] Finished Load Kernel Modules.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 6.459413] systemd-journald[163]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /media/ram...
Mounting /var/volatile...
[ 6.647899] audit: type=1334 audit(1651167747.272:2): prog-id=5 op=LOAD
[ 6.655401] audit: type=1334 audit(1651167747.280:3): prog-id=6 op=LOAD
Starting Rule-based Manage�…for Device Events and Files...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
[ 7.261550] random: crng init done
[ OK ] Listening on PC/SC Smart Card Daemon Activation Socket.
Starting Weston socket...
Starting D-Bus System Message Bus...
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ 7.374018] ina2xx 2-0040: power monitor ina226 (Rshunt = 10000 uOhm)
[ OK ] Finished Load/Save Random Seed.[ 7.382968] ina2xx 2-0041: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.396205] ina2xx 2-0042: power monitor ina226 (Rshunt = 10000 uOhm)
[ OK ] Listening on Weston socket.[ 7.406385] ina2xx 2-0043: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.416333] ina2xx 2-0044: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.424278] ina2xx 2-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[ 7.432282] ina2xx 2-0046: power monitor ina226 (Rshunt = 10000 uOhm)
[ OK ] Reached target Socket Units.[ 7.440121] ina2xx 2-0047: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.452387] ina2xx 2-0048: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.459981] ina2xx 2-0049: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.467878] ina2xx 2-004a: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.475596] ina2xx 2-004b: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.482924] ina2xx 2-004c: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.490230] ina2xx 2-004d: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.497408] ina2xx 2-004e: power monitor ina226 (Rshunt = 10000 uOhm)
[ 7.504710] ina2xx 2-004f: power monitor ina226 (Rshunt = 10000 uOhm)
[ OK ] Found device /dev/ttyS2.
[ OK ] Finished Reboot and dump vmcore via kexec.
[ 7.623066] CAN device driver interface
[ 7.680400] mc: Linux media interface: v0.10
[ 7.703306] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a9000000
[ 7.719788] k3-dsp-rproc 4d80800000.dsp: configured DSP for IPC-only mode
[ 7.722006] PVR_K: 195: Device: 4e20000000.gpu
[ 7.727191] remoteproc remoteproc0: 4d80800000.dsp is available
[ 7.737877] remoteproc remoteproc0: attaching to 4d80800000.dsp
[ 7.744157] k3-dsp-rproc 4d80800000.dsp: DSP initialized in IPC-only mode
[ 7.751087] j721e-pcie-host 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[ 7.755445] PVR_K: 195: Read BVNC 22.104.208.318 from HW device registers
[ 7.759295] j721e-pcie-host 2900000.pcie: IO 0x0010001000..0x0010010fff -> 0x0010001000
[ 7.766609] rproc-virtio rproc-virtio.10.auto: assigned reserved memory node vision-apps-c66-dma-memory@a9000000
[ 7.775056] j721e-pcie-host 2900000.pcie: MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[ 7.775092] PVR_K: 195: RGX Device registered with BVNC 22.104.208.318
[ 7.787300] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 7.793125] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
[ 7.813659] rproc-virtio rproc-virtio.10.auto: registered virtio0 (type 7)
[ 7.821198] remoteproc remoteproc0: remote processor 4d80800000.dsp is now attached
[ 7.831055] k3-dsp-rproc 4d80800000.dsp: register pm nitifiers in remoteproc mode
[ 7.840629] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a8000000
[ 7.852369] k3-dsp-rproc 4d81800000.dsp: configured DSP for IPC-only mode
[ 7.855056] [drm] Initialized pvr 23.3.6512818 20170530 for 4e20000000.gpu on minor 0
[ 7.860164] remoteproc remoteproc1: 4d81800000.dsp is available
[ 7.867886] videodev: Linux video capture interface: v2.00
[ 7.878586] remoteproc remoteproc1: attaching to 4d81800000.dsp
[ 7.885716] j721e-pcie-host 2900000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 7.913228] k3-dsp-rproc 4d81800000.dsp: DSP initialized in IPC-only mode
[ 7.933260] rproc-virtio rproc-virtio.13.auto: assigned reserved memory node vision-apps-c66-dma-memory@a8000000
[ 7.946297] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 7.949226] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
[ 7.952479] rproc-virtio rproc-virtio.13.auto: registered virtio1 (type 7)
[ 7.965780] remoteproc remoteproc1: remote processor 4d81800000.dsp is now attached
[ 7.973499] k3-dsp-rproc 4d81800000.dsp: register pm nitifiers in remoteproc mode
[ 7.983073] k3-dsp-rproc 64800000.dsp: assigned reserved memory node vision-apps-c71-dma-memory@b2000000
[ 7.996996] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode
[ 8.009711] remoteproc remoteproc2: 64800000.dsp is available
[ 8.027102] remoteproc remoteproc2: attaching to 64800000.dsp
[ 8.044874] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[ 8.069230] remoteproc remoteproc2: unsupported resource 65538
[ 8.098433] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode
[ 8.108076] platform 41000000.r5f: configured R5F for IPC-only mode
[ 8.114631] platform 41000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
[ 8.124923] remoteproc remoteproc3: 41000000.r5f is available
[ 8.133486] rproc-virtio rproc-virtio.14.auto: assigned reserved memory node vision-apps-c71-dma-memory@b2000000
[ 8.133602] remoteproc remoteproc3: attaching to 41000000.r5f
[ 8.149511] Unable to handle kernel paging request at virtual address ffff800011ffffff
[ 8.157487] Mem abort info:
[ 8.160286] ESR = 0x0000000096000006
[ 8.164118] EC = 0x25: DABT (current EL), IL = 32 bits
[ 8.169954] SET = 0, FnV = 0
[ 8.173865] EA = 0, S1PTW = 0
[ 8.178709] FSC = 0x06: level 2 translation fault
[ 8.183710] Data abort info:
[ 8.189764] ISV = 0, ISS = 0x00000006
[ 8.194047] CM = 0, WnR = 0
[ 8.196129] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 8.197639] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000082f40000
[ 8.202597] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
[ 8.209445] [ffff800011ffffff] pgd=10000008dffff003, p4d=10000008dffff003, pud=10000008dfffe003, pmd=0000000000000000
[ 8.228001] Internal error: Oops: 0000000096000006 [#1] PREEMPT SMP
[ 8.232534] rproc-virtio rproc-virtio.14.auto: registered virtio2 (type 7)
[ 8.234263] Modules linked in: videobuf2_dma_sg videobuf2_dma_contig videobuf2_memops v4l2_mem2mem ti_k3_r5_remoteproc(+) videobuf2_v4l2 videobuf2_6
[ 8.246302] remoteproc remoteproc2: remote processor 64800000.dsp is now attached
[ 8.294233] CPU: 1 PID: 197 Comm: systemd-udevd Tainted: G O 6.1.80-ti-g2e423244f8c0 #1
[ 8.294238] Hardware name: Texas Instruments J721e EVM (DT)
[ 8.294241] pstate: 00000005 (nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 8.294245] pc : rproc_handle_resources.constprop.0+0x94/0x168
[ 8.294260] lr : rproc_boot+0x450/0x570
[ 8.294265] sp : ffff800009d0b770
[ 8.294267] x29: ffff800009d0b770 x28: ffff00082af614d0 x27: ffff00082df10f80
[ 8.294273] x26: ffffffffffffffff
[ 8.303833] k3-dsp-rproc 64800000.dsp: register pm nitifiers in remoteproc mode
[ 8.311100] x25: ffff800012000000 x24: ffff800008ebd020
[ 8.311104] x23: ffff00082af61038 x22: 0000000000000000 x21: ffff800009257778
[ 8.311109] x20: ffff00082af61000 x19: 0000000000000000 x18: ffffffffffffffff
[ 8.311114] x17: 0000000000000000 x16: ffff00082953c000 x15: ffffffffffffffff
[ 8.311119] x14: ffffffffffffffff x13: ffffffffffffffff x12: ffffffffffffffff
[ 8.311125] x11: ffffffffffffffff x10: ffffffffffffffff x9 : ffffffffffffffff
[ 8.311130] x8 : ffffffffffffffff x7 : ffffffffffffffff x6 : ffffffffffffffff
[ 8.402229] x5 : ffff00082dd88f00 x4 : ffff800012000100 x3 : 00000000000000fd
[ 8.409349] x2 : 00000000ffffffff x1 : ffff800012000003 x0 : ffff800012000000
[ 8.416468] Call trace:
[ 8.418903] rproc_handle_resources.constprop.0+0x94/0x168
[ 8.424379] rproc_boot+0x450/0x570
[ 8.427856] rproc_add+0xcc/0x16c
[ 8.431157] k3_r5_probe+0x624/0xdc0 [ti_k3_r5_remoteproc]
[ 8.436640] platform_probe+0x68/0xe0
[ 8.440290] really_probe+0xbc/0x2dc
[ 8.443855] __driver_probe_device+0x78/0x114
[ 8.448197] driver_probe_device+0xd8/0x15c
[ 8.452367] __driver_attach+0x94/0x19c
[ 8.456189] bus_for_each_dev+0x74/0xd4
[ 8.460011] driver_attach+0x24/0x30
[ 8.463573] bus_add_driver+0x154/0x20c
[ 8.467396] driver_register+0x78/0x130
[ 8.471220] __platform_driver_register+0x28/0x34
[ 8.475908] k3_r5_rproc_driver_init+0x20/0x1000 [ti_k3_r5_remoteproc]
[ 8.482422] do_one_initcall+0x54/0x1d0
[ 8.486245] do_init_module+0x48/0x1d0
[ 8.489982] load_module+0x18f4/0x1c80
[ 8.493718] __do_sys_finit_module+0xac/0x104
[ 8.498060] __arm64_sys_finit_module+0x20/0x30
[ 8.502578] invoke_syscall+0x48/0x114
[ 8.506314] el0_svc_common.constprop.0+0xd4/0xfc
[ 8.511003] do_el0_svc+0x20/0x30
[ 8.514305] el0_svc+0x28/0xa0
[ 8.517348] el0t_64_sync_handler+0xbc/0x140
[ 8.521605] el0t_64_sync+0x18c/0x190
[ 8.525255] Code: 128002b3 913fa021 97ffe64f 1400002e (b87a6b20)
[ 8.531330] ---[ end trace 0000000000000000 ]---
[ 8.632905] img_enc 4200000.video-encoder: vxe_enc_probe: using heap 1 for internal alloc
[ OK ] Started D-Bus System Message Bus.
[ 8.678498] img_enc 4200000.video-encoder: encoder registered as /dev/video1
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
Starting DEMO...
[ 8.805822] img_dec 4300000.video-decoder: decoder registered as /dev/video0
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
Starting Update pmic regis�…fety feature on power rails...
Starting Expand the rootfs�…ll size of the boot device....
[ OK ] Started strongSwan IPsec I�…IKEv2 [ 8.947724] audit: type=1334 audit(1651176431.724:4): prog-id=7 op=LOAD
daemon using ipsec.conf.
Starting User Login Management...[ 8.965032] audit: type=1334 audit(1651176431.736:5): prog-id=8 op=LOAD
[ OK ] Started TEE Supplicant.
Starting Telnet Server...
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Finished Telnet Server.
[ OK ] Reached target Preparation for Network.
Starting Network Configuration...
[ OK ] Finished Update pmic regis�…safety feature on power rails.
[ OK ] Started DEMO.
[ 9.238019] j721e-pcie-host 2900000.pcie: PCI host bridge to bus 0000:00
[ 9.289874] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 9.310818] m_can_platform 40528000.can: m_can device registered (irq=816, version=32)
[ 9.326749] m_can_platform 40568000.can: m_can device registered (irq=817, version=32)
[ 9.330363] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[ 9.340787] m_can_platform 2701000.can: m_can device registered (irq=818, version=32)
[ 9.345502] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[ 9.359231] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[ 9.367353] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 9.373949] m_can_platform 2721000.can: m_can device registered (irq=819, version=32)
[ 9.377184] pci 0000:00:00.0: supports D1
[ 9.388896] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 9.394752] pci 0000:00:00.0: reg 0x224: [mem 0x00000000-0x003fffff 64bit]
[ 9.402091] pci 0000:00:00.0: VF(n) BAR0 space: [mem 0x00000000-0x00ffffff 64bit] (contains BAR0 for 4 VFs)
[ 9.442570] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 9.463315] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[ 9.470212] pci 0000:00:00.0: BAR 7: assigned [mem 0x10400000-0x113fffff 64bit]
[ 9.477669] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 9.483427] pcieport 0000:00:00.0: PME: Signaling with IRQ 821
[ 9.489904] pcieport 0000:00:00.0: AER: enabled with IRQ 821
[ 9.495981] j721e-pcie-host 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[ 9.504956] j721e-pcie-host 2910000.pcie: IO 0x0018001000..0x0018010fff -> 0x0018001000
[ 9.513918] j721e-pcie-host 2910000.pcie: MEM 0x0018011000..0x001fffffff -> 0x0018011000
[ 9.525163] j721e-pcie-host 2910000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ OK ] Started Telephony service.
[ OK ] Started User Login Management.
[ 9.958052] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 10.231614] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 10.238496] cfg80211: Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[ 10.418267] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled
[ 10.429842] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c
[ 10.430469] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled
[ 10.446604] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled
[ 10.456996] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled
[ 10.468403] scsi host0: ufshcd
[ 10.484007] remoteproc remoteproc4: b034000.pru is available
[ 10.490016] remoteproc remoteproc5: b004000.rtu is available
[ 10.497109] remoteproc remoteproc6: b00a000.txpru is available
[ 10.503676] remoteproc remoteproc7: b038000.pru is available
[ 10.510986] remoteproc remoteproc8: b006000.rtu is available
[ 10.518330] remoteproc remoteproc9: b00c000.txpru is available
[ 10.524408] scsi 0:0:0:49488: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[ 10.525382] remoteproc remoteproc10: b134000.pru is available
[ 10.539057] remoteproc remoteproc11: b104000.rtu is available
[ 10.545918] scsi 0:0:0:49476: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[ 10.555086] j721e-pcie-host 2910000.pcie: PCI host bridge to bus 0001:00
[ 10.562610] cdns-ufshcd 4e84000.ufs: ufshcd_scsi_add_wlus: BOOT WLUN not found
[ 10.565935] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 10.571220] remoteproc remoteproc12: b10a000.txpru is available
[ 10.575954] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[ 10.582385] remoteproc remoteproc13: b138000.pru is available
[ 10.592166] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[ 10.603819] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400
[ 10.606978] remoteproc remoteproc14: b106000.rtu is available
[ 10.609882] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 10.617669] remoteproc remoteproc15: b10c000.txpru is available
[ 10.625400] pci 0001:00:00.0: supports D1
[ 10.636409] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[ 10.653567] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 10.663590] pci_bus 0001:01: busn_res: [bus 01-ff] end is updated to 01
[ 10.670340] pci 0001:00:00.0: PCI bridge to [bus 01]
[ 10.676700] pcieport 0001:00:00.0: PME: Signaling with IRQ 843
[ 10.687050] pcieport 0001:00:00.0: AER: enabled with IRQ 843
[ 10.695643] j721e-pcie-host 2920000.pcie: host bridge /bus@100000/pcie@2920000 ranges:
[ 10.704832] j721e-pcie-host 2920000.pcie: IO 0x4400001000..0x4400010fff -> 0x0000001000
[ 10.714138] j721e-pcie-host 2920000.pcie: MEM 0x4400011000..0x4407ffffff -> 0x0000011000
[ 10.723153] j721e-pcie-host 2920000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 10.802257] m_can_platform 40528000.can mcu_mcan0: renamed from can0
[ 10.822934] m_can_platform 2701000.can main_mcan0: renamed from can2
[ 10.850096] m_can_platform 40568000.can mcu_mcan1: renamed from can1
[ 10.884893] m_can_platform 2721000.can main_mcan2: renamed from can3
[ 11.031815] Bluetooth: Core ver 2.22
[ 11.035661] NET: Registered PF_BLUETOOTH protocol family
[ 11.041213] Bluetooth: HCI device and connection manager initialized
[ 11.047653] Bluetooth: HCI socket layer initialized
[ 11.052648] Bluetooth: L2CAP socket layer initialized
[ 11.057822] Bluetooth: SCO socket layer initialized
[ OK ] Finished Expand the rootfs�…full size of the boot device..
[ OK ] Listening on Load/Save RF �…itch Status /dev/rfkill Watch.
[ OK ] Started Network Configuration.
Starting Network Name Resolution...
[ 11.248924] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[ 11.258650] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
Starting containerd container runtime...
[ OK ] Started Netperf Benchmark Server.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Simple Network Ma�…ent Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Finished Enable and configure wl18xx bluetooth stack.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Weston, a Wayland�…ositor, as a system service...
[ 11.728702] xhci-hcd xhci-hcd.15.auto: xHCI Host Controller
[ 11.734440] j721e-pcie-host 2920000.pcie: PCI host bridge to bus 0002:00
[ 11.734512] xhci-hcd xhci-hcd.15.auto: new USB bus registered, assigned bus number 1
[ 11.741458] pci_bus 0002:00: root bus resource [bus 00-ff]
[ 11.750746] xhci-hcd xhci-hcd.15.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000018010
[ 11.754416] pci_bus 0002:00: root bus resource [io 0x20000-0x2ffff] (bus address [0x1000-0x10fff])
[ 11.764719] xhci-hcd xhci-hcd.15.auto: irq 853, io mem 0x06410000
[ 11.773170] pci_bus 0002:00: root bus resource [mem 0x4400011000-0x4407ffffff] (bus address [0x00011000-0x07ffffff])
[ 11.779894] xhci-hcd xhci-hcd.15.auto: xHCI Host Controller
[ 11.789573] pci 0002:00:00.0: [104c:b00d] type 01 class 0x060400
[ 11.795807] xhci-hcd xhci-hcd.15.auto: new USB bus registered, assigned bus number 2
[ 11.801304] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 11.809676] xhci-hcd xhci-hcd.15.auto: Host supports USB 3.0 SuperSpeed
[ 11.818989] pci 0002:00:00.0: supports D1
[ 11.825448] hub 1-0:1.0: USB hub found
[ 11.830287] pci 0002:00:00.0: PME# supported from D0 D1 D3hot
[ 11.832961] hub 1-0:1.0: 1 port detected
[ 11.844314] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 11.855650] pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 11.865317] hub 2-0:1.0: USB hub found
[ 11.869616] hub 2-0:1.0: 1 port detected
[ 11.878439] pci_bus 0002:01: busn_res: [bus 01-ff] end is updated to 01
[ 11.886767] pci 0002:00:00.0: PCI bridge to [bus 01]
[ 11.892264] pcieport 0002:00:00.0: PME: Signaling with IRQ 857
[ 11.902614] pcieport 0002:00:00.0: AER: enabled with IRQ 857
Starting Save/Restore Sound Card State...
[ 12.097543] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ OK ] Finished Save/Restore Sound Card State.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Created slice Slice /system/systemd-fsck.
[ OK ] Reached target Sound Card.
[ OK ] Found device /dev/mmcblk0p1.
[ 12.258392] hub 1-1:1.0: USB hub found
[ 12.262288] hub 1-1:1.0: 4 ports detected
Starting File System Check on /dev/mmcblk0p1...
[ OK ] Finished Synchronize System and HW clocks.
[ 12.474906] audit: type=1334 audit(1651176435.252:6): prog-id=9 op=LOAD
[ 12.483090] audit: type=1334 audit(1651176435.260:7): prog-id=10 op=LOAD
Starting User Database Manager...
[ OK ] Started User Database Manager.
[ OK ] Finished File System Check on /dev/mmcblk0p1.
[ OK ] Created slice User Slice of UID 1000.
Mounting /run/media/rootfs-mmcblk0p1...
Starting User Runtime Directory /run/user/1000...
[ 12.860420] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Quota mode: none.
[ OK ] Mounted /run/media/rootfs-mmcblk0p1.
[ OK ] Finished User Runtime Directory /run/user/1000.
Starting User Manager for UID 1000...
[ 13.066514] audit: type=1006 audit(1651176435.844:8): pid=748 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
[ 13.079849] audit: type=1300 audit(1651176435.844:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffff773518 a2=4 a3=ffffb7d9f020 items=0)
[ 13.107262] audit: type=1327 audit(1651176435.844:8): proctitle="(systemd)"
[ OK ] Started User Manager for UID 1000.
[ OK ] Started Session c1 of User weston 14.230664] audit: type=1006 audit(1651176437.008:9): pid=690 uid=0 old-auid=4294967295 auid=1000 tty=tty71
0m.
[ 14.244655] audit: type=1300 audit(1651176437.008:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffff773518 a2=4 a3=ffffb7d9f020 items=0)
[ 14.271040] audit: type=1327 audit(1651176437.008:9): proctitle="(weston)"
[ OK ] Found device /dev/mmcblk1p1.
Starting File System Check on /dev/mmcblk1p1...
[FAILED] Failed to start Weston, a �…mpositor, as a system service.
See 'systemctl status weston.service' for details.
[ OK ] Finished File System Check on /dev/[ 15.370575] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
mmcblk1p1.
[ 15.381323] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Mounting /run/media/BOOT-mmcblk1p1...
[ OK ] Mounted /run/media/BOOT-mmcblk1p1.
[ OK ] Started Simple Network Man�…ement Protocol (SNMP) Daemon..
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project j721e-evm -
Arago 2023.10 j721e-evm -
j721e-evm login: ***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
adwaita-icon-theme-symbolic
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gnu-config
grub-common
grub-editenv
grub-efi
gzip
hidapi
less
libasm1
libatomic-dev
libatomic1
libbfd
libdebuginfod1
libdw1
libeigen-dev
libelf1
libgcc-s-dev
libgcc1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmpc3
libmpfr6
libopcodes
libqt5charts-examples
libqt5charts-plugins
libqt5charts-qmlplugins
libqt5charts5
libqt5sensors-plugins
libqt5sensors-qmlplugins
libqt5sensors5
libqt5serialport-examples
libqt5serialport-plugins
libqt5serialport-qmlplugins
libqt5serialport5
libqt5svg-examples
libqt5svg-plugins
libqt5svg-qmlplugins
libqt5svg5
libqt5virtualkeyboard-plugins
libqt5virtualkeyboard-qmlplugins
libqt5virtualkeyboard5
libqt5webchannel-plugins
libqt5webchannel-qmlplugins
libqt5webchannel5
libreadline-dev
libreadline8
libstdc++-dev
libstdc++6
libunistring2
m4-dev
m4
make
nettle
parted
piglit
qt3d-plugins
qt3d-qmlplugins
qt3d
qtbase-examples
qtbase-plugins
qtbase-qmlplugins
qtbase
qtconnectivity-plugins
qtconnectivity-qmlplugins
qtconnectivity
qtdeclarative-plugins
qtdeclarative-qmlplugins
qtdeclarative-tools
qtdeclarative
qtgraphicaleffects-qmlplugins
qtlocation-examples
qtlocation-plugins
qtlocation-qmlplugins
qtlocation
qtmultimedia-examples
qtmultimedia-plugins
qtmultimedia-qmlplugins
qtmultimedia
qtquics-qmlplugins.control
qtquics2-plugins.control
qtquics2-qmlplugins.control
qtquics2.control
qtscript-examples
qtscript-plugins
qtscript-qmlplugins
qtscript
qtwayland-examples
qtwayland-plugins
qtwayland-qmlplugins
qtwayland
tar
which
If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ 22.378219] platform connector: deferred probe pending
[ 22.383369] platform regulator-dp-pwr: deferred probe pending
[ 22.389106] platform main-r5fss-cpsw9g-virt-mac1: deferred probe pending
[ 22.395799] platform main-r5fss-cpsw9g-virt-mac0: deferred probe pendin