Other Parts Discussed in Thread: TDA4VH
Tool/software:
Hi TI experts,
We are using tda4vh SDK0900 linux native driver to test EST. The network topology is as follows:
The config of TDA4vh:
We tested EST with iperf3, we configured EST on top of interface eth0, which is a gigabit network port. We have priority 0 to 6 in EST in a 40us time slice and priority 7 in another time slice of 40us. So we think the rate of udp testing through iperf3 should be about 500M, but after our actual testing, the packet rate of priority 6 and priority 7 is about 300M only.
We found a lot of packet loss on the eth0 interface.
Why is the rate of priority 7 packets not half the rate of the gigabit port after the time slice is split equally on the gigabit port eth0?
Best Regards,
Ruijie