Does the new display driver support 1280x1024 resolution? If cann't , how to modify the driver?
Please help me, thank you very much!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does DVO2 supports 1024x768 or 640x480 ? If It can, what params cant make it work?
the following is found in VPSS_Video_Driver_UserGuide.pdf:
Switching fb0(graphics0) output from HDMI VEVC(display0) to DVO2 VENC(display1)
Follow the steps below to switch graphics0(fb0)output from HDMI to DVO2 VENC
• Disable graphics 0
#echo 0 > /sys/devices/platform/vpss/graphics0/enabled
• Switch output VENC
# echo 1:dvo2 > /sys/devices/platform/vpss/graphics0/nodes
• Enable graphics 0
#echo 1 > /sys/devices/platform/vpss/graphics0/enabled
echo 720p-60 > /sys/devices/platform/vpss/display0/mode
when I input : echo 1024x768 > /sys/devices/platform/vpss/display0/mode, it say not support param.
Can anyone help me? Thanks!
We do support 1280x1024 on DVO2 output.
display0 is for on-chip HDMI, since you are using DVO2, so it should be display1, please follow below steps:
echo 0 > /sys/devices/platform/vpss/display1/enabled
echo 1280x1024@60 > /sys/devices/platform/vpss/display1/mode
echo 1 > /sys/devices/platform/vpss/display1/enabled
Regards,
yihe
1024x768 is not one of the enumerated formats but you can specify specific timing parameters explicitly.
Have a look at http://ap-fpdsp-swapps.dal.design.ti.com/index.php/DM816X_C6A816X_AM389X_VPSS_Video_Driver_User_Guide_PSP_04.00.00.12 and search for "timings" for more details.
Basically, replace"echo 1024x768 > /sys/devices/platform/vpss/display0/mode" with "echo 65000,1024/24/160/136,768/3/29/6,1 > /sys/devices/platform/vpss/display0/timings"
These numbers come from the VESA specification for 1024x768@60.
BR,
Steve
Hi,
Its supported in TI816X-LINUX-PSP-04.00.01.13 PSP release. You need to do it using timing sysfs entry rather than mode. Further since XGA is a VESA resolution, protocol will be DVI instead of HDMI. Many TVs many not support XGA resolution. Try connecting it to monitor instead of TV
Regards,
Hardik Shah