Part Number: PROCESSOR-SDK-AM62X
Other Parts Discussed in Thread: SK-AM62B-P1
Tool/software:
Dear Support Team,
The SDK we use is processor_sdk_09_02_01_09, our company has customized the core board and base board based on AM6254, the hardware connection is as follows, one CPSW port ETH0 is connected to PC 1 (e.g. laptop), and the other CPSW port ETH1 is connected to PC 2 (e.g. laptop). Now we want to use CPSW's SWITCH mode, but we have a problem where the board can't ping PC1 and PC2. I collected some log information (am62x log.txt) and CPSW related device tree configuration (cpsw dts.txt). I've been researching for over a week and can't find what the problem is, can you help me see what's wrong? Thank you!
&cpsw3g {
pinctrl-names = "default";
pinctrl-0 = <&main_rgmii1_pins_default &main_rgmii2_pins_default>;
cpts@3d000 {
/* MAP HW3_TS_PUSH to GENF1 */
ti,pps = <2 1>;
};
};
&cpsw_port2 {
phy-mode = "rgmii-rxid";
phy-handle = <&cpsw3g_phy1>;
};
&cpsw3g_mdio {
reset-gpios = <&mcu_gpio0 1 GPIO_ACTIVE_LOW &mcu_gpio0 3 GPIO_ACTIVE_LOW>;
reset-delay-us = <100>; /* set reset hold time to 100us */
cpsw3g_phy1: ethernet-phy@1 {
reg = <1>;
ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
ti,min-output-impedance;
};
};
# our cpsw switch mode init script
root@AM62x-Tronlong:~# cat init_cpsw_switch_mode.sh
#!/bin/sh
ip link set dev eth0 down
ip link set dev eth1 down
devlink dev param set platform/8000000.ethernet name switch_mode value true cmode runtime
echo 1 > /sys/kernel/debug/8000000.ethernet/Port1/cut_thru_rx_pri_mask
echo 1 > /sys/kernel/debug/8000000.ethernet/Port1/cut_thru_tx_pri_mask
echo 1 > /sys/kernel/debug/8000000.ethernet/Port2/cut_thru_rx_pri_mask
echo 1 > /sys/kernel/debug/8000000.ethernet/Port2/cut_thru_tx_pri_mask
ethtool --set-priv-flags eth0 cut-thru on
ethtool --set-priv-flags eth1 cut-thru on
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth0 up
sleep 5
ip link set dev eth1 up
sleep 5
ip link set dev eth0 master br0
ip link set dev eth1 master br0
ip link set dev br0 type bridge stp_state 1
ip link set dev br0 up
ip addr add 192.168.1.2/24 dev br0
bridge vlan add dev br0 vid 1 pvid untagged self
# run the init_cpsw_switch_mode.sh
root@AM62x-Tronlong:~# ./init_cpsw_switch_mode.sh
[ 27.618499] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
[ 27.638395] am65-cpsw-nuss 8000000.ethernet eth1: Link is Down
[ 27.852007] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 28.063159] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [YT8521SH Gigabit Ethernet] (irq=POLL)
[ 28.063192] am65-cpsw-nuss 8000000.ethernet: Init cut_thru
[ 28.063202] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[ 31.143589] am65-cpsw-nuss 8000000.ethernet: Port1: Enable cut_thru rx:00000001 tx:00000001 hwspeed:3 (00000101)
[ 31.143649] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 31.143715] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 33.106962] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [TI DP83867] (irq=POLL)
[ 33.106989] am65-cpsw-nuss 8000000.ethernet: Init cut_thru
[ 33.106999] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
[ 37.191631] am65-cpsw-nuss 8000000.ethernet: Port2: Enable cut_thru rx:00000001 tx:00000001 hwspeed:3 (00000101)
[ 37.191685] am65-cpsw-nuss 8000000.ethernet eth1: Link is Up - 1Gbps/Full - flow control rx/tx
[ 37.191744] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
[ 38.125196] br0: port 1(eth0) entered blocking state
[ 38.125241] br0: port 1(eth0) entered disabled state
[ 38.132580] device eth0 entered promiscuous mode
[ 38.136980] kauditd_printk_skb: 3 callbacks suppressed
[ 38.137009] audit: type=1700 audit(1722328862.992:13): dev=eth0 prom=256 old_prom=0 auid=4294967295 uid=0 gid=0 ses=4294967295
[ 38.137683] audit: type=1300 audit(1722328862.992:13): arch=c00000b7 syscall=211 success=yes exit=40 a0=3 a1=ffffe7166408 a2=0 a3=ffffaa8f5840 items=0 ppid=1369 pid=1412 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=ttyS2 ses=4294967295 comm="ip" exe="/sbin/ip.iproute2" key=(null)
[ 38.137703] audit: type=1327 audit(1722328862.992:13): proctitle=6970006C696E6B00736574006465760065746830006D617374657200627230
[ 38.144927] br0: port 2(eth1) entered blocking state
[ 38.144987] br0: port 2(eth1) entered disabled state
[ 38.149660] device eth1 entered promiscuous mode
[ 38.149735] audit: type=1700 audit(1722328863.012:14): dev=eth1 prom=256 old_prom=0 auid=4294967295 uid=0 gid=0 ses=4294967295
[ 38.150458] audit: type=1300 audit(1722328863.012:14): arch=c00000b7 syscall=211 success=yes exit=40 a0=3 a1=ffffdaf8d228 a2=0 a3=ffffbb394840 items=0 ppid=1369 pid=1413 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=ttyS2 ses=4294967295 comm="ip" exe="/sbin/ip.iproute2" key=(null)
[ 38.150511] audit: type=1327 audit(1722328863.012:14): proctitle=6970006C696E6B00736574006465760065746831006D617374657200627230
[ 38.330644] br0: port 2(eth1) entered blocking state
[ 38.330913] br0: port 1(eth0) entered blocking state
root@AM62x-Tronlong:~# [ 39.356621] br0: port 1(eth0) entered blocking state
[ 39.357562] br0: port 2(eth1) entered blocking state
root@AM62x-Tronlong:~# [ 42.324726] br0: port 1(eth0) entered learning state
[ 42.324999] br0: port 1(eth0) entered forwarding state
[ 42.325103] br0: port 2(eth1) entered learning state
[ 42.325176] br0: port 2(eth1) entered forwarding state
[ 42.325665] IPv6: ADDRCONF(NETDEV_CHANGE): br0: link becomes ready
root@AM62x-Tronlong:~# ifconfig -a
br0 Link encap:Ethernet HWaddr E2:88:D4:3A:74:9E
inet addr:192.168.1.2 Bcast:0.0.0.0 Mask:255.255.255.0
inet6 addr: fe80::e088:d4ff:fe3a:749e/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:36 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:4574 (4.4 KiB)
eth0 Link encap:Ethernet HWaddr 28:B5:E8:DE:E7:93
inet6 addr: fe80::2ab5:e8ff:fede:e793/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:36 errors:0 dropped:0 overruns:0 frame:0
TX packets:168 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:4219 (4.1 KiB) TX bytes:17780 (17.3 KiB)
eth1 Link encap:Ethernet HWaddr 28:B5:E8:DE:E7:94
inet6 addr: fe80::2ab5:e8ff:fede:e794/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:40 errors:0 dropped:0 overruns:0 frame:0
TX packets:163 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:4061 (3.9 KiB) TX bytes:17258 (16.8 KiB)
eth2 Link encap:Ethernet HWaddr A2:4A:20:65:0D:EC
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:92 errors:0 dropped:0 overruns:0 frame:0
TX packets:92 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:7678 (7.4 KiB) TX bytes:7678 (7.4 KiB)
main_mcan0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:227
mcu_mcan0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
mcu_mcan1 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@AM62x-Tronlong:~# netstat -nr
Kernel IP routing table
Destination Gateway Genmask Flags MSS Window irtt Iface
192.168.1.0 0.0.0.0 255.255.255.0 U 0 0 0 br0
root@AM62x-Tronlong:~# ethtool -S eth0
NIC statistics:
p0_rx_good_frames: 531
p0_rx_broadcast_frames: 28
p0_rx_multicast_frames: 503
p0_rx_crc_errors: 0
p0_rx_oversized_frames: 0
p0_rx_undersized_frames: 0
p0_ale_drop: 0
p0_ale_overrun_drop: 0
p0_rx_octets: 51986
p0_tx_good_frames: 76
p0_tx_broadcast_frames: 54
p0_tx_multicast_frames: 22
p0_tx_octets: 8584
p0_tx_64B_frames: 372
p0_tx_65_to_127B_frames: 141
p0_tx_128_to_255B_frames: 63
p0_tx_256_to_511B_frames: 31
p0_tx_512_to_1023B_frames: 0
p0_tx_1024B_frames: 0
p0_net_octets: 60570
p0_rx_bottom_fifo_drop: 0
p0_rx_port_mask_drop: 0
p0_rx_top_fifo_drop: 0
p0_ale_rate_limit_drop: 0
p0_ale_vid_ingress_drop: 23
p0_ale_da_eq_sa_drop: 0
p0_ale_block_drop: 0
p0_ale_secure_drop: 0
p0_ale_auth_drop: 0
p0_ale_unknown_ucast: 0
p0_ale_unknown_ucast_bytes: 0
p0_ale_unknown_mcast: 74
p0_ale_unknown_mcast_bytes: 9608
p0_ale_unknown_bcast: 0
p0_ale_unknown_bcast_bytes: 0
p0_ale_pol_match: 0
p0_ale_pol_match_red: 0
p0_ale_pol_match_yellow: 0
p0_ale_mcast_sa_drop: 0
p0_ale_dual_vlan_drop: 0
p0_ale_len_err_drop: 0
p0_ale_ip_next_hdr_drop: 0
p0_ale_ipv4_frag_drop: 0
p0_tx_mem_protect_err: 0
p0_tx_pri0: 76
p0_tx_pri1: 0
p0_tx_pri2: 0
p0_tx_pri3: 0
p0_tx_pri4: 0
p0_tx_pri5: 0
p0_tx_pri6: 0
p0_tx_pri7: 0
p0_tx_pri0_bcnt: 8584
p0_tx_pri1_bcnt: 0
p0_tx_pri2_bcnt: 0
p0_tx_pri3_bcnt: 0
p0_tx_pri4_bcnt: 0
p0_tx_pri5_bcnt: 0
p0_tx_pri6_bcnt: 0
p0_tx_pri7_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri1_drop: 0
p0_tx_pri2_drop: 0
p0_tx_pri3_drop: 0
p0_tx_pri4_drop: 0
p0_tx_pri5_drop: 0
p0_tx_pri6_drop: 0
p0_tx_pri7_drop: 0
p0_tx_pri0_drop_bcnt: 0
p0_tx_pri1_drop_bcnt: 0
p0_tx_pri2_drop_bcnt: 0
p0_tx_pri3_drop_bcnt: 0
p0_tx_pri4_drop_bcnt: 0
p0_tx_pri5_drop_bcnt: 0
p0_tx_pri6_drop_bcnt: 0
p0_tx_pri7_drop_bcnt: 0
rx_good_frames: 217
rx_broadcast_frames: 53
rx_multicast_frames: 164
rx_pause_frames: 0
rx_crc_errors: 0
rx_align_code_errors: 0
rx_oversized_frames: 0
rx_jabber_frames: 0
rx_undersized_frames: 0
rx_fragments: 0
ale_drop: 168
ale_overrun_drop: 0
rx_octets: 26184
tx_good_frames: 340
tx_broadcast_frames: 86
tx_multicast_frames: 254
tx_pause_frames: 0
tx_deferred_frames: 0
tx_collision_frames: 31
tx_single_coll_frames: 0
tx_mult_coll_frames: 7
tx_excessive_collisions: 0
tx_late_collisions: 0
rx_ipg_error: 0
tx_carrier_sense_errors: 0
tx_octets: 34267
tx_64B_frames: 253
tx_65_to_127B_frames: 201
tx_128_to_255B_frames: 77
tx_256_to_511B_frames: 26
tx_512_to_1023B_frames: 0
tx_1024B_frames: 0
net_octets: 60451
rx_bottom_fifo_drop: 0
rx_port_mask_drop: 168
rx_top_fifo_drop: 0
ale_rate_limit_drop: 0
ale_vid_ingress_drop: 64
ale_da_eq_sa_drop: 0
ale_block_drop: 0
ale_secure_drop: 0
ale_auth_drop: 0
ale_unknown_ucast: 0
ale_unknown_ucast_bytes: 0
ale_unknown_mcast: 123
ale_unknown_mcast_bytes: 13013
ale_unknown_bcast: 40
ale_unknown_bcast_bytes: 5548
ale_pol_match: 0
ale_pol_match_red: 0
ale_pol_match_yellow: 0
ale_mcast_sa_drop: 0
ale_dual_vlan_drop: 0
ale_len_err_drop: 0
ale_ip_next_hdr_drop: 0
ale_ipv4_frag_drop: 0
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 0
tx_mem_protect_err: 0
tx_pri0: 340
tx_pri1: 0
tx_pri2: 0
tx_pri3: 0
tx_pri4: 0
tx_pri5: 0
tx_pri6: 0
tx_pri7: 0
tx_pri0_bcnt: 34191
tx_pri1_bcnt: 0
tx_pri2_bcnt: 0
tx_pri3_bcnt: 0
tx_pri4_bcnt: 0
tx_pri5_bcnt: 0
tx_pri6_bcnt: 0
tx_pri7_bcnt: 0
tx_pri0_drop: 0
tx_pri1_drop: 0
tx_pri2_drop: 0
tx_pri3_drop: 0
tx_pri4_drop: 0
tx_pri5_drop: 0
tx_pri6_drop: 0
tx_pri7_drop: 0
tx_pri0_drop_bcnt: 0
tx_pri1_drop_bcnt: 0
tx_pri2_drop_bcnt: 0
tx_pri3_drop_bcnt: 0
tx_pri4_drop_bcnt: 0
tx_pri5_drop_bcnt: 0
tx_pri6_drop_bcnt: 0
tx_pri7_drop_bcnt: 0
root@AM62x-Tronlong:~# ethtool -S eth1
NIC statistics:
p0_rx_good_frames: 533
p0_rx_broadcast_frames: 28
p0_rx_multicast_frames: 505
p0_rx_crc_errors: 0
p0_rx_oversized_frames: 0
p0_rx_undersized_frames: 0
p0_ale_drop: 0
p0_ale_overrun_drop: 0
p0_rx_octets: 52114
p0_tx_good_frames: 76
p0_tx_broadcast_frames: 54
p0_tx_multicast_frames: 22
p0_tx_octets: 8584
p0_tx_64B_frames: 374
p0_tx_65_to_127B_frames: 141
p0_tx_128_to_255B_frames: 63
p0_tx_256_to_511B_frames: 31
p0_tx_512_to_1023B_frames: 0
p0_tx_1024B_frames: 0
p0_net_octets: 60698
p0_rx_bottom_fifo_drop: 0
p0_rx_port_mask_drop: 0
p0_rx_top_fifo_drop: 0
p0_ale_rate_limit_drop: 0
p0_ale_vid_ingress_drop: 23
p0_ale_da_eq_sa_drop: 0
p0_ale_block_drop: 0
p0_ale_secure_drop: 0
p0_ale_auth_drop: 0
p0_ale_unknown_ucast: 0
p0_ale_unknown_ucast_bytes: 0
p0_ale_unknown_mcast: 74
p0_ale_unknown_mcast_bytes: 9608
p0_ale_unknown_bcast: 0
p0_ale_unknown_bcast_bytes: 0
p0_ale_pol_match: 0
p0_ale_pol_match_red: 0
p0_ale_pol_match_yellow: 0
p0_ale_mcast_sa_drop: 0
p0_ale_dual_vlan_drop: 0
p0_ale_len_err_drop: 0
p0_ale_ip_next_hdr_drop: 0
p0_ale_ipv4_frag_drop: 0
p0_tx_mem_protect_err: 0
p0_tx_pri0: 76
p0_tx_pri1: 0
p0_tx_pri2: 0
p0_tx_pri3: 0
p0_tx_pri4: 0
p0_tx_pri5: 0
p0_tx_pri6: 0
p0_tx_pri7: 0
p0_tx_pri0_bcnt: 8584
p0_tx_pri1_bcnt: 0
p0_tx_pri2_bcnt: 0
p0_tx_pri3_bcnt: 0
p0_tx_pri4_bcnt: 0
p0_tx_pri5_bcnt: 0
p0_tx_pri6_bcnt: 0
p0_tx_pri7_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri1_drop: 0
p0_tx_pri2_drop: 0
p0_tx_pri3_drop: 0
p0_tx_pri4_drop: 0
p0_tx_pri5_drop: 0
p0_tx_pri6_drop: 0
p0_tx_pri7_drop: 0
p0_tx_pri0_drop_bcnt: 0
p0_tx_pri1_drop_bcnt: 0
p0_tx_pri2_drop_bcnt: 0
p0_tx_pri3_drop_bcnt: 0
p0_tx_pri4_drop_bcnt: 0
p0_tx_pri5_drop_bcnt: 0
p0_tx_pri6_drop_bcnt: 0
p0_tx_pri7_drop_bcnt: 0
rx_good_frames: 233
rx_broadcast_frames: 118
rx_multicast_frames: 115
rx_pause_frames: 0
rx_crc_errors: 0
rx_align_code_errors: 0
rx_oversized_frames: 0
rx_jabber_frames: 0
rx_undersized_frames: 0
rx_fragments: 0
ale_drop: 121
ale_overrun_drop: 0
rx_octets: 27513
tx_good_frames: 277
tx_broadcast_frames: 27
tx_multicast_frames: 250
tx_pause_frames: 0
tx_deferred_frames: 0
tx_collision_frames: 7
tx_single_coll_frames: 0
tx_mult_coll_frames: 31
tx_excessive_collisions: 0
tx_late_collisions: 0
rx_ipg_error: 0
tx_carrier_sense_errors: 0
tx_octets: 28701
tx_64B_frames: 256
tx_65_to_127B_frames: 130
tx_128_to_255B_frames: 104
tx_256_to_511B_frames: 20
tx_512_to_1023B_frames: 0
tx_1024B_frames: 0
net_octets: 56214
rx_bottom_fifo_drop: 0
rx_port_mask_drop: 121
rx_top_fifo_drop: 0
ale_rate_limit_drop: 0
ale_vid_ingress_drop: 6
ale_da_eq_sa_drop: 0
ale_block_drop: 0
ale_secure_drop: 0
ale_auth_drop: 0
ale_unknown_ucast: 0
ale_unknown_ucast_bytes: 0
ale_unknown_mcast: 92
ale_unknown_mcast_bytes: 10623
ale_unknown_bcast: 47
ale_unknown_bcast_bytes: 4611
ale_pol_match: 0
ale_pol_match_red: 0
ale_pol_match_yellow: 0
ale_mcast_sa_drop: 0
ale_dual_vlan_drop: 0
ale_len_err_drop: 0
ale_ip_next_hdr_drop: 0
ale_ipv4_frag_drop: 0
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 0
tx_mem_protect_err: 0
tx_pri0: 277
tx_pri1: 0
tx_pri2: 0
tx_pri3: 0
tx_pri4: 0
tx_pri5: 0
tx_pri6: 0
tx_pri7: 0
tx_pri0_bcnt: 28685
tx_pri1_bcnt: 0
tx_pri2_bcnt: 0
tx_pri3_bcnt: 0
tx_pri4_bcnt: 0
tx_pri5_bcnt: 0
tx_pri6_bcnt: 0
tx_pri7_bcnt: 0
tx_pri0_drop: 0
tx_pri1_drop: 0
tx_pri2_drop: 0
tx_pri3_drop: 0
tx_pri4_drop: 0
tx_pri5_drop: 0
tx_pri6_drop: 0
tx_pri7_drop: 0
tx_pri0_drop_bcnt: 0
tx_pri1_drop_bcnt: 0
tx_pri2_drop_bcnt: 0
tx_pri3_drop_bcnt: 0
tx_pri4_drop_bcnt: 0
tx_pri5_drop_bcnt: 0
tx_pri6_drop_bcnt: 0
tx_pri7_drop_bcnt: 0
root@AM62x-Tronlong:~# brctl show
bridge name bridge id STP enabled interfaces
br0 8000.e288d43a749e yes eth0
eth1
root@AM62x-Tronlong:~# brctl showmacs br0
port no mac addr is local? ageing timer
1 28:b5:e8:de:e7:93 yes 0.00
1 28:b5:e8:de:e7:93 yes 0.00
2 28:b5:e8:de:e7:94 yes 0.00
2 28:b5:e8:de:e7:94 yes 0.00