This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62X: Compile debian system, update image source Connection timed out

Part Number: PROCESSOR-SDK-AM62X

Tool/software:

I could not compile debian on 09.02.01.010.
compile command:sudo ./build.sh am62-bookworm-09.02.01.010
View the am62-bookworm-09.02.01.010.log file and find the following problem
I: running apt-get update...
Get:1 mirrors.aliyun.com/debian bookworm InRelease [151 kB]
Get:2 mirrors.aliyun.com/debian buster InRelease [122 kB]
Get:4 mirrors.aliyun.com/.../contrib arm64 Packages [45.7 kB]
Get:5 mirrors.aliyun.com/.../non-free-firmware arm64 Packages [5832 B]
Get:3 texasinstruments.github.io/ti-debpkgs bookworm InRelease [9695 B]
Get:6 mirrors.aliyun.com/.../main arm64 Packages [8688 kB]
Get:7 texasinstruments.github.io/.../main Sources [2699 B]
Get:8 texasinstruments.github.io/.../non-free arm64 Packages [3778 B]
Get:9 texasinstruments.github.io/.../main arm64 Packages [11.8 kB]
Get:10 deb.debian.org/debian bookworm InRelease [151 kB]
Get:11 mirrors.aliyun.com/.../main arm64 Packages [7737 kB]
Get:12 deb.debian.org/.../contrib arm64 Packages [45.7 kB]
Get:13 deb.debian.org/.../main arm64 Packages [8688 kB]
Get:14 mirrors.aliyun.com/.../contrib arm64 Packages [38.4 kB]
Get:15 mirrors.aliyun.com/.../non-free arm64 Packages [53.9 kB]
Ign:13 deb.debian.org/.../main arm64 Packages
Ign:16 deb.debian.org/.../non-free-firmware arm64 Packages
Ign:13 deb.debian.org/.../main arm64 Packages
Ign:16 deb.debian.org/.../non-free-firmware arm64 Packages
Ign:13 deb.debian.org/.../main arm64 Packages
Ign:16 deb.debian.org/.../non-free-firmware arm64 Packages
Ign:13 deb.debian.org/.../main arm64 Packages
Ign:13 deb.debian.org/.../main arm64 Packages
Ign:13 deb.debian.org/.../main arm64 Packages
Ign:13 deb.debian.org/.../main arm64 Packages
Ign:13 deb.debian.org/.../main arm64 Packages
Err:13 deb.debian.org/.../main arm64 Packages
Connection timed out [IP: 151.101.90.132 80]
Fetched 17.1 MB in 3min 12s (89.1 kB/s)
Reading package lists...
W: mirrors.aliyun.com/.../debian-archive-keyring.gpg), see the DEPRECATION section in apt-key(8) for details.
W: mirrors.aliyun.com/.../debian-archive-keyring.gpg), see the DEPRECATION section in apt-key(8) for details.
W: deb.debian.org/.../debian-archive-keyring.gpg), see the DEPRECATION section in apt-key(8) for details.
E: Failed to fetch deb.debian.org/.../Packages  Connection timed out [IP: 151.101.90.132 80]
E: Some index files failed to download. They have been ignored, or old ones used instead.
E: apt-get update --error-on=any -oAPT::Status-Fd=<$fd> -oDpkg::Use-Pty=false failed
W: listening on child socket failed:
E: mmdebstrap failed to run
2024-08-01 13:47:57,886 bdebstrap ERROR: mmdebstrap failed with exit code 25. See above for details.

There's a Connection timed out problem. Why? Is TI officially under maintenance or update?
This didn't happen when I compiled last week, but the Connection timed out problem started yesterday.
I checked the proxy network and it's working.