Other Parts Discussed in Thread: TDA4VM
Tool/software:
This is the configuration description and test results of the Ethernet loopback test using TDA4VM
Development environment:
SDK 9.1(Linux run on A72, MCU2_0 run Ethfw with Freertos and the R5F core binary is from vision app); platform is TDA4VM


Hardware connection
You need to connect port3 and port8 to the two ubuntu PCs that need to communicate



fig1 :port interface definition fig2:Example of a PC-TDA4VM-PC connection fig3: detail of port connection
Run and Test
Start by making sure that the Vision App is correctly install to sd card and that the vision_apps_init.sh is running successfully in TDA4VM
Perform the following steps:
1. Network address settings

fig1: PC1 address

fig 2: TDA4VM eth1(Port 3 &Port 8) address

fig3: PC2 address
2. TDA4VM ping two PC


fig 1: TDA4VM ping PC1 fig 2: TDA4VM ping PC2
3.PC1 ping PC2 through TDA4VM, PC2 ping PC1 through TDA4VM

PC1 ping PC2

PC2 ping PC1