Hi,
I'm using EZSDK 5.02.02.60 and 816x/389x EVM rev F.
When i connect usb mouse and keyboard after booting,
console output messages that indicate usb devices detection.
Then i can use usb mouse, but usb keyboard input doesn't work. I input characters to browser using usb keyboard.
And I found TI wiki topic, http://processors.wiki.ti.com/index.php/EZ_SDK_FAQ .
The topic of "What is supported on Web Browser?" on it says that
" Do not connect the keyboard interface on web browser it will be supported in next release."
Doesn't EZSDK 5.02.02.60 support usb keyboard input ?