Other Parts Discussed in Thread: ADS7846
Hi all,
I have a problem while configuring SPI2. Firstly i know that, HS USB uses SPI2, so I need to close USB, According to this i configured GPMC_NBE1 pin mux as a GPIO in evm.h file. (_U-BootSource_/board/ti/evm/evm.h)
MUX_VAL(CP(GPMC_NBE1), (IDIS | PTU | EN | M4)) /*GPIO_61*/\
Then i added MUX_VAL for SPI2,
MUX_VAL(CP(MCSPI2_CLK), (IEN | PTD | DIS | M0)) /*McSPI2_CLK*/\
MUX_VAL(CP(MCSPI2_SIMO), (IEN | PTD | DIS | M0)) /*McSPI2_SIMO*/\
MUX_VAL(CP(MCSPI2_SOMI), (IEN | PTD | DIS | M0)) /*McSPI2_SOMI*/\
MUX_VAL(CP(MCSPI2_CS0), (IEN | PTD | EN | M0)) /*McSPI2_CS0*/\
MUX_VAL(CP(MCSPI2_CS1), (IEN | PTD | EN | M0)) /*McSPI2_CS1*/\
After saved evm.h, i compiled Uboot like this,
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm distclean
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm omap3_evm_config
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm
After these steps, configured kernel to, i removed all USB configs from omap3_evm_defconfig and configured SPI configs like this,
CONFIG_SPI=y
CONFIG_SPI_MASTER=y
CONFIG_SPI_OMAP24XX=y
CONFIG_SPI_SPIDEV=y
After these added below lines to board-omap3evm.c file (arch/arm/mach-omap2/board-omap3evm.c),
struct spi_board_info omap3evm_spi_board_info[] = {
[0] = {
.modalias = "ads7846",
.bus_num = 1,
.chip_select = 0,
.max_speed_hz = 1500000,
.controller_data = &ads7846_mcspi_config,
.irq = OMAP_GPIO_IRQ(OMAP3_EVM_TS_GPIO),
.platform_data = &ads7846_config,
},
/*A.Caliskan*/
[1] = {
.modalias = "spidev",
.bus_num = 2,
.chip_select = 0,
.max_speed_hz = 1000000,
.mode = SPI_MODE_0,
},
[2] = {
.modalias = "spidev",
.bus_num = 2,
.chip_select = 1,
.max_speed_hz = 24000000,
.mode = SPI_MODE_0,
},
/*A.Caliskan*/
};
After these steps i compiled kernel as below,
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm distclean
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm omap3_evm_defconfig
$ make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm uImage modules
and boot the board with new Uboot and Kernel. After run a SPI test program did not see something on SCK MISO MOSI CS0 pins, Then check the GPMC_NBE1 pin from board with the Voltmeter i see it HIGH. Then configured omap3_evm_init function which in board-omap3evm.c file like these,
/* Select EHCI port on main board */
// omap_mux_init_gpio(61, OMAP_PIN_INPUT_PULLUP);
// gpio_request(OMAP3_EVM_EHCI_SELECT, "select EHCI port");
// gpio_direction_output(OMAP3_EVM_EHCI_SELECT, 0);
// gpio_set_value(OMAP3_EVM_EHCI_SELECT, 0);
/* setup SPI2 config */
omap_mux_init_gpio(61, OMAP_PIN_INPUT_PULLUP);
gpio_request(OMAP3_EVM_SPI2_SELECT, "select SPI2 port");
gpio_direction_output(OMAP3_EVM_SPI2_SELECT, 0);
gpio_set_value(OMAP3_EVM_SPI2_SELECT, 1);
Closed EHCI port and configured GPIO_61 (GPMC_NBE1) pin to LOW, After these changes i compiled the kernel again, and boot, but nothing change...
Where is the problem?
Best regards,
Ahmet