This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VEN-Q1: Please help confirm CSI-2 function

Part Number: TDA4VEN-Q1

Tool/software:

Hi Expert,

TDA4 Entry can support 2x CSI (4L) -> 2.5Gbps RX throughput per lane (20Gbps total)

Could TDA4 Entry handle these 20Gbps signals at the same time?

Customer requirements are as follows (the SoC in the picture is TDA4 Entry)

The signals from the four cameras, which are 8MP cameras, will enter the MAX96724 at the same time, and then the MAX96724 will output the MIPI signal to the SOC.

Thanks

Daniel