This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM C6678 critical issue....

EVM C6678 is connected to PC via USB cable in the static IP mode.
While trying to connect target in the target configuration core files this is what is happening.
I'm using CCS v5.0.3.0023 and the OS is Windows 7 .
The drivers are installed and it is shown correctly in the device manager.
I've run the HUA demo.

 

 

Please reply sooner.