Part Number: PROCESSOR-SDK-AM64X
Tool/software:
Hello!
This is actually a follow-up for this post:
which has been locked for some reason although not solved.
There are additional findings I found worth sharing on that matter.
As it turned out, in the SDK version 09.02.01.10 in junction with the TMDS64GPEVM TFTP/NFS is only working on interface eth0.
On interface eth2 TFTP boot is working via U-Boot, but NFS not (as discussed in the aforementioned thread).
On interface eth1 TFTP boot is not working via U-Boot, hence the system is not coming to the stage where NFS would be needed.
Although I can stably use the TMDS64GPEVM via TFTP/NFS boot now, there is still the question what is the issue
with eth2.
Regards,
Mario