This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can AM1808 output camera video to TFT LCD?

Anonymous
Anonymous
Other Parts Discussed in Thread: AM1808

Hi,

 

I would like to ask a question on AM1808 LCD output.

 

If the application requires outputting video input from camera to TFT LCD screen via AM1808, what is the solution?

 

After reading the datasheet carefully, I found that the video output ability of AM1808 is rather limited. To bridge input with output, the same format sets should be supported both at the front and the end side, like in DM6437. However, unlike digital media processor DM6437 whose VPSS is capable of doing conversion between various formats, including (YUV, RGB) pair, I found no hardware video format conversion ability in AM1808:

 

 

 

VPIF

LCDC TFT mode (BPP=12 or 16, not using pallette)

YUV

RGB

BPP 8, 10, 12

12(supported?) or 16

 

 

 

The only intersection between {VPIF format} and {LCDC format} is 12-bit RGB; however, as asked in Does AM1808 LCDC support 12-bit TFT mode?, the description on TFT output modes was not particularly clear regarding 12-bit mode.

 

Is my understanding on VPIF and LCDC correct? If 12-bit TFT mode is supported, is it the only way to output camera video input on LCD? If 12-bit TFT mode is not supported, does it mean via TFT LCD there is no way to display camera video input?

 

 

 

Zheng

 

  • Zheng,

    Your understanding is correct.

    12-bit TFT is not supported.

    Processing & conversion would have to be done by the ARM.

  • Hi Paul,


    I am using AM1808, and i designed 16-Bit TFT LCD port and CAMERA via VPIF interface.

    Will this support together to capture the image and watching the still while taking the snap in LCD.

    I Would like to know first, AM1808 should support these two options.

    Another point how to take the snap and can convert that to jpeg format.

    Please explain how to develop together.


    Thanks,
    Francis