SOMAM1808 10-1602QHIR-B
MPC Data WinCE 6.0 v1.0, v1.3
TI,
I bought a new AM1808 SOM with 128MB of DDR (above). I installed a correctly built Eboot and it downloads WinCE 6.0 from platform builder. It launches and then immediately reboots into Eboot, redownloads and relaunches. It will do this repeatedly. My 64MB SOM and build works fine (with 64MB patch). The 128MB SOM’s label is:
1017950
REV A
3211MC2033
SOMAM1808
10-1602QHIR-B
According to “PCN 474: Hardware Changes”, this SOM has had a DDR upgrade. I am told by LogicPD that the WinCE bootloader needs to have its DDR ID updated. The Micron DDR part numbers are:
MT46H64M16LFCK-6:A Old
MT46H64M16LFBF-6 IT:B New
Has this update already been done? If not, what is the best way to get this done? I must get this running.
Regards,
Nelson