Part Number: AM3352
Tool/software:
I am using the USB controller as a peripheral, and I need to be able to signal to the host to remote wake up. According to the TRM (revision P) 16.2.8.1 it says that "Initiating a remote wakeup –If the software wants to initiate a remote wakeup while the controller is in Suspend mode, it should set the POWER[RESUME] bit to 1. The software should leave then this bit set for approximately 10 ms (minimum of 2 ms, a maximum of 15 ms) before resetting it to 0." However, this POWER[RESUME} register and bit combination are unknowable.
Can someone explain the proper procedure to make this type of signalllng happen? For reference I am using TI SDK Linux 4.14.40 with the included linux USB drivers.
Much Appreciated,
Brian