This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U-Q1: Serdes support in uboot

Part Number: DRA821U-Q1
Other Parts Discussed in Thread: DRA821

Tool/software:

Hi Team,

We are working on DRA821 CPU with Linux sdk 09.02. we want to test serdes feature in uboot, when we configured serdes in uboot, boot hangs and returns with below mentioned error.

cdns,torrent serdes@5060000: Timeout waiting for CMN ready
cdns,torrent serdes@5060000: PHY: Failed to power on serdes@5060000: -110.
phy_power_on failed!!: -110

So,  is serdes validated in u-boot?. if yes,  any additional changes am i missing

Note: All the dts and board/ti/j721e/evm.c file changes are done properly

Regards,

Nikhil K

  • Hi Nikhil,

    What is your serdes configuration?

    So,  is serdes validated in u-boot?. if yes,  any additional changes am i missing

    By default, for j7200, PCIe and SGMII links are configured in serdes. So yes, some configurations are supported from u-boot. But not all are supported.

    Regards,
    Tanmay

  • Hi Tanmay,

    We want to test USB3.0 in uboot(usb3.0 signals from serdes LANE4).

    This is my dts settings

    &serdes0 {
            status="okay";
            serdes0_usb_link: phy@1 {
                    reg = <3>;
                    cdns,num-lanes = <1>;
                    #phy-cells = <0>;
                    cdns,phy-type = <PHY_TYPE_USB3>;
                    resets = <&serdes_wiz0 4>;
            };
    };

    &usb0 {
            dr_mode = "host";       
            phy-names = "cdns3,usb3-phy";
            phys = <&serdes0_usb_link>;
            status="okay";
    };

    &serdes_ln_ctrl {
            status="okay";
            idle-states = <J7200_SERDES0_LANE0_PCIE1_LANE0>, <J7200_SERDES0_LANE1_PCIE1_LANE1>,
                          <J7200_SERDES0_LANE2_IP4_UNUSED>, <J7200_SERDES0_LANE3_USB>;
    };

    &usb_serdes_mux {
            idle-states = <1>; /* USB0 to SERDES lane 3 */
    };

    in board/ti/j721e/evm.c file im enabling "configure_serdes_torrent()" function, in this function i'm observing while doing phy power on (generic_phy_power_on()) facing the failure as mentioned earlier.

    Seems like this is not related to usb settings, serdes itself not getting activated.

    Note: In kernel we able to test this feature successfully, but i enable serdes in uboot in kernel also im observing same error.

    Regards,

    Nikhil K

  • Hi Nikhil,

    By default serdes on j7200 is used for PCIe+QSGMII. To use USB on the same serdes, you would have to remove one of them, either PCIe or QSGMII. From the looks of it, based on your serdes_lane_ctrl, you have removed QSGMII. But you also have to remove the node in device-tree for QSGMII link. Can you confirm that you have done this?

    Apart from this can you ensure the USB configs are present for u-boot?

    For other devices, USB is tested at u-boot.

    Regards,
    Tanmay

  • Hi Tanmay,

    Thanks for the reply,

    I have removed QSGMII entry from dts.

    Also usb configuration looks fine compared to kernel

    we have tested usb in 2.0 otg mode, that works properly, so the usb configuration are fine it seems.

    But here serdes phy itself not probing...

    Regards,

    Nikhil K

  • Hi Tanmay,

    Is there any update on this case?

    Regards,

    Nikhil K

  • Hi Tanmay,
    Is there any update ?

    Regards,

    Nikhil K

  • Hi Nikhil,

    Sorry for the delay.

    But here serdes phy itself not probing..

    Have you verified this with additional prints in the u-boot?

    Can you share the complete updated device-tree with all the changes.

    Regards,
    Tanmay

  • Have you verified this with additional prints in the u-boot?

    Yes, its failing below mentioned section in serdes driver

            /*
             * Wait for cmn_ready assertion
             * PHY_PMA_CMN_CTRL1[0] == 1
             */
            ret = regmap_field_read_poll_timeout(cdns_phy->phy_pma_cmn_ctrl_1,
                                                 read_val, read_val, 1000,
                                                 PLL_LOCK_TIMEOUT);
            if (ret) {
                    dev_err(cdns_phy->dev, "Timeout waiting for CMN ready\n");
                    return ret;
    }

    Find the dts changes

    // SPDX-License-Identifier: GPL-2.0
    /*
     * Copyright (C) 2020 Texas Instruments Incorporated - https://www.ti.com/
     */
    
    /dts-v1/;
    
    #include "k3-j7200-som-p0.dtsi"
    #include <dt-bindings/gpio/gpio.h>
    #include <dt-bindings/net/ti-dp83867.h>
    #include <dt-bindings/mux/ti-serdes.h>
    #include <dt-bindings/phy/phy.h>
    
    / {
    	chosen {
    		stdout-path = "serial2:115200n8";
    		bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000";
    	};
    
            aliases {
                    i2c0 = &wkup_i2c0;
                    i2c1 = &mcu_i2c0;
            };
    
    	evm_12v0: fixedregulator-evm12v0 {
    		/* main supply */
    		compatible = "regulator-fixed";
    		regulator-name = "evm_12v0";
    		regulator-min-microvolt = <12000000>;
    		regulator-max-microvolt = <12000000>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vsys_3v3: fixedregulator-vsys3v3 {
    		/* Output of LM5140 */
    		compatible = "regulator-fixed";
    		regulator-name = "vsys_3v3";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    		vin-supply = <&evm_12v0>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vsys_5v0: fixedregulator-vsys5v0 {
    		/* Output of LM5140 */
    		compatible = "regulator-fixed";
    		regulator-name = "vsys_5v0";
    		regulator-min-microvolt = <5000000>;
    		regulator-max-microvolt = <5000000>;
    		vin-supply = <&evm_12v0>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vdd_mmc1: fixedregulator-sd {
    		compatible = "regulator-fixed";
    		regulator-name = "vdd_mmc1";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    		regulator-boot-on;
    		enable-active-high;
    		vin-supply = <&vsys_3v3>;
                    pinctrl-names = "default";
                    pinctrl-0 = <&wkup_vdd_mmc1_pins_default>;
                    gpio = <&wkup_gpio0 84 GPIO_ACTIVE_HIGH>;
    	};
    
    	vdd_sd_dv: gpio-regulator-sd-dv {
    		compatible = "regulator-gpio";
    		regulator-name = "vdd_sd_dev";
                    pinctrl-names = "default";
                    pinctrl-0 = <&main_vdd_sd_pins_default>;
                    regulator-min-microvolt = <1800000>;
    		regulator-max-microvolt = <3300000>;
    		regulator-boot-on;
    		vin-supply = <&vsys_5v0>;
    		gpios = <&main_gpio0 55 GPIO_ACTIVE_HIGH>;
    		states = <1800000 0x0>,
    			 <3300000 0x1>;
    	};
    };
    
    &main_gpio0 {
    	status = "okay";
    };
    
    &wkup_pmx0 {
    
            wkup_eth_rst_pins_default: wkup_eth_rst_default_pins {
                    pinctrl-single,pins = <
                            J721E_WKUP_IOPAD(0x24, PIN_OUTPUT_PULLUP, 7) /* (A8) MCU_OSPI0_D6.WKUP_GPIO0_25 */
                    >;
            };
    };
    
    &wkup_pmx2 {
            status = "okay";
    
            mcu_i2c0_pins_default: mcu-i2c0-default-pins {
                  pinctrl-single,pins = <
                            J721E_WKUP_IOPAD(0x0A0, PIN_INPUT_PULLUP, 0) /* (G21) MCU_I2C0_SCL */
                            J721E_WKUP_IOPAD(0x0A4, PIN_INPUT_PULLUP, 0) /* (G20) MCU_I2C0_SDA */
                    >;
            };
    };
    
    &wkup_pmx3 {
            status = "okay";
    
            wkup_vdd_mmc1_pins_default: wkup-vdd-mmc1-pins-default {
                    pinctrl-single,pins = <
                            J721E_WKUP_IOPAD(0x1C, PIN_OUTPUT, 7) /* (E18) WKUP_GPIO0_84 */
                    >;
            };
    };
    
    &main_pmx0 {
            status = "okay";
    
            main_vdd_sd_pins_default: main-vdd-sd-pins-default {
                    pinctrl-single,pins = <
                            J721E_IOPAD(0x18, PIN_OUTPUT, 7) /* (V17) RMII1_TX_EN.GPIO0_7 */
    			/*J721E_IOPAD(0xd0, PIN_OUTPUT, 7) /* (T5) SPI0_D1.GPIO0_55 */
                    >;
            };
    	main_mmc1_pins_default: main-mmc1-pins-default {
    		pinctrl-single,pins = <
    			J721E_IOPAD(0x104, PIN_INPUT, 0) /* (M20) MMC1_CMD */
    			J721E_IOPAD(0x100, PIN_INPUT, 0) /* (P21) MMC1_CLK */
    			J721E_IOPAD(0xfc, PIN_INPUT, 0) /* (P25) MMC1_CLKLB */
    			J721E_IOPAD(0xf8, PIN_INPUT, 0) /* (M19) MMC1_DAT0 */
    			J721E_IOPAD(0xf4, PIN_INPUT, 0) /* (N21) MMC1_DAT1 */
    			J721E_IOPAD(0xf0, PIN_INPUT, 0) /* (N20) MMC1_DAT2 */
    			J721E_IOPAD(0xec, PIN_INPUT, 0) /* (N19) MMC1_DAT3 */
    			J721E_IOPAD(0xe4, PIN_INPUT, 8) /* (V1) TIMER_IO0.MMC1_SDCD */
    		>;
    	};
    	
    	main_usbss0_pins_default: main-usbss0-pins-default {
    		pinctrl-single,pins = <
    			J721E_IOPAD(0x120, PIN_OUTPUT, 0) /* (T4) USB0_DRVVBUS */
    		>;
    	};
    };
    
    &wkup_uart0 {
    	/* Wakeup UART is used by System firmware */
    	status = "reserved";
    };
    
    &main_uart0 {
    	/* Shared with ATF on this platform */
    	power-domains = <&k3_pds 146 TI_SCI_PD_SHARED>;
    };
    
    &main_uart2 {
    	/* MAIN UART 2 is used by R5F firmware */
    	status = "reserved";
    };
    
    &main_uart3 {
    	/* UART not brought out */
    	status = "disabled";
    };
    
    &main_uart4 {
    	/* UART not brought out */
    	status = "disabled";
    };
    
    &main_uart5 {
    	/* UART not brought out */
    	status = "disabled";
    };
    
    &main_uart6 {
    	/* UART not brought out */
    	status = "disabled";
    };
    
    &main_uart7 {
    	/* UART not brought out */
    	status = "disabled";
    };
    
    &main_uart8 {
    	/* UART not brought out */
    	status = "disabled";
    };
    
    &main_uart9 {
    	/* UART not brought out */
    	status = "disabled";
    };
    
    &main_gpio0 {
            status = "okay";
    };
    
    &main_gpio2 {
    	status = "disabled";
    };
    
    &main_gpio4 {
    	status = "disabled";
    };
    
    &main_gpio6 {
    	status = "disabled";
    };
    
    &wkup_gpio0 {
            status = "okay";
    };
    
    &wkup_gpio1 {
    	status = "disabled";
    };
    
    &main_sdhci0 {
    	/* eMMC */
    	non-removable;
    	ti,driver-strength-ohm = <50>;
    	disable-wp;
    	status="okay";
    };
    
    &main_sdhci1 {
    	pinctrl-0 = <&main_mmc1_pins_default>;
    	pinctrl-names = "default";
    	vmmc-supply = <&vdd_mmc1>;
    	vqmmc-supply = <&vdd_sd_dv>;
    	ti,driver-strength-ohm = <50>;
    	disable-wp;
    	status="okay";
    };
    
    &serdes_ln_ctrl {
    	status="okay";
    	idle-states = <J7200_SERDES0_LANE0_PCIE1_LANE0>, <J7200_SERDES0_LANE1_PCIE1_LANE1>,
    		      <J7200_SERDES0_LANE2_IP4_UNUSED>, <J7200_SERDES0_LANE3_USB>;
    };
    
    &usb_serdes_mux {
    	idle-states = <1>; /* USB0 to SERDES lane 3 */
    };
    
    &usbss0 {
    
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_usbss0_pins_default>;
    	ti,vbus-divider;
    };
    
    &usb0 {
    	dr_mode = "host";	
    	phy-names = "cdns3,usb3-phy";
    	phys = <&serdes0_usb_link>;
    	status="okay";
    };
    
    &tscadc0 {
    	adc {
    		ti,adc-channels = <0 1 2 3 4 5 6 7>;
    	};
    };
    
    &serdes_refclk {
    	status="okay";
    	clock-frequency = <100000000>;
    };
    
    &serdes0 {
    	status="okay";
    	serdes0_pcie_link: phy@0 {
    		reg = <0>;
    		cdns,num-lanes = <2>;
    		#phy-cells = <0>;
    		cdns,phy-type = <PHY_TYPE_PCIE>;
    		resets = <&serdes_wiz0 1>, <&serdes_wiz0 2>;
    	};
    
            serdes0_usb_link: phy@1 {
                    reg = <3>;
                    cdns,num-lanes = <1>;
                    #phy-cells = <0>;
                    cdns,phy-type = <PHY_TYPE_USB3>;
                    resets = <&serdes_wiz0 4>;
            };
    };
    
    &serdes_wiz0 {
    	status = "okay";
    };
    
    &pcie1_rc {
    	phys = <&serdes0_pcie_link>;
    	phy-names = "pcie-phy";
    	num-lanes = <2>;
    	status="okay";
    };
    
    &pcie1_ep {
    	phys = <&serdes0_pcie_link>;
    	phy-names = "pcie-phy";
    	num-lanes = <2>;
    	status = "disabled";
    };
    
    &wkup_gpio0 {
    	status = "okay";
    };
    

    // SPDX-License-Identifier: GPL-2.0
    /*
     * Copyright (C) 2020 Texas Instruments Incorporated - https://www.ti.com/
     */
    
    #include "k3-j7200-binman.dtsi"
    
    / {
    	chosen {
    		stdout-path = "serial2:115200n8";
    		tick-timer = &timer1;
    	};
    
    	aliases {
    		i2c0 = &wkup_i2c0;
    		i2c1 = &mcu_i2c0;
    	};
    };
    
    &cbass_main {
    	bootph-pre-ram;
    };
    
    &main_navss {
    	bootph-pre-ram;
    };
    
    &cbass_mcu_wakeup {
    	bootph-pre-ram;
    
    	timer1: timer@40400000 {
    		compatible = "ti,omap5430-timer";
    		reg = <0x0 0x40400000 0x0 0x80>;
    		ti,timer-alwon;
    		clock-frequency = <250000000>;
    		bootph-pre-ram;
    	};
    
    	chipid@43000014 {
    		bootph-pre-ram;
    	};
    
    	mcu_navss: bus@28380000 {
    		bootph-pre-ram;
    		#address-cells = <2>;
    		#size-cells = <2>;
    
    		ringacc@2b800000 {
    			reg =	<0x0 0x2b800000 0x0 0x400000>,
    				<0x0 0x2b000000 0x0 0x400000>,
    				<0x0 0x28590000 0x0 0x100>,
    				<0x0 0x2a500000 0x0 0x40000>,
    				<0x0 0x28440000 0x0 0x40000>;
    			reg-names = "rt", "fifos", "proxy_gcfg", "proxy_target", "cfg";
    			bootph-pre-ram;
    		};
    
    		dma-controller@285c0000 {
    			reg =	<0x0 0x285c0000 0x0 0x100>,
    				<0x0 0x284c0000 0x0 0x4000>,
    				<0x0 0x2a800000 0x0 0x40000>,
    				<0x0 0x284a0000 0x0 0x4000>,
    				<0x0 0x2aa00000 0x0 0x40000>,
    				<0x0 0x28400000 0x0 0x2000>;
    			reg-names = "gcfg", "rchan", "rchanrt", "tchan",
    					    "tchanrt", "rflow";
    			bootph-pre-ram;
    		};
    	};
    };
    
    &secure_proxy_main {
    	bootph-pre-ram;
    };
    
    &dmsc {
    	bootph-pre-ram;
    	k3_sysreset: sysreset-controller {
    		compatible = "ti,sci-sysreset";
    		bootph-pre-ram;
    	};
    };
    
    &k3_pds {
    	bootph-pre-ram;
    };
    
    &k3_clks {
    	bootph-pre-ram;
    };
    
    &k3_reset {
    	bootph-pre-ram;
    };
    
    &wkup_pmx0 {
    	bootph-pre-ram;
    };
    
    &main_pmx0 {
    	bootph-pre-ram;
    };
    
    &main_uart0 {
    	bootph-pre-ram;
    };
    
    &mcu_uart0 {
    	bootph-pre-ram;
    };
    
    &main_sdhci0 {
    	bootph-pre-ram;
    };
    
    &main_sdhci1 {
    	bootph-pre-ram;
    };
    
    &wkup_i2c0 {
    	bootph-pre-ram;
    };
    
    &main_usbss0_pins_default {
    	bootph-pre-ram;
    };
    
    &usbss0 {
    	bootph-pre-ram;
    };
    
    &usb0 {
            dr_mode = "host";
            phy-names = "cdns3,usb3-phy";
    	bootph-pre-ram;
    };
    
    &fss {
    	bootph-pre-ram;
    };
    
    &wkup_gpio0 {
    	bootph-pre-ram;
    };
    
    &serdes_ln_ctrl {
    	u-boot,mux-autoprobe;
    };
    
    &usb_serdes_mux {
    	u-boot,mux-autoprobe;
    };
    
    &serdes0 {
    	bootph-pre-ram;
    };
    
    &main_r5fss0 {
    	ti,cluster-mode = <0>;
    };
    

    Regards,

    Nikhil K

  • Hi Tanmay,

    Any update on this case?

    Regards,

    Nikhil K

  • Hi Nikhil,

    Sorry for the delayed response.

    Can you dump the following register:

    • 0x05060404
    • 0x05060408
    • 0x0506040C
    • 0x05060480
    • 0x05060484
    • 0x05060488
    • 0x0506048C
    • 0x050604C0
    • 0x050604C4
    • 0x050604C8
    • 0x050604CC
    • 0x05060500
    • 0x05060504
    • 0x05060508
    • 0x0506050C
    • 0x05060540
    • 0x05060544
    • 0x05060548
    • 0x0506054C
    • 0x0506E000

    Also, is that same USB working on linux kernel.

    Regards,
    Tanmay