Part Number: SK-AM64B
Tool/software:
Hi there,
I'm booting the SK EVM in bootmode Ethernet. BOOP server and TFTP are working and the tiboot3.bin from the Linux SDK is started. It just doesn't work:
U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000)
EEPROM not available at 0x50, trying to read at 0x51
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)')
SPL initial stack usage: 13408 bytes
Trying to boot from eth device
Loading Environment from MMC... MMC Device 0 not found
*** Warning - No MMC card found, using default environment
No ethernet found.
No Ethernet devices found
SPL: failed to boot from all boot devices
I gues I need a U-Boot that's set up for this.
Where can I find / how can I compile a U-Boot to boot from Ethernet on the SK EVM board?
best regards,
Joachim