Other Parts Discussed in Thread: AM1808
hello,
I am using Am1808. i ran ti sdk setup. Setup did the installation for host PC and configured the SDK kit for NFS deployment.
But i am unable to start the kernel this is the following sequence which gets displayed on the terminal
print
ethaddr=00:08:ee:04:ad:36
ipaddr=130.0.3.165
bootdelay=4
baudrate=115200
oldbootargs=console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off
autoload=no
bootfile=uImage-am180x-evm.bin
serverip=130.0.125.144
netmask=255.255.0.0
bootcmd=tftp;bootm
gatewayip=130.0.125.144
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2009.11 (Apr 15 2011 - 13:22:24)
bootargs=console=ttyS2,115200n8 rw noinitrd mem=64M@0xc4000000 root=/dev/nfs nfsroot=130.0.125.144:/home/sanket/ti-sdk-am180x-evm-05.02.00.00/targetNFS,nolock,rsize=1024,wsize=1024 ip=130.0.3.165:130.0.125.144:130.0.125.144:255.255.0.0:sanket::off
Environment size: 609/65532 bytes
U-Boot > boot
Using device
TFTP from server 130.0.125.144; our IP address is 130.0.3.165
Filename 'uImage-am180x-evm.bin'.
Load address: 0xc0700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
###############################################################
done
Bytes transferred = 2317256 (235bc8 hex)
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Arago/2.6.37-psp03.21.00.04.sdk/
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2317192 Bytes = 2.2 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
What could be the issue and please suggest ways to debug this. I have a AM1808 Rev A EVM of logicpd and using SDK 5.02 - latest drop from ti.com.
Sanket