This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with Beagleboard XM rev.C and android.

Hello everyone.

we just bought a Beagleboard xm to assist us with our development. We flashed the sd card with the gingerbread 2.3.4 version 2.1 release and we have it up and running.

The problem is...ethernet port is blinking...but there's no panel to configure the ethernet in the menus...and hence it's not working...how can we do that?

 

  Also...we are working with a 3M EX II  usb touchscreen....we asked 3m for support and they gave us a driver: config_usb_touchscreen_3m...even with that the touchscreen does not work....anyone can help?

 

Thanks in advance.