Part Number: J784S4XEVM
Tool/software:
I would like to understand the process of configuring CAN on J784S4. Specifically i want to know
1. How do i configure muxed pins as CAN High and CAN Low pin.
2. As there are several uC cores and uP cores. How do i configure a particular instance of a CAN peripheral to be used by a particular core.
3. Where are the APIs for configuring CAN documentad?
3. I saw that there is CSL library and MCAL layer. Can MCAL be used if i am only freeRTOS or is it ment only to be used with Autosar?
4. Is there any example that run on J784s4 out of the box