Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH
Tool/software:
Hi,
we want to toggle GPIO pin 50 on the TDA4VH via PDK. As far as we understood we therefore need to configure the GPIO module.
The configuration we have so far:
enum Pins { GPIO0_50 = 0U, PIN_MAX };
uint32_t gpioBaseAddr[PIN_MAX] = { CSL_WKUP_GPIO0_BASE };
GPIO_PinConfig gpioPinConfigs[PIN_MAX] = {
GPIO_DEVICE_CONFIG(1U, 18U) /* 50 = port 1, pin 18 */
| GPIO_CFG_IN_INT_NONE | GPIO_CFG_OUTPUT
}
GPIO_CallbackFxn gpioCallbackFunctions[PIN_MAX] = { NULL };
GPIO_v0_Config GPIO_v0_config = {
gpioPinConfigs,
gpioCallbackFunctions,
sizeof(gpioPinConfigs) / sizeof(GPIO_PinConfig),
sizeof(gpioCallbackFunctions) / sizeof(GPIO_CallbackFxn),
0x8U /* R5F */
}
static void Board_initGPIO(void)
{
GPIO_v0_HwAttrs gpio_cfg;
for (int looper = 0U; looper < PIN_MAX; looper++)
{
GPIO_socGetInitCfg(looper, &gpio_cfg);
gpio_cfg.baseAddr = gpioBaseAddr[looper];
GPIO_socSetInitCfg(looper, &gpio_cfg);
}
}
void main()
{
Board_initGPIO();
GPIO_init();
GPIO_write(GPIO0_50, 0U);
}
Since it currently doesn't seem to work: Did we miss anything in the configuration?
Thanks,
Thomas