This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: SD card boot mode Failed to load 'boot.scr'

Part Number: AM62A7

Tool/software:

Hi Ti

Today I created an SD card using BalenaEtcher, but I couldn't access the system and kept restarting.

In addition, when I use the WIC file on the official website to create an SD card and configure the environment variable to setenv name_overlays k3-am62x-sk-csi2-imx219.dtbo, the above problems also occur.

https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_02_01_09/exports/docs/linux/Overview/Processor_SDK_Linux_create_SD_card.html#processor-sdk-linux-create-sd-card-using-balena

log

 SD_card_boot_log.log

plese help me check.

Regist

Daohong