This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J784S4: Cannot receive data on CAN bus on SDK-J784S4 9.2

Part Number: PROCESSOR-SDK-J784S4

Tool/software:

Hello everyone,

We are testing the CAN setup on the Linux Bootloader (SPL + U-Boot) on the A72 Linux core by following the instructions in section 4.9.3 of the provided J784S4 MCAN User Guide.

We attempted the internal loopback (as it’s mentioned that this does not require any additional setup) between two terminals on the board. One terminal executes the cansend command, while the other uses candump to listen for and receive any incoming messages. We tested this on all three enabled CAN interfaces (mcu_mcan0, mcu_mcan1, main_mcan16), but nothing is being received.

Additionally, we tried using an external transmitter by connecting Vector's VN1610 jumper wires to J46 on the EVA board and the USB-C to the PC. We used an application that utilizes Vector's XL Driver Library API to send data to the CAN bus, but still, nothing is being received.

y connecting Vector's VN1610 jumper wires to J46 on the EVA board and the USB-C to the PC, with an application utilizing Vector's XL Driver Library API to send data to the CAN bus, but still nothing is being received.

It's worth mentioning that all relevant steps from related questions have been verified:

  • After executing the command to turn on CAN interfaces mentioned in the CAN Utilities section of the Linux MCAN Driver Guide, the following interfaces are shown:

    • ip addr show | grep can
      4: mcu_mcan0: mtu 16 qdisc pfifo_fast state UP group default qlen 10
       link/can 
      5: mcu_mcan1: mtu 16 qdisc pfifo_fast state UP group default qlen 10
       link/can 
      6: main_mcan16: mtu 16 qdisc pfifo_fast state UP group default...
      
  • The code changes mentioned in this Git commit have been verified and are present in our DTS files.

Also, is there any way to enable debug logs for CAN to diagnose if anything under the hood is problematic?

Regards,
Dušan

  • Hi Dušan,

    I see that there is a mixture of RTOS and Linux driver/documentation. Since you are using cansend, I assume you are using the Linux driver.

    Can you do an external loopback and see if you can send and receive? Please send the full logs of this experiment.

    As for logs, the driver being used should be this driver:

    https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/drivers/net/can/m_can/m_can_platform.c?h=ti-linux-6.1.y

    You can put some printk statements in there to debug.

    Regards,

    Takuma

  • Hi Takuma,

    Yes, I am using a Linux driver.

    We tried using an external loopback between main_mcan16 (J46) and mcu_mcan0 (J42) with jumper wires, but still no success—no messages have been received.

    I will provide a picture of our setup so you can check if everything is in order.

    Another concern is that the internal loopback is also not working, even though others have reported success with receiving messages in similar setups.

    I'm also sending you logs from the ipconfig -a and dmesg (which were executed after setting up CAN interfaces) commands to help identify any issues we may have overlooked.

    Regards,


    Dušan

    eth0: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
            ether 3c:e0:64:62:4a:97  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    eth1: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
            inet 192.168.238.87  netmask 255.255.255.0  broadcast 192.168.238.255
            inet6 fe80::8892:4ff:fe85:c128  prefixlen 64  scopeid 0x20<link>
            ether 8a:92:04:85:c1:28  txqueuelen 1000  (Ethernet)
            RX packets 8908  bytes 1091000 (1.0 MiB)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 922  bytes 497746 (486.0 KiB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    eth2: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
            inet6 fe80::72fa:9cff:fede:4423  prefixlen 64  scopeid 0x20<link>
            ether 70:fa:9c:de:44:23  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 46  bytes 10120 (9.8 KiB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    eth3: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500
            inet6 fe80::72fe:7eff:febb:ad7a  prefixlen 64  scopeid 0x20<link>
            ether 70:fe:7e:bb:ad:7a  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 45  bytes 10050 (9.8 KiB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    lo: flags=73<UP,LOOPBACK,RUNNING>  mtu 65536
            inet 127.0.0.1  netmask 255.0.0.0
            inet6 ::1  prefixlen 128  scopeid 0x10<host>
            loop  txqueuelen 1000  (Local Loopback)
            RX packets 92  bytes 7654 (7.4 KiB)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 92  bytes 7654 (7.4 KiB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    main_mcan16: flags=193<UP,RUNNING,NOARP>  mtu 16
            unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00  txqueuelen 10  (UNSPEC)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
            device interrupt 126  
    
    mcu_mcan0: flags=193<UP,RUNNING,NOARP>  mtu 16
            unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00  txqueuelen 10  (UNSPEC)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
            device interrupt 124  
    
    mcu_mcan1: flags=193<UP,RUNNING,NOARP>  mtu 16
            unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00  txqueuelen 10  (UNSPEC)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
            device interrupt 125  
    
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
    [    0.000000] Linux version 6.1.80-ti-g2e423244f8c0 (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Wed Mar 20 14:43:33 UTC 2024
    [    0.000000] Machine model: Texas Instruments J784S4 EVM
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002880000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a5000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a5100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a8000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a8100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 48 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-rtos-ipc-memory-region@ac000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000af000000, size 48 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@af000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b2000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@b2000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b2100000, size 5 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_0-memory@b2100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b4000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-dma-memory@b4000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b4100000, size 5 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-memory@b4100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b6000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_2-dma-memory@b6000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b6100000, size 5 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_2-memory@b6100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b8000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_3-dma-memory@b8000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b8100000, size 5 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_3-memory@b8100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ba000000, size 64 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@ba000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000be000000, size 8 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-queues@be000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000be800000, size 24 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-buffers@be800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 2048 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000980000000, size 1792 MiB
    [    0.000000] OF: reserved mem: initialized node linux-cma-buffers@980000000, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   [mem 0x0000000100000000-0x0000000fffffffff]
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a8ffffff]
    [    0.000000]   node   0: [mem 0x00000000a9000000-0x00000000abffffff]
    [    0.000000]   node   0: [mem 0x00000000ac000000-0x00000000b2603fff]
    [    0.000000]   node   0: [mem 0x00000000b2604000-0x00000000b3ffffff]
    [    0.000000]   node   0: [mem 0x00000000b4000000-0x00000000b4603fff]
    [    0.000000]   node   0: [mem 0x00000000b4604000-0x00000000b5ffffff]
    [    0.000000]   node   0: [mem 0x00000000b6000000-0x00000000b6603fff]
    [    0.000000]   node   0: [mem 0x00000000b6604000-0x00000000b7ffffff]
    [    0.000000]   node   0: [mem 0x00000000b8000000-0x00000000b8603fff]
    [    0.000000]   node   0: [mem 0x00000000b8604000-0x00000000b9ffffff]
    [    0.000000]   node   0: [mem 0x00000000ba000000-0x00000000bfffffff]
    [    0.000000]   node   0: [mem 0x00000000c0000000-0x00000000ffffffff]
    [    0.000000]   node   0: [mem 0x0000000880000000-0x00000008ffffffff]
    [    0.000000]   node   0: [mem 0x0000000900000000-0x0000000fffffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x0000000fffffffff]
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.4
    [    0.000000] percpu: Embedded 20 pages/cpu s41064 r8192 d32664 u81920
    [    0.000000] pcpu-alloc: s41064 r8192 d32664 u81920 alloc=20*4096
    [    0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [0] 4 [0] 5 [0] 6 [0] 7 
    [    0.000000] Detected PIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: Spectre-v3a
    [    0.000000] CPU features: detected: Spectre-BHB
    [    0.000000] CPU features: detected: ARM erratum 1742098
    [    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 8257536
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02880000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=82eb3a92-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 4194304 (order: 13, 33554432 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 2097152 (order: 12, 16777216 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] software IO TLB: area num 8.
    [    0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
    [    0.000000] Memory: 27524696K/33554432K available (11712K kernel code, 1258K rwdata, 3812K rodata, 1984K init, 438K bss, 4194728K reserved, 1835008K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=8, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu: 	RCU event tracing is enabled.
    [    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=8.
    [    0.000000] 	Trampoline variant of Tasks RCU enabled.
    [    0.000000] 	Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=8
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: [Firmware Bug]: GICR region 0x0000000001900000 has overlapping address
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 960 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] Root IRQ handler: gic_handle_irq
    [    0.000000] GICv3: GICv3 features: 16 PPIs
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @93c800000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x000000093c050000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x000000093c060000
    [    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008427] Console: colour dummy device 80x25
    [    0.012997] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.023668] pid_max: default: 32768 minimum: 301
    [    0.028405] LSM: Security Framework initializing
    [    0.033220] Mount-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.041020] Mountpoint-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.050114] cblist_init_generic: Setting adjustable number of callback queues.
    [    0.057507] cblist_init_generic: Setting shift to 3 and lim to 1.
    [    0.063769] cblist_init_generic: Setting adjustable number of callback queues.
    [    0.071155] cblist_init_generic: Setting shift to 3 and lim to 1.
    [    0.077459] rcu: Hierarchical SRCU implementation.
    [    0.082356] rcu: 	Max phase no-delay instances is 1000.
    [    0.087838] Platform MSI: msi-controller@1820000 domain created
    [    0.094030] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
    [    0.103461] EFI services will not be available.
    [    0.108292] smp: Bringing up secondary CPUs ...
    [    0.121364] Detected PIPT I-cache on CPU1
    [    0.121417] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
    [    0.121430] GICv3: CPU1: using allocated LPI pending table @0x000000093c070000
    [    0.121460] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
    [    0.129904] Detected PIPT I-cache on CPU2
    [    0.129949] GICv3: CPU2: found redistributor 2 region 0:0x0000000001940000
    [    0.129962] GICv3: CPU2: using allocated LPI pending table @0x000000093c080000
    [    0.129985] CPU2: Booted secondary processor 0x0000000002 [0x411fd080]
    [    0.138388] Detected PIPT I-cache on CPU3
    [    0.138431] GICv3: CPU3: found redistributor 3 region 0:0x0000000001960000
    [    0.138443] GICv3: CPU3: using allocated LPI pending table @0x000000093c090000
    [    0.138467] CPU3: Booted secondary processor 0x0000000003 [0x411fd080]
    [    0.146917] Detected PIPT I-cache on CPU4
    [    0.146998] GICv3: CPU4: found redistributor 100 region 0:0x0000000001980000
    [    0.147012] GICv3: CPU4: using allocated LPI pending table @0x000000093c0a0000
    [    0.147043] CPU4: Booted secondary processor 0x0000000100 [0x411fd080]
    [    0.155505] Detected PIPT I-cache on CPU5
    [    0.155556] GICv3: CPU5: found redistributor 101 region 0:0x00000000019a0000
    [    0.155569] GICv3: CPU5: using allocated LPI pending table @0x000000093c0b0000
    [    0.155594] CPU5: Booted secondary processor 0x0000000101 [0x411fd080]
    [    0.164019] Detected PIPT I-cache on CPU6
    [    0.164072] GICv3: CPU6: found redistributor 102 region 0:0x00000000019c0000
    [    0.164085] GICv3: CPU6: using allocated LPI pending table @0x000000093c0c0000
    [    0.164108] CPU6: Booted secondary processor 0x0000000102 [0x411fd080]
    [    0.172529] Detected PIPT I-cache on CPU7
    [    0.172583] GICv3: CPU7: found redistributor 103 region 0:0x00000000019e0000
    [    0.172595] GICv3: CPU7: using allocated LPI pending table @0x000000093c0d0000
    [    0.172619] CPU7: Booted secondary processor 0x0000000103 [0x411fd080]
    [    0.172664] smp: Brought up 1 node, 8 CPUs
    [    0.353640] SMP: Total of 8 processors activated.
    [    0.358445] CPU features: detected: 32-bit EL0 Support
    [    0.363700] CPU features: detected: CRC32 instructions
    [    0.368997] CPU: All CPU(s) started at EL2
    [    0.373186] alternatives: applying system-wide alternatives
    [    0.379839] devtmpfs: initialized
    [    0.393400] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.403378] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
    [    0.434434] pinctrl core: initialized pinctrl subsystem
    [    0.440084] DMI not present or invalid.
    [    0.444327] NET: Registered PF_NETLINK/PF_ROUTE protocol family
    [    0.451652] DMA: preallocated 4096 KiB GFP_KERNEL pool for atomic allocations
    [    0.459675] DMA: preallocated 4096 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.468398] DMA: preallocated 4096 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.476630] audit: initializing netlink subsys (disabled)
    [    0.482248] audit: type=2000 audit(0.340:1): state=initialized audit_enabled=0 res=1
    [    0.482442] thermal_sys: Registered thermal governor 'step_wise'
    [    0.490166] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.496386] cpuidle: using governor menu
    [    0.507123] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.514148] ASID allocator initialised with 65536 entries
    [    0.527778] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@100000/pinctrl@a40000/mcu-cpsw-cpts
    [    0.539883] KASLR disabled due to lack of seed
    [    0.547170] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.554121] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
    [    0.560526] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.567461] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
    [    0.573863] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.580797] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
    [    0.587199] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.594134] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
    [    0.601210] k3-chipinfo 43000014.chipid: Family:J784S4 rev:SR1.0 JTAGID[0x0bb8002f] Detected
    [    0.610722] iommu: Default domain type: Translated 
    [    0.615707] iommu: DMA domain TLB invalidation policy: strict mode 
    [    0.622218] SCSI subsystem initialized
    [    0.626115] libata version 3.00 loaded.
    [    0.626193] usbcore: registered new interface driver usbfs
    [    0.631812] usbcore: registered new interface driver hub
    [    0.637251] usbcore: registered new device driver usb
    [    0.642598] pps_core: LinuxPPS API ver. 1 registered
    [    0.647670] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.657007] PTP clock support registered
    [    0.661092] EDAC MC: Ver: 3.0.0
    [    0.664750] FPGA manager framework
    [    0.668254] Advanced Linux Sound Architecture Driver Initialized.
    [    0.674862] clocksource: Switched to clocksource arch_sys_counter
    [    0.681199] VFS: Disk quotas dquot_6.6.0
    [    0.685224] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.695162] Carveout Heap: Exported 960 MiB at 0x0000000900000000
    [    0.701439] NET: Registered PF_INET protocol family
    [    0.706817] IP idents hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.719690] tcp_listen_portaddr_hash hash table entries: 16384 (order: 6, 262144 bytes, linear)
    [    0.728719] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
    [    0.736653] TCP established hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.745739] TCP bind hash table entries: 65536 (order: 9, 2097152 bytes, linear)
    [    0.754138] TCP: Hash tables configured (established 262144 bind 65536)
    [    0.761009] UDP hash table entries: 16384 (order: 7, 524288 bytes, linear)
    [    0.768358] UDP-Lite hash table entries: 16384 (order: 7, 524288 bytes, linear)
    [    0.776228] NET: Registered PF_UNIX/PF_LOCAL protocol family
    [    0.782291] RPC: Registered named UNIX socket transport module.
    [    0.788350] RPC: Registered udp transport module.
    [    0.793154] RPC: Registered tcp transport module.
    [    0.797956] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.804543] NET: Registered PF_XDP protocol family
    [    0.809441] PCI: CLS 0 bytes, default 64
    [    0.814068] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
    [    0.823295] Initialise system trusted keyrings
    [    0.827941] workingset: timestamp_bits=46 max_order=23 bucket_order=0
    [    0.836484] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.842675] NFS: Registering the id_resolver key type
    [    0.847851] Key type id_resolver registered
    [    0.852123] Key type id_legacy registered
    [    0.856241] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.863090] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.890200] Key type asymmetric registered
    [    0.894385] Asymmetric key parser 'x509' registered
    [    0.899391] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
    [    0.907020] io scheduler mq-deadline registered
    [    0.911652] io scheduler kyber registered
    [    0.917973] pinctrl-single 4301c000.pinctrl: 13 pins, size 52
    [    0.923949] pinctrl-single 4301c038.pinctrl: 11 pins, size 44
    [    0.929978] pinctrl-single 4301c068.pinctrl: 72 pins, size 288
    [    0.936176] pinctrl-single 4301c190.pinctrl: 1 pins, size 4
    [    0.942000] pinctrl-single 11c000.pinctrl: 72 pins, size 288
    [    0.948356] pinctrl-single a40000.pinctrl: 512 pins, size 2048
    [    0.957770] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
    [    0.969416] loop: module loaded
    [    0.973281] megasas: 07.719.03.00-rc1
    [    0.978549] tun: Universal TUN/TAP device driver, 1.6
    [    0.984089] VFIO - User Level meta-driver version: 0.3
    [    0.989721] usbcore: registered new interface driver usb-storage
    [    0.996178] i2c_dev: i2c /dev entries driver
    [    1.001111] sdhci: Secure Digital Host Controller Interface driver
    [    1.007428] sdhci: Copyright(c) Pierre Ossman
    [    1.012001] sdhci-pltfm: SDHCI platform and OF driver helper
    [    1.018209] ledtrig-cpu: registered to indicate activity on CPUs
    [    1.024447] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    1.031193] usbcore: registered new interface driver usbhid
    [    1.036925] usbhid: USB HID core driver
    [    1.041355] optee: probing for conduit method.
    [    1.045911] optee: revision 4.1 (012cdca4)
    [    1.062303] optee: dynamic shared memory is enabled
    [    1.071683] optee: initialized driver
    [    1.076429] Initializing XFRM netlink socket
    [    1.080810] NET: Registered PF_PACKET protocol family
    [    1.086004] Key type dns_resolver registered
    [    1.090538] registered taskstats version 1
    [    1.094737] Loading compiled-in X.509 certificates
    [    1.105444] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)')
    [    1.153847] omap_i2c 42120000.i2c: bus 1 rev0.12 at 400 kHz
    [    1.160113] pca953x 0-0020: supply vcc not found, using dummy regulator
    [    1.166924] pca953x 0-0020: using no AI
    [    1.195486] pca953x 0-0022: supply vcc not found, using dummy regulator
    [    1.202302] pca953x 0-0022: using AI
    [    1.206595] omap_i2c 2000000.i2c: bus 0 rev0.12 at 400 kHz
    [    1.212377] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 177 domain created
    [    1.220909] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 10 domain created
    [    1.230151] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 283 domain created
    [    1.238801] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 321 created
    [    1.250598] ti-udma 311a0000.dma-controller: Number of rings: 48
    [    1.257789] ti-udma 311a0000.dma-controller: Channels: 48 (bchan: 0, tchan: 16, rchan: 32)
    [    1.267441] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:328
    [    1.277318] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
    [    1.284077] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
    [    1.292959] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[878,128] sci-dev-id:315
    [    1.303106] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
    [    1.309865] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
    [    1.317726] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 262, base_baud = 6000000) is a 8250
    [    1.327139] 2880000.serial: ttyS2 at MMIO 0x2880000 (irq = 263, base_baud = 3000000) is a 8250
    [    1.335989] printk: console [ttyS2] enabled
    [    1.344432] printk: bootconsole [ns16550a0] disabled
    [    1.394868] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.404107] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
    [    1.412374] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
    [    1.425218] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
    [    1.432426] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
    [    1.438585] pps pps0: new PPS source ptp0
    [    1.442715] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
    [    1.490866] davinci_mdio c200f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.499866] davinci_mdio c200f00.mdio: phy[0]: device c200f00.mdio:00, driver TI DP83867
    [    1.507957] am65-cpsw-nuss c200000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
    [    1.520692] am65-cpsw-nuss c200000.ethernet: Use random MAC address
    [    1.526946] am65-cpsw-nuss c200000.ethernet: initialized cpsw ale version 1.4
    [    1.534064] am65-cpsw-nuss c200000.ethernet: ALE Table size 64
    [    1.540168] am65-cpsw-nuss c200000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
    [    1.550195] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010c, freq:250000000, add_val:3 pps:0
    [    1.558950] mmc0: CQHCI version 5.10
    [    1.598887] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
    [    1.690306] mmc0: Command Queue Engine enabled
    [    1.694769] mmc0: new HS200 MMC card at address 0001
    [    1.700133] mmcblk0: mmc0:0001 G1M15L 29.6 GiB 
    [    1.705860] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB 
    [    1.711596] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB 
    [    1.717225] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (240:0)
    [    1.792637] tps6594-rtc tps6594-rtc.4.auto: registered as rtc0
    [    1.799335] tps6594-rtc tps6594-rtc.4.auto: setting system clock to 2024-08-15T08:53:24 UTC (1723712004)
    [    1.809131] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fca100
    [    1.815914] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fca100
    [    1.822691] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fca100
    [    1.829464] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fca100
    [    1.836246] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fca100
    [    1.843023] omap-mailbox 31f85000.mailbox: omap mailbox rev 0x66fca100
    [    1.851474] ti-udma 285c0000.dma-controller: Channels: 22 (tchan: 11, rchan: 11, gp-rflow: 8)
    [    1.861375] ti-udma 31150000.dma-controller: Channels: 66 (tchan: 33, rchan: 33, gp-rflow: 16)
    [    1.873098] spi-nand spi0.0: Winbond SPI NAND was found.
    [    1.878404] spi-nand spi0.0: 128 MiB, block size: 256 KiB, page size: 4096, OOB size: 128
    [    1.886722] 7 fixed-partitions partitions found on MTD device spi0.0
    [    1.893066] Creating 7 MTD partitions on "spi0.0":
    [    1.897851] 0x000000000000-0x000000100000 : "ospi_nand.tiboot3"
    [    1.904771] 0x000000100000-0x000000300000 : "ospi_nand.tispl"
    [    1.911730] 0x000000300000-0x000000700000 : "ospi_nand.u-boot"
    [    1.919396] 0x000000700000-0x000000740000 : "ospi_nand.env"
    [    1.925567] 0x000000740000-0x000000780000 : "ospi_nand.env.backup"
    [    1.932325] 0x000002000000-0x000007fc0000 : "ospi_nand.rootfs"
    [    1.969808] 0x000007fc0000-0x000008000000 : "ospi_nand.phypattern"
    [    1.978619] spi-nor spi1.0: mt25qu512a (65536 Kbytes)
    [    1.983705] 7 fixed-partitions partitions found on MTD device 47050000.spi.0
    [    1.990741] Creating 7 MTD partitions on "47050000.spi.0":
    [    1.996213] 0x000000000000-0x000000100000 : "qspi.tiboot3"
    [    2.002197] 0x000000100000-0x000000300000 : "qspi.tispl"
    [    2.008047] 0x000000300000-0x000000700000 : "qspi.u-boot"
    [    2.013941] 0x000000700000-0x000000740000 : "qspi.env"
    [    2.019589] 0x000000740000-0x000000780000 : "qspi.env.backup"
    [    2.025832] 0x000000800000-0x000003fc0000 : "qspi.rootfs"
    [    2.031752] 0x000003fc0000-0x000004000000 : "qspi.phypattern"
    [    2.074870] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    2.084097] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
    [    2.092364] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
    [    2.105216] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
    [    2.112423] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
    [    2.118580] pps pps0: new PPS source ptp1
    [    2.122717] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
    [    2.132605] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
    [    2.178869] davinci_mdio c200f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    2.187978] davinci_mdio c200f00.mdio: phy[0]: device c200f00.mdio:00, driver TI DP83867
    [    2.196070] am65-cpsw-nuss c200000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
    [    2.208812] am65-cpsw-nuss c200000.ethernet: Use random MAC address
    [    2.215066] am65-cpsw-nuss c200000.ethernet: initialized cpsw ale version 1.4
    [    2.222185] am65-cpsw-nuss c200000.ethernet: ALE Table size 64
    [    2.228314] am65-cpsw-nuss c200000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
    [    2.238081] am65-cpsw-nuss c200000.ethernet: set new flow-id-base 82
    [    2.246069] mmc1: CQHCI version 5.10
    [    2.246356] debugfs: Directory 'pd:74' with parent 'pm_genpd' already present!
    [    2.256885] debugfs: Directory 'pd:73' with parent 'pm_genpd' already present!
    [    2.264106] debugfs: Directory 'pd:72' with parent 'pm_genpd' already present!
    [    2.271797] debugfs: Directory 'pd:335' with parent 'pm_genpd' already present!
    [    2.279119] debugfs: Directory 'pd:333' with parent 'pm_genpd' already present!
    [    2.286425] debugfs: Directory 'pd:332' with parent 'pm_genpd' already present!
    [    2.290506] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
    [    2.308751] ALSA device list:
    [    2.311717]   No soundcards found.
    [    2.315304] Waiting for root device PARTUUID=82eb3a92-02...
    [    2.348636] mmc1: new ultra high speed SDR104 SDHC card at address 5048
    [    2.355613] mmcblk1: mmc1:5048 SD32G 28.8 GiB 
    [    2.361609]  mmcblk1: p1 p2
    [    2.373566] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
    [    2.382106] VFS: Mounted root (ext4 filesystem) on device 179:98.
    [    2.389083] devtmpfs: mounted
    [    2.392745] Freeing unused kernel memory: 1984K
    [    2.397374] Run /sbin/init as init process
    [    2.401461]   with arguments:
    [    2.401463]     /sbin/init
    [    2.401465]   with environment:
    [    2.401466]     HOME=/
    [    2.401468]     TERM=linux
    [    2.578032] NET: Registered PF_INET6 protocol family
    [    2.583608] Segment Routing with IPv6
    [    2.587284] In-situ OAM (IOAM) with IPv6
    [    2.609862] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
    [    2.641347] systemd[1]: Detected architecture arm64.
    [    2.715920] systemd[1]: Hostname set to <j784s4-evm>.
    [    2.778973] systemd-sysv-generator[191]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.915376] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    2.955888] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.002526] systemd[1]: Queued start job for default target Graphical Interface.
    [    3.046706] systemd[1]: Created slice Slice /system/getty.
    [    3.068176] systemd[1]: Created slice Slice /system/modprobe.
    [    3.091928] systemd[1]: Created slice Slice /system/serial-getty.
    [    3.115764] systemd[1]: Created slice User and Session Slice.
    [    3.139017] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [    3.162972] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [    3.187016] systemd[1]: Reached target Path Units.
    [    3.202918] systemd[1]: Reached target Remote File Systems.
    [    3.222913] systemd[1]: Reached target Slice Units.
    [    3.238921] systemd[1]: Reached target Swaps.
    [    3.284981] systemd[1]: Listening on RPCbind Server Activation Socket.
    [    3.310967] systemd[1]: Reached target RPC Port Mapper.
    [    3.334183] systemd[1]: Listening on Process Core Dump Socket.
    [    3.355009] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [    3.379169] systemd[1]: Listening on Journal Audit Socket.
    [    3.399081] systemd[1]: Listening on Journal Socket (/dev/log).
    [    3.419103] systemd[1]: Listening on Journal Socket.
    [    3.435131] systemd[1]: Listening on Network Service Netlink Socket.
    [    3.459135] systemd[1]: Listening on udev Control Socket.
    [    3.479033] systemd[1]: Listening on udev Kernel Socket.
    [    3.499059] systemd[1]: Listening on User Database Manager Socket.
    [    3.535103] systemd[1]: Mounting Huge Pages File System...
    [    3.553254] systemd[1]: Mounting POSIX Message Queue File System...
    [    3.577033] systemd[1]: Mounting Kernel Debug File System...
    [    3.591114] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
    [    3.607143] systemd[1]: Mounting Temporary Directory /tmp...
    [    3.629438] systemd[1]: Starting Create List of Static Device Nodes...
    [    3.656823] systemd[1]: Starting Load Kernel Module configfs...
    [    3.676846] systemd[1]: Starting Load Kernel Module drm...
    [    3.697625] systemd[1]: Starting Load Kernel Module fuse...
    [    3.708957] fuse: init (API version 7.37)
    [    3.730449] systemd[1]: Starting Start psplash boot splash screen...
    [    3.795268] systemd[1]: Starting RPC Bind...
    [    3.811010] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
    [    3.826701] systemd[1]: Starting Journal Service...
    [    3.847144] systemd[1]: Starting Load Kernel Modules...
    [    3.858675] cryptodev: loading out-of-tree module taints kernel.
    [    3.865486] cryptodev: driver 1.12 loaded.
    [    3.872471] systemd[1]: Starting Generate network units from Kernel command line...
    [    3.901729] systemd[1]: Starting Remount Root and Kernel File Systems...
    [    3.912277] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
    [    3.937709] systemd[1]: Starting Coldplug All udev Devices...
    [    3.963470] systemd[1]: Started RPC Bind.
    [    3.983194] systemd[1]: Started Journal Service.
    [    4.336043] systemd-journald[211]: Received client request to flush runtime journal.
    [    4.545104] audit: type=1334 audit(1723712007.240:2): prog-id=5 op=LOAD
    [    4.551736] audit: type=1334 audit(1723712007.248:3): prog-id=6 op=LOAD
    [    4.707039] random: crng init done
    [    4.723494] CAN device driver interface
    [    4.751886] j721e-pcie-host 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
    [    4.759922] j721e-pcie-host 2900000.pcie:       IO 0x0010001000..0x0010010fff -> 0x0010001000
    [    4.768544] j721e-pcie-host 2900000.pcie:      MEM 0x0010011000..0x0017ffffff -> 0x0010011000
    [    4.779486] j721e-pcie-host 2900000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    4.793374] mc: Linux media interface: v0.10
    [    4.812001] videodev: Linux video capture interface: v2.00
    [    4.813441] PVR_K:  247: Device: 4e20000000.gpu
    [    4.819542] mtdblock: MTD device 'ospi_nand.tiboot3' is NAND, please consider using UBI block devices instead.
    [    4.825311] PVR_K:  247: Read BVNC 36.53.104.796 from HW device registers
    [    4.825972] mtdblock: MTD device 'ospi_nand.env' is NAND, please consider using UBI block devices instead.
    [    4.833777] mtdblock: MTD device 'ospi_nand.tispl' is NAND, please consider using UBI block devices instead.
    [    4.838633] mtdblock: MTD device 'ospi_nand.u-boot' is NAND, please consider using UBI block devices instead.
    [    4.839173] mtdblock: MTD device 'ospi_nand.env.backup' is NAND, please consider using UBI block devices instead.
    [    4.839383] PVR_K:  247: RGX Device registered BVNC 36.53.104.796 with 1 core in the system
    [    4.839549] mtdblock: MTD device 'ospi_nand.rootfs' is NAND, please consider using UBI block devices instead.
    [    4.844434] k3-dsp-rproc 64800000.dsp: assigned reserved memory node vision-apps-c71-dma-memory@b2000000
    [    4.847972] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode
    [    4.859587] mtdblock: MTD device 'ospi_nand.phypattern' is NAND, please consider using UBI block devices instead.
    [    4.868598] remoteproc remoteproc0: 64800000.dsp is available
    [    4.871476] [drm] Initialized pvr 23.3.6512818 20170530 for 4e20000000.gpu on minor 0
    [    4.937430] remoteproc remoteproc0: attaching to 64800000.dsp
    [    4.956176] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    4.962595] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    4.972682] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.001018] remoteproc remoteproc0: unsupported resource 65538
    [    5.002144] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
    [    5.004068] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.004079] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.004095] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.007292] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode
    [    5.019179] platform 41000000.r5f: configured R5F for IPC-only mode
    [    5.024885] rproc-virtio rproc-virtio.7.auto: assigned reserved memory node vision-apps-c71-dma-memory@b2000000
    [    5.034063] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.034226] platform 41000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
    [    5.035522] remoteproc remoteproc1: 41000000.r5f is available
    [    5.035585] remoteproc remoteproc1: attaching to 41000000.r5f
    [    5.038076] platform 41000000.r5f: R5F core initialized in IPC-only mode
    [    5.038088] rproc-virtio rproc-virtio.8.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
    [    5.042746] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    5.047071] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.047609] virtio_rpmsg_bus virtio1: rpmsg host is online
    [    5.047764] rproc-virtio rproc-virtio.7.auto: registered virtio1 (type 7)
    [    5.047802] remoteproc remoteproc0: remote processor 64800000.dsp is now attached
    [    5.047808] k3-dsp-rproc 64800000.dsp: register pm nitifiers in remoteproc mode
    [    5.052931] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
    [    5.052941] k3-dsp-rproc 65800000.dsp: assigned reserved memory node vision-apps-c71_1-dma-memory@b4000000
    [    5.053059] rproc-virtio rproc-virtio.8.auto: registered virtio0 (type 7)
    [    5.053067] remoteproc remoteproc1: remote processor 41000000.r5f is now attached
    [    5.053331] platform 41400000.r5f: configured R5F for remoteproc mode
    [    5.053663] platform 41400000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a1000000
    [    5.058329] remoteproc remoteproc3: 41400000.r5f is available
    [    5.062788] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.064883] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
    [    5.068966] k3-dsp-rproc 65800000.dsp: configured DSP for IPC-only mode
    [    5.074001] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
    [    5.078878] remoteproc remoteproc3: loading /lib/firmware/j784s4-mcu-r5f0_1-fw failed with error -22
    [    5.235848] remoteproc remoteproc3: Direct firmware load for j784s4-mcu-r5f0_1-fw failed with error -22
    [    5.245445] remoteproc remoteproc3: powering up 41400000.r5f
    [    5.251194] remoteproc remoteproc3: loading /lib/firmware/j784s4-mcu-r5f0_1-fw failed with error -22
    [    5.251232] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.260351] remoteproc remoteproc3: Direct firmware load for j784s4-mcu-r5f0_1-fw failed with error -22
    [    5.260366] remoteproc remoteproc3: request_firmware failed: -22
    [    5.264820] remoteproc remoteproc2: 65800000.dsp is available
    [    5.264867] remoteproc remoteproc2: attaching to 65800000.dsp
    [    5.265086] remoteproc remoteproc2: unsupported resource 65538
    [    5.265190] k3-dsp-rproc 65800000.dsp: DSP initialized in IPC-only mode
    [    5.265201] rproc-virtio rproc-virtio.9.auto: assigned reserved memory node vision-apps-c71_1-dma-memory@b4000000
    [    5.265550] virtio_rpmsg_bus virtio2: rpmsg host is online
    [    5.265564] rproc-virtio rproc-virtio.9.auto: registered virtio2 (type 7)
    [    5.265568] remoteproc remoteproc2: remote processor 65800000.dsp is now attached
    [    5.265573] k3-dsp-rproc 65800000.dsp: register pm nitifiers in remoteproc mode
    [    5.266254] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.266329] k3-dsp-rproc 66800000.dsp: assigned reserved memory node vision-apps-c71_2-dma-memory@b6000000
    [    5.275526] k3-dsp-rproc 66800000.dsp: configured DSP for IPC-only mode
    [    5.275574] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
    [    5.281580] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.288959] remoteproc remoteproc4: 66800000.dsp is available
    [    5.297509] m_can_platform 40528000.can: m_can device registered (irq=636, version=32)
    [    5.299642] remoteproc remoteproc4: attaching to 66800000.dsp
    [    5.307212] m_can_platform 40568000.can: m_can device registered (irq=637, version=32)
    [    5.316065] remoteproc remoteproc4: unsupported resource 65538
    [    5.323131] m_can_platform 26a1000.can: m_can device registered (irq=638, version=32)
    [    5.328194] k3-dsp-rproc 66800000.dsp: DSP initialized in IPC-only mode
    [    5.336550] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.342951] rproc-virtio rproc-virtio.10.auto: assigned reserved memory node vision-apps-c71_2-dma-memory@b6000000
    [    5.352040] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.365770] virtio_rpmsg_bus virtio3: rpmsg host is online
    [    5.368607] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.375461] rproc-virtio rproc-virtio.10.auto: registered virtio3 (type 7)
    [    5.381351] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd
    [    5.387039] remoteproc remoteproc4: remote processor 66800000.dsp is now attached
    [    5.387048] k3-dsp-rproc 66800000.dsp: register pm nitifiers in remoteproc mode
    [    5.395086] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.401091] k3-dsp-rproc 67800000.dsp: assigned reserved memory node vision-apps-c71_3-dma-memory@b8000000
    [    5.409049] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.416312] k3-dsp-rproc 67800000.dsp: configured DSP for IPC-only mode
    [    5.422539] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.429965] remoteproc remoteproc5: 67800000.dsp is available
    [    5.444402] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.445858] remoteproc remoteproc5: attaching to 67800000.dsp
    [    5.454564] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.461020] remoteproc remoteproc5: unsupported resource 65538
    [    5.465692] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.472638] k3-dsp-rproc 67800000.dsp: DSP initialized in IPC-only mode
    [    5.480680] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.487073] rproc-virtio rproc-virtio.11.auto: assigned reserved memory node vision-apps-c71_3-dma-memory@b8000000
    [    5.488989] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled
    [    5.488997] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled
    [    5.489001] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled
    [    5.489004] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled
    [    5.494379] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.495639] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c
    [    5.500656] virtio_rpmsg_bus virtio4: rpmsg host is online
    [    5.504217] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xd
    [    5.509846] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.512568] scsi host0: ufshcd
    [    5.518955] rproc-virtio rproc-virtio.11.auto: registered virtio4 (type 7)
    [    5.521741] m_can_platform 40528000.can mcu_mcan0: renamed from can0
    [    5.526739] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.531370] remoteproc remoteproc5: remote processor 67800000.dsp is now attached
    [    5.537099] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.537125] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.542888] k3-dsp-rproc 67800000.dsp: register pm nitifiers in remoteproc mode
    [    5.544967] scsi 0:0:0:49488: Well-known LUN    TOSHIBA  THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
    [    5.545883] scsi 0:0:0:49476: Well-known LUN    TOSHIBA  THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
    [    5.546625] cdns-ufshcd 4e84000.ufs: ufshcd_scsi_add_wlus: BOOT WLUN not found
    [    5.549738] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.559994] mtdblock: MTD device 'ospi_nand.phypattern' is NAND, please consider using UBI block devices instead.
    [    5.563507] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.563530] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.622702] mtdblock: MTD device 'ospi_nand.env.backup' is NAND, please consider using UBI block devices instead.
    [    5.623827] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.658710] m_can_platform 40568000.can mcu_mcan1: renamed from can1
    [    5.661308] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.661331] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.669613] mtdblock: MTD device 'ospi_nand.u-boot' is NAND, please consider using UBI block devices instead.
    [    5.806994] j721e-pcie-host 2900000.pcie: PCI host bridge to bus 0000:00
    [    5.827785] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    5.838794] pci_bus 0000:00: root bus resource [io  0x0000-0xffff] (bus address [0x10001000-0x10010fff])
    [    5.838798] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
    [    5.838834] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
    [    5.861182] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
    [    5.870983] pci 0000:00:00.0: supports D1
    [    5.875018] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
    [    5.883275] m_can_platform 26a1000.can main_mcan16: renamed from can2
    [    5.883575] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
    [    5.898035] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
    [    5.904671] pci 0000:00:00.0: PCI bridge to [bus 01]
    [    5.909990] pcieport 0000:00:00.0: PME: Signaling with IRQ 649
    [    5.916107] pcieport 0000:00:00.0: AER: enabled with IRQ 649
    [    5.921841] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.922211] j721e-pcie-host 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    5.927612] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.927628] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.944651] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    5.950544] j721e-pcie-host 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    5.956219] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    5.964714] j721e-pcie-host 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    5.973722] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.988217] j721e-pcie-host 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    6.001907] mtdblock: MTD device 'ospi_nand.tiboot3' is NAND, please consider using UBI block devices instead.
    [    6.055523] mtdblock: MTD device 'ospi_nand.rootfs' is NAND, please consider using UBI block devices instead.
    [    6.483703] mtdblock: MTD device 'ospi_nand.env' is NAND, please consider using UBI block devices instead.
    [    6.508427] mtdblock: MTD device 'ospi_nand.tispl' is NAND, please consider using UBI block devices instead.
    [    6.641263] audit: type=1334 audit(1723712009.336:4): prog-id=7 op=LOAD
    [    6.648191] audit: type=1334 audit(1723712009.344:5): prog-id=8 op=LOAD
    [    6.844894] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    6.861248] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    6.872165] cfg80211: Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
    [    6.915463] Bluetooth: Core ver 2.22
    [    6.919125] NET: Registered PF_BLUETOOTH protocol family
    [    6.924435] Bluetooth: HCI device and connection manager initialized
    [    6.930797] Bluetooth: HCI socket layer initialized
    [    6.935673] Bluetooth: L2CAP socket layer initialized
    [    6.940737] Bluetooth: SCO socket layer initialized
    [    6.987966] am65-cpsw-nuss c200000.ethernet eth1: PHY [c200f00.mdio:00] driver [TI DP83867] (irq=POLL)
    [    6.997295] am65-cpsw-nuss c200000.ethernet eth1: configuring for phy/rgmii-rxid link mode
    [    6.999052] j721e-pcie-host 2910000.pcie: PCI host bridge to bus 0001:00
    [    7.012291] pci_bus 0001:00: root bus resource [bus 00-ff]
    [    7.017791] pci_bus 0001:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
    [    7.023081] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
    [    7.027818] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
    [    7.041948] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
    [    7.048905] pci 0001:00:00.0: [104c:b013] type 01 class 0x060400
    [    7.063222] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
    [    7.073027] pci 0001:00:00.0: supports D1
    [    7.082380] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
    [    7.086883] k3_r5_rproc bus@100000:bus@28380000:r5fss@41000000: Timed out waiting for 41400000.r5f core to power up!
    [    7.088173] pci 0001:00:00.0: reg 0x224: [mem 0x00000000-0x003fffff 64bit]
    [    7.100400] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    7.100580] platform 5c00000.r5f: configured R5F for IPC-only mode
    [    7.100811] platform 5c00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
    [    7.101826] remoteproc remoteproc6: 5c00000.r5f is available
    [    7.101875] remoteproc remoteproc6: attaching to 5c00000.r5f
    [    7.102596] platform 5c00000.r5f: R5F core initialized in IPC-only mode
    [    7.102605] rproc-virtio rproc-virtio.12.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
    [    7.103089] virtio_rpmsg_bus virtio5: rpmsg host is online
    [    7.103107] rproc-virtio rproc-virtio.12.auto: registered virtio5 (type 7)
    [    7.103111] remoteproc remoteproc6: remote processor 5c00000.r5f is now attached
    [    7.103275] platform 5d00000.r5f: configured R5F for IPC-only mode
    [    7.103406] platform 5d00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
    [    7.104026] remoteproc remoteproc7: 5d00000.r5f is available
    [    7.104079] remoteproc remoteproc7: attaching to 5d00000.r5f
    [    7.104398] platform 5d00000.r5f: R5F core initialized in IPC-only mode
    [    7.104406] rproc-virtio rproc-virtio.13.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
    [    7.104972] virtio_rpmsg_bus virtio6: rpmsg host is online
    [    7.104988] rproc-virtio rproc-virtio.13.auto: registered virtio6 (type 7)
    [    7.104992] remoteproc remoteproc7: remote processor 5d00000.r5f is now attached
    [    7.105493] pci 0001:00:00.0: VF(n) BAR0 space: [mem 0x00000000-0x00ffffff 64bit] (contains BAR0 for 4 VFs)
    [    7.106734] platform 5e00000.r5f: configured R5F for IPC-only mode
    [    7.106929] platform 5e00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a5000000
    [    7.107577] remoteproc remoteproc8: 5e00000.r5f is available
    [    7.107628] remoteproc remoteproc8: attaching to 5e00000.r5f
    [    7.107930] platform 5e00000.r5f: R5F core initialized in IPC-only mode
    [    7.107938] rproc-virtio rproc-virtio.14.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a5000000
    [    7.108604] virtio_rpmsg_bus virtio7: rpmsg host is online
    [    7.108618] rproc-virtio rproc-virtio.14.auto: registered virtio7 (type 7)
    [    7.108622] remoteproc remoteproc8: remote processor 5e00000.r5f is now attached
    [    7.108793] platform 5f00000.r5f: configured R5F for IPC-only mode
    [    7.108896] platform 5f00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a6000000
    [    7.109338] remoteproc remoteproc9: 5f00000.r5f is available
    [    7.109373] remoteproc remoteproc9: attaching to 5f00000.r5f
    [    7.109605] platform 5f00000.r5f: R5F core initialized in IPC-only mode
    [    7.109611] rproc-virtio rproc-virtio.15.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a6000000
    [    7.109780] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0xd
    [    7.110288] virtio_rpmsg_bus virtio8: rpmsg host is online
    [    7.110303] rproc-virtio rproc-virtio.15.auto: registered virtio8 (type 7)
    [    7.110307] remoteproc remoteproc9: remote processor 5f00000.r5f is now attached
    [    7.111242] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    7.111572] virtio_rpmsg_bus virtio6: creating channel rpmsg_chrdev addr 0xd
    [    7.112537] platform 5900000.r5f: configured R5F for IPC-only mode
    [    7.112718] platform 5900000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a7000000
    [    7.113293] remoteproc remoteproc10: 5900000.r5f is available
    [    7.113349] remoteproc remoteproc10: attaching to 5900000.r5f
    [    7.113676] platform 5900000.r5f: R5F core initialized in IPC-only mode
    [    7.113685] rproc-virtio rproc-virtio.16.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a7000000
    [    7.114232] virtio_rpmsg_bus virtio9: rpmsg host is online
    [    7.114252] rproc-virtio rproc-virtio.16.auto: registered virtio9 (type 7)
    [    7.114257] remoteproc remoteproc10: remote processor 5900000.r5f is now attached
    [    7.114422] platform 5a00000.r5f: configured R5F for IPC-only mode
    [    7.114555] platform 5a00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a8000000
    [    7.114997] virtio_rpmsg_bus virtio7: creating channel rpmsg_chrdev addr 0xd
    [    7.115462] remoteproc remoteproc11: 5a00000.r5f is available
    [    7.115501] remoteproc remoteproc11: attaching to 5a00000.r5f
    [    7.115685] platform 5a00000.r5f: R5F core initialized in IPC-only mode
    [    7.115695] rproc-virtio rproc-virtio.17.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a8000000
    [    7.116141] virtio_rpmsg_bus virtio10: rpmsg host is online
    [    7.116159] rproc-virtio rproc-virtio.17.auto: registered virtio10 (type 7)
    [    7.116163] remoteproc remoteproc11: remote processor 5a00000.r5f is now attached
    [    7.116546] virtio_rpmsg_bus virtio8: creating channel rpmsg_chrdev addr 0xd
    [    7.119942] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
    [    7.120285] virtio_rpmsg_bus virtio9: creating channel rpmsg_chrdev addr 0xd
    [    7.122144] virtio_rpmsg_bus virtio10: creating channel rpmsg_chrdev addr 0xd
    [    7.122372] virtio_rpmsg_bus virtio10: creating channel rpmsg_chrdev addr 0x15
    [    7.122542] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x15
    [    7.122589] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15
    [    7.122918] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0x15
    [    7.123384] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0x15
    [    7.123717] virtio_rpmsg_bus virtio9: creating channel rpmsg_chrdev addr 0x15
    [    7.123895] virtio_rpmsg_bus virtio6: creating channel rpmsg_chrdev addr 0x15
    [    7.124093] virtio_rpmsg_bus virtio7: creating channel rpmsg_chrdev addr 0x15
    [    7.124454] virtio_rpmsg_bus virtio8: creating channel rpmsg_chrdev addr 0x15
    [    7.124634] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0x15
    [    7.124821] virtio_rpmsg_bus virtio10: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.124912] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.125958] virtio_rpmsg_bus virtio7: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.126049] virtio_rpmsg_bus virtio8: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.126451] virtio_rpmsg_bus virtio3: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.126475] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    7.132421] pci_bus 0001:01: busn_res: [bus 01-ff] end is updated to 01
    [    7.137868] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    7.137971] virtio_rpmsg_bus virtio4: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.138036] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.138102] virtio_rpmsg_bus virtio6: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.145974] pci 0001:00:00.0: BAR 7: assigned [mem 0x18400000-0x193fffff 64bit]
    [    7.150555] virtio_rpmsg_bus virtio9: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.154616] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    7.154643] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    7.160124] pci 0001:00:00.0: PCI bridge to [bus 01]
    [    7.335036] virtio_rpmsg_bus virtio5: creating channel ti.ethfw.notifyservice addr 0x72
    [    7.336993] pcieport 0001:00:00.0: PME: Signaling with IRQ 653
    [    7.343228] virtio_rpmsg_bus virtio5: creating channel ti.ethfw.ethdevice addr 0x71
    [    7.353595] pcieport 0001:00:00.0: AER: enabled with IRQ 653
    [    7.360480] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    7.433148] virtio_rpmsg_bus virtio5: creating channel ti.ipc4.ping-pong addr 0xe
    [    7.439689] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    7.792100] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    7.799205] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    7.809500] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    7.818935] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    7.834052] ti_cpsw_proxy_client virtio5.ti.ethfw.ethdevice.-1.113: 1 Virtual Switch Port(s), 1 Virtual MAC Only Port(s)
    [    7.846433] ti_cpsw_proxy_client virtio5.ti.ethfw.ethdevice.-1.113: Virt Port: 0, Type: Switch Port, Iface: eth2, Num TX: 2, Num RX: 1, Token: 0
    [    7.864898] ti_cpsw_proxy_client virtio5.ti.ethfw.ethdevice.-1.113: Virt Port: 4, Type: MAC Port, Iface: eth3, Num TX: 1, Num RX: 1, Token: 400
    [    7.880162] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [    7.885927] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [    7.894996] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    7.933790] ti_cpsw_proxy_client virtio5.ti.ethfw.ethdevice.-1.113: started virt port: 0 on interface eth2
    [    7.971292] ti_cpsw_proxy_client virtio5.ti.ethfw.ethdevice.-1.113: started virt port: 4 on interface eth3
    [    8.184389] audit: type=1334 audit(1723712010.880:6): prog-id=9 op=LOAD
    [    8.191042] audit: type=1334 audit(1723712010.888:7): prog-id=10 op=LOAD
    [    8.409285] audit: type=1006 audit(1723712011.104:8): pid=784 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
    [    8.422239] audit: type=1300 audit(1723712011.104:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffdb2f0dd8 a2=4 a3=ffffb4220020 items=0 ppid=1 pid=784 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [    8.448800] audit: type=1327 audit(1723712011.104:8): proctitle="(systemd)"
    [    8.816118] audit: type=1006 audit(1723712011.512:9): pid=777 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1
    [    8.831575] audit: type=1300 audit(1723712011.512:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffdb2f0dd8 a2=4 a3=ffffb4220020 items=0 ppid=1 pid=777 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
    [    8.858599] audit: type=1327 audit(1723712011.512:9): proctitle="(weston)"
    [   10.060350] am65-cpsw-nuss c200000.ethernet eth1: Link is Up - 100Mbps/Full - flow control off
    [   10.068980] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
    [   18.091877] cdns-mhdp8546 a000000.dp-bridge: invalid resource
    [   18.097632] cdns-mhdp8546 a000000.dp-bridge: Failed to get SAPB memory resource, HDCP not supported
    [   18.106688] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [   18.112581] platform regulator-dp0-prw: deferred probe pending
    [   18.118412] platform regulator-dp1-prw: deferred probe pending
    [   18.124237] platform main-r5fss-cpsw9g-virt-mac1: deferred probe pending
    [   18.130926] platform main-r5fss-cpsw9g-virt-mac0: deferred probe pending
    [   18.137616] platform dp0-connector: deferred probe pending
    [   18.143094] platform a000000.dp-bridge: deferred probe pending
    [ 1176.221341] IPv6: ADDRCONF(NETDEV_CHANGE): mcu_mcan0: link becomes ready
    [ 1177.248713] IPv6: ADDRCONF(NETDEV_CHANGE): mcu_mcan1: link becomes ready
    [ 1177.255479] IPv6: ADDRCONF(NETDEV_CHANGE): main_mcan16: link becomes ready
    

  • Hi Dušan,

    Thank you for the logs. My desire was more to look into how the CAN interface is being initialized so that I can replicate the same initialization sequence on my setup. So, I tried my best to replicate below with the information I can gather from your logs.

    Please compare below with the logs and commands that you are using.

    Below is the full logs including boot, the initialization of CAN, and candump/cansend on 9.2 Linux SDK on J784S4 EVM. You can see that the message I constructed "DEADBEEF" is being sent from main_mcan16 and received on mcu_mcan0: 

    9_2_j784s4_logs.txt

    In above logs, I have the same connection as your picture:

    Additionally, here are some logs from internal loopback where I have nothing physically connected:

    root@j784s4-evm:~# ip link set main_mcan16 type can bitrate 500000 loopback on
    root@j784s4-evm:~# ip link set up main_mcan16
    root@j784s4-evm:~# candump main_mcan16 &
    [1] 1247
    root@j784s4-evm:~# cansend main_mcan16 111#DEADBEEF
      main_mcan16  111   [4]  DE AD BE EF
      main_mcan16  111   [4]  DE AD BE EF
    root@j784s4-evm:~#
    
    

    Regards,

    Takuma

  • Hi Takuma,

    Thank you very much for your effort in setting up the exact same configuration for testing.

    It turns out that we didn't realize we needed to explicitly set the "loopback on" parameter for internal loopback mode, and that was the solution.

    Regarding the external loopback mode, the only difference was that you set the bitrate to 500,000 instead of 1,000,000, as stated in the SDK documentation. After making this change, everything worked perfectly.

    Interestingly, after retrying with a bitrate of 1,000,000 and following the documentation, everything is now working as expected. Do you have any idea why this might be the case?

    Lastly, I’m encountering an issue with setting the interface to CAN FD with a fixed bitrate. When I execute the command:

    $ ip link set main_mcan16 type can bitrate 1000000 fd on

    I received the error "RTNETLINK answers: Operation not supported." However, setting it with a variable bitrate works properly:

    $ ip link set mcu_mcan0 type can bitrate 1000000 dbitrate 4000000 fd on

    Is this a hardware limitation or could it be related to the driver configuration?

    Regards,
    Dušan

  • Hi Dušan,

    I'm glad you were able to get the CAN interface working.

    Interestingly, after retrying with a bitrate of 1,000,000 and following the documentation, everything is now working as expected. Do you have any idea why this might be the case?

    I am not quite sure. It could be that some step was missed.

    Is this a hardware limitation or could it be related to the driver configuration?

    I would say this is a driver limitation. Based on the Linux kernel documentation, it looks like both arbitration bitrate and data dbitrate must be defined for CAN-FD mode: https://www.kernel.org/doc/Documentation/networking/can.txt. It assume at some point the fixed bitrate command worked, but some things had changed since we wrote our Linux documentation. I'll see if we can get it update.

    Regards,

    Takuma