Other Parts Discussed in Thread: AM3517
Hi,
I am testing am3517, and when I boot from micro SD, not SD, then I can't enter the system, and log printed on the console is like this:
----------------------------------------------------------------------------------------------------------------------------------------
......
......
emac-mii: probed
rtc-s35390a 1-0030: setting system clock to 2000-01-01 00:19:10 UTC (946685950)
omapdss DPI error: display already enabled
omap_vout omap_vout: 'lcd' Display already enabled
omapdss DPI error: display already enabled
omap_vout omap_vout: 'lcd' Display already enabled
omap_vout omap_vout: Buffer Size = 3686400
omap_vout omap_vout: : registered and initialized video device 1
omap_vout omap_vout: Buffer Size = 3686400
omap_vout omap_vout: : registered and initialized video device 2
Waiting 1sec before mounting root device...
VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)
Please append a correct "root=" boot option; here are the available partitions:
1f00 512 mtdblock0 (driver?)
1f01 1792 mtdblock1 (driver?)
1f02 256 mtdblock2 (driver?)
1f03 5120 mtdblock3 (driver?)
1f04 516608 mtdblock4 (driver?)
b300 1921024 mmcblk0 driver: mmcblk
b301 72261 mmcblk0p1
b302 955867 mmcblk0p2
b303 891607 mmcblk0p3
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
I am not sure what is the problem.
When I boot from SD card, using the the same system, that is OK. but now I have a similar board with micro SD. I have no idea.
Thanks,
Kevin