This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 IPNC:time out occur in boot_procedure

 

 

Hi,

 

Please find the bootlog while booting through nfs.

 

NAND read: device 0 offset 0x700000, size 0xe00000
Skipping bad block 0x00b80000
 14680064 bytes read: OK

Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1915316 Bytes =  1.8 MB
   Load Address: 80008000
   Entry Point:  80008000
## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1915316 Bytes =  1.8 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.6.0 (root@mayank-laptop) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Thu O1
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM368 IPNC
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 170000000, vpssrate: 340000000
PLL0: vencrate_sd: 75555555, ddrrate: 340000000 mmcsdrate: 48571428
PLL1: armrate: 432000000, voicerate: 20571428, vencrate_hd: 27000000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 12288
Kernel command line: console=ttyS1,115200n8 noinitrd rw root=/dev/nfs nfsroot=10.17.1.101:/home/mayank/DM36/ipnc/target/filesys,nolock mem=48M ip=dhcp davin0
PID hash table entries: 256 (order: 8, 1024 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 48MB = 48MB total
Memory: 44440KB available (3297K code, 684K data, 184K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
DM365 IPIPE initialized in Single Shot mode
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 512 (order: -1, 2048 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 2048 bind 1024)
TCP reno registered

 ***davinci_spi_board_init()!<6>
 ***davinci_spi_board_init_End(0)!<5>VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Oct 13 2011 11:42:55 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
davinci_ldc initialized
facedetect major#: 252, minor# 0
facedetect driver registered
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is deadbeaf
TI DaVinci EMAC Linux version updated 4.0
netconsole: not configured, aborting
Linux video capture interface: v2.00
vpfe_init
starting ccdc_reset...<7>
End of ccdc_reset...<5>vpfe_probe
Trying to register davinci display video device.
layer=c0676000,layer->video_dev=c0676160
Trying to register davinci display video device.
layer=c0650e00,layer->video_dev=c0650f60
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Creating 7 MTD partitions on "nand_davinci.0":
0x00000000-0x00300000 : "bootloader"
0x00300000-0x00500000 : "params"
0x00500000-0x00700000 : "kernel"
0x00700000-0x02700000 : "filesystem"
0x02700000-0x02900000 : "data1"
0x02900000-0x02d00000 : "Calibration"
0x02d00000-0x08000000 : "data2"
nand_davinci nand_davinci.0: hardware revision: 2.3
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
dm_spi.0: davinci SPI Controller driver at 0xc3866000 (irq = 42) use_dma=0
musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Peripheral mode controller at c3868000 using DMA, IRQ 12
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
CQ0093 Voice Codec 0.1
asoc: cq93vc <-> davinci-vcif mapping ok
ALSA device list:
  #0: On-chip voice codec (cq93vc)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-01-01 03:43:14 (946698194)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests .., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 10.17.0.15
IP-Config: Complete:
      device=eth0, addr=10.17.0.15, mask=255.255.240.0, gw=255.255.255.255,
     host=10.17.0.15, domain=, nis-domain=(none),
     bootserver=0.0.0.0, rootserver=10.17.1.101, rootpath=
Looking up port of RPC 100003/2 on 10.17.1.101
Looking up port of RPC 100005/1 on 10.17.1.101
VFS: Mounted root (nfs filesystem).
Freeing init memory: 184K
INIT: version 2.86 booting
0
Starting the hotplug events dispatcher: udevd.
Synthesizing the initial hotplug events...done.
Waiting for /dev to be fully populated...done.
0
Starting mounting local filesystems: mount none on /dev/shm type tmpfs (rw,size=5M)
none on /var/run type tmpfs (rw)
none on /tmp type tmpfs (rw,sync)
Setting up networking ....
Starting hotplug subsystem:
   pci    
   pci      [success]
   usb    
   usb      [success]
   isapnp 
   isapnp   [success]
   ide    
   ide      [success]
   input  
   input    [success]
   scsi   
   scsi     [success]
done.
Starting portmap daemon: portmap.
Starting internet superserver: inetd.
insmod: /opt/ipnc/modules/crc-ccitt.ko: No such file or directory
insmod: /opt/ipnc/modules/libcrc32c.ko: No such file or directory
insmod: /opt/ipnc/modules/deadline-iosched.ko: No such file or directory
insmod: /opt/ipnc/modules/cfq-iosched.ko: No such file or directory
insmod: /opt/ipnc/modules/i2c-emac.ko: No such file or directory
insmod: /opt/ipnc/modules/sbull.ko: No such file or directory
insmod: /opt/ipnc/modules/crc32c.ko: No such file or directory
insmod: /opt/ipnc/modules/deflate.ko: No such file or directory
insmod: /opt/ipnc/modules/des.ko: No such file or directory
insmod: /opt/ipnc/modules/md5.ko: No such file or directory
insmod: /opt/ipnc/modules/sha1.ko: No such file or directory
insmod: /opt/ipnc/modules/nls_ascii.ko: No such file or directory
insmod: /opt/ipnc/modules/nls_utf8.ko: No such file or directory
insmod: /opt/ipnc/modules/exportfs.ko: No such file or directory
insmod: /opt/ipnc/modules/nfsd.ko: No such file or directory
insmod: /opt/ipnc/modules/loop.ko: No such file or directory
insmod: /opt/ipnc/modules/tun.ko: No such file or directory
insmod: /opt/ipnc/modules/slhc.ko: No such file or directory
insmod: /opt/ipnc/modules/netconsole.ko: No such file or directory
insmod: /opt/ipnc/modules/ppp_generic.ko: No such file or directory
insmod: /opt/ipnc/modules/ppp_synctty.ko: No such file or directory
insmod: /opt/ipnc/modules/ppp_async.ko: No such file or directory
insmod: /opt/ipnc/modules/ppp_deflate.ko: No such file or directory
insmod: /opt/ipnc/modules/davinci_emac.ko: No such file or directory
insmod: /opt/ipnc/modules/mmc_core.ko: No such file or directory
insmod: /opt/ipnc/modules/mmc_block.ko: No such file or directory
insmod: /opt/ipnc/modules/davinci-mmc.ko: No such file or directory
insmod: /opt/ipnc/modules/usbcore.ko: No such file or directory
insmod: /opt/ipnc/modules/musb_hdrc.ko: No such file or directory
insmod: /opt/ipnc/modules/usbmon.ko: No such file or directory
insmod: /opt/ipnc/modules/scsi_transport_iscsi.ko: No such file or directory
insmod: /opt/ipnc/modules/libiscsi.ko: No such file or directory
insmod: /opt/ipnc/modules/iscsi_tcp.ko: No such file or directory
mount: RPC: Remote system error - Network is unreachable
CSL: Module install successful, device major num = 251
CSL: Module version 0.10.00, built on Oct 13 2011 11:48:26
I2C: Module install successful, device major num = 250
DMA: Module install successful, device major num = 249
DRV: Module install successful
DRV: Module built on Oct 13 2011 11:48:28
DRV: EDMACC.QUEPRI  = 00000777
DRV: SYSTEM.MSTPRI0 = 00440022
DRV: SYSTEM.MSTPRI1 = 00000244
DRV: ISP.BCR        = 00000002
DRV: SYSTEM.MISC    = 00000391
CMEMK module: built on Oct 13 2011 at 11:47:58
  Reference Linux version 2.6.18
  File /home/mayank/DM36/dvsdk_2_10_01_18_v2.6/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
allocated heap buffer 0xc4000000 of size 0x5000000
CMEM Range Overlaps Kernel Physical - allowing overlap
CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83000000)
cmemk initialized
EDMAK module: built on Oct 13 2011 at 11:48:01
  Reference Linux version 2.6.18
  File /home/mayank/DM36/dvsdk_2_10_01_18_v2.6/linuxutils_2_24_03/packages/ti/sdo/linuxutils/edma/src/module/edmak.c
IRQK module: built on Oct 13 2011 at 11:48:02
  Reference Linux version 2.6.18
  File /home/mayank/DM36/dvsdk_2_10_01_18_v2.6/linuxutils_2_24_03/packages/ti/sdo/linuxutils/irq/src/module/irqk.c
irqk initialized
Creat queue id:0
queue id:0
Creat queue id:32769
queue id:32769
FileMngThread created
queue id:32769
AlramThread created
Share memory init success
IPNC_DM368_2.6.0 (root@mayank-laptop) (gcc version 4.2.0 (Monta
Creat queue id:65538
queue id:65538
queue id:65538
Creat queue id:98307
queue id:98307
Check_device_version : DEVICE VER = 1 !!
AviMngThr create faill!!

CPU is DM368
./av_server.out DM368 NTSC APPRO2A AEWB 720P H264 5000000 RCOFF AUTO MENUOFF &
Kill queue id:65538
Starting mounting local filesystems: mount mount: none already mounted on /dev/shm
mount: none already mounted on /var/run
mount: none already mounted on /tmp
nothing was mounted
Setting up networking ....
Starting hotplug subsystem:
   pci    
   pci      [success]
   usb    
   usb      [success]
   isapnp 
   isapnp   [success]
   ide    
   ide      [success]
   input  
   input    [success]
   scsi   
   scsi     [success]
done.
Starting portmap daemon: portmap.
Starting internet superserver: inetd.
insmod: /opt/ipnc/modules/crc-ccitt.ko: No such file or directory
insmod: /opt/ipnc/modules/libcrc32c.ko: No such file or directory
insmod: /opt/ipnc/modules/deadline-iosched.ko: No such file or directory
insmod: /opt/ipnc/modules/cfq-iosched.ko: No such file or directory
insmod: /opt/ipnc/modules/i2c-emac.ko: No such file or directory
insmod: /opt/ipnc/modules/sbull.ko: No such file or directory
insmod: /opt/ipnc/modules/crc32c.ko: No such file or directory
insmod: /opt/ipnc/modules/deflate.ko: No such file or directory
insmod: /opt/ipnc/modules/des.ko: No such file or directory
insmod: /opt/ipnc/modules/md5.ko: No such file or directory
insmod: /opt/ipnc/modules/sha1.ko: No such file or directory
insmod: /opt/ipnc/modules/nls_ascii.ko: No such file or directory
insmod: /opt/ipnc/modules/nls_utf8.ko: No such file or directory
insmod: /opt/ipnc/modules/exportfs.ko: No such file or directory
insmod: /opt/ipnc/modules/nfsd.ko: No such file or directory
insmod: /opt/ipnc/modules/loop.ko: No such file or directory
insmod: /opt/ipnc/modules/tun.ko: No such file or directory
insmod: /opt/ipnc/modules/slhc.ko: No such file or directory
insmod: /opt/ipnc/modules/netconsole.ko: No such file or directory
insmod: /opt/ipnc/modules/ppp_generic.ko: No such file or directory
insmod: /opt/ipnc/modules/ppp_synctty.ko: No such file or directory
insmod: /opt/ipnc/modules/ppp_async.ko: No such file or directory
insmod: /opt/ipnc/modules/ppp_deflate.ko: No such file or directory
insmod: /opt/ipnc/modules/davinci_emac.ko: No such file or directory
insmod: /opt/ipnc/modules/mmc_core.ko: No such file or directory
insmod: /opt/ipnc/modules/mmc_block.ko: No such file or directory
insmod: /opt/ipnc/modules/davinci-mmc.ko: No such file or directory
insmod: /opt/ipnc/modules/usbcore.ko: No such file or directory
insmod: /opt/ipnc/modules/musb_hdrc.ko: No such file or directory
insmod: /opt/ipnc/modules/usbmon.ko: No such file or directory
insmod: /opt/ipnc/modules/scsi_transport_iscsi.ko: No such file or directory
insmod: /opt/ipnc/modules/libiscsi.ko: No such file or directory
insmod: /opt/ipnc/modules/iscsi_tcp.ko: No such file or directory
 sbulla: unknown partition table
mkdosfs 3.0.6 (04 Oct 2009)
unable to get drive geometry, using default 255/63
/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
Root directory contains 512 slots.
Volume ID is 7ef08d42, no volume label.
queue id:0

TimeOut occure in boot_proc.

Program exit.
ApproDrvInit: 3
Creat queue id:131074
queue id:131074


INIT: Entering runlevel: 3

MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774)

10.17.0.15 login: root


Welcome to MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774).

login[892]: root login  on `console'

# ls
# pwd
/root
# cd /mnt/
/mnt/mmc/      /mnt/nand/     /mnt/ramdisk/
# cd /mnt/mmc/
# ls
# cd /opt/ipnc/mayank/
# ./main.out
vpfe ccdc capture vpfe ccdc capture.1: No decoder registered
init_camera_capture:open::: No such device or address
# ls /dev
MAKEDEV           edma              mtd5              sbulla
audio             fd                mtd5ro            shm
cmem              full              mtd6              snd
console           i2c               mtd6ro            sndstat
core              initctl           mtdblock0         sound
csl0              irqk              mtdblock1         spidev0.0
csl1              kmem              mtdblock2         stderr
csl2              kmsg              mtdblock3         stdin
csl3              loop              mtdblock4         stdout
csl4              mem               mtdblock5         tts
csl5              mixer             mtdblock6         tty
csl6              mtd0              net               urandom
csl7              mtd0ro            null              v4l
csl8              mtd1              port              vc
csl9              mtd1ro            ppp               vcc
davinci_ldc       mtd2              ptmx              video0
dev_dma           mtd2ro            pts               video2
dev_i2c           mtd3              random            video3
dm365_facedetect  mtd3ro            rd                watchdog
dm365mmap         mtd4              rtc               zero
dsp               mtd4ro            rtc0
# ls
capture_prev_rsz_ss_raw_bayer  v4l2.out
main.out                       v4l2m.out
# pwd
/opt/ipnc/mayank
# ifconfig
eth0      Link encap:Ethernet  HWaddr DE:AD:BE:AF:00:00 
          inet addr:10.17.0.15  Bcast:10.17.15.255  Mask:255.255.240.0
          UP BROADCAST NOTRAILERS RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:10365 errors:0 dropped:0 overruns:0 frame:0
          TX packets:4800 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:5648176 (5.3 MiB)  TX bytes:738123 (720.8 KiB)
          Interrupt:52 Base address:0x7000

lo        Link encap:Local Loopback 
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:16436  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

#

Please find my bootargs below:

bootdelay=4
baudrate=115200
setboot=setenv bootargs $(bootargs)
bootamd=nboot 0x80700000 0 0x500000;bootm
bootfile=""
setenv=bootargs console=ttyS1,115200n8 noinitrd rw root=/dev/nfs nfsroot=10.17.8.125:/home/mayank/DM36/ipnc/target/filesys,nolock mem=48M ip=dhcp
ip=ddr 10.17.8.125
ethaddr=00:0C:0C:A0:FF:FA
bootcmd=nand read 0x82000000 0x700000 0xE00000;nboot 0x80700000 0 0x500000;bootm 0x80700000
eth=00:0C:0C:A0:07:Ea
rootpath=/home/mayank/DM36/ipnc/target/filesys
nfshost=10.17.1.101
filesize=1D39F4
fileaddr=80700000
ipaddr=10.17.8.131
serverip=10.17.1.101
bootargs=console=ttyS1,115200n8 noinitrd rw root=/dev/nfs nfsroot=10.17.1.101:/home/mayank/DM36/ipnc/target/filesys,nolock mem=48M ip=dhcp davinci_capture.d0
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 1.3.4 (Dec  9 2010 - 17:44:14) DM368-IPNC-1.0.1

Environment size: 837/131068 bytes

 

As indicated in bold above i am getting timeout occur in boor_procedure.

also the ip address i am getting after booting from the board is 10.17.0.15,though in bootargs i haven'se t anywhere this ip.

Thanks and Regards,

Mayank