Part Number: TMDSIDK572
Tool/software:
Hi,
Is it possible to recreate the bootable image in SD card for Linux specifically the one with the Arago Project for linux evm 572?
The boot up shows as below before it was corrupted.
[ 7.452688] omap_gpio 48057000.gpio: Could not set line 16 debounce to 20000 microseconds (-22)
[ 7.470382] palmas-rtc 48070000.i2c:tps659038@58:tps659038_rtc: rtc core: registered 48070000.i2c:tps659038@58:tps659038_rtc as rtc0
[ 7.590415] remoteproc remoteproc0: powering up 58820000.ipu
[ 7.597602] remoteproc remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 6884184
[ 7.607224] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 7.612889] remoteproc remoteproc0: registered virtio0 (type 7)
[ 7.619014] Driver for 1-wire Dallas network protocol.
[ 7.620078] remoteproc remoteproc0: remote processor 58820000.ipu is now up
[ 7.632240] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x3d
[ 7.639918] virtio_rpmsg_bus virtio0: msg received with no recipient
[ 7.714661] remoteproc remoteproc1: powering up 55020000.ipu
[ 7.720514] remoteproc remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 3747220
[ 7.728633] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 7.754571] omap_rtc 48838000.rtc: registered as rtc1
[ 7.811639] omap_hdq 480b2000.1w: OMAP HDQ Hardware Rev 0.:. Driver in Interrupt mode
[ 7.820777] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 7.831682] remoteproc remoteproc1: registered virtio1 (type 7)
[ 7.849976] ov2659 0-0030: Sensor detection failed (3030, 0)
[ 7.859189] remoteproc remoteproc1: remote processor 55020000.ipu is now up
[ 7.876513] virtio_rpmsg_bus virtio1: creating channel rpmsg-rpc addr 0x65
[ 7.896869] virtio_rpmsg_bus virtio1: creating channel rpmsg-rpc addr 0x66
[ 8.005779] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 8.015141] omap-des 480a5000.des: will run requests pump with realtime priority
[ 8.030610] w1_master_driver w1_bus_master1: Attaching one wire slave 01.000000000000 crc 3d
[ 8.050125] w1_master_driver w1_bus_master1: Family 1 for 01.000000000000.3d is not registered.
[ 8.327820] phy phy-4a084000.phy.3: Linked as a consumer to regulator.21
[ 8.336412] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 8.348899] phy phy-4a085000.phy.4: Linked as a consumer to regulator.21
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ 8.563094] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 8.568983] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 8.584233] net eth1: initializing cpsw version 1.15 (0)
[ 8.619985] virtio_rpmsg_bus virtio0: msg received with no recipient
[ 8.711815] vpe 489d0000.vpe: Device registered as /dev/video0
[ 8.728429] Micrel KSZ9031 Gigabit PHY 48485000.mdio:01: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=48485000.mdio:01, irq=POLL)
[ 8.746480] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 8.754962] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ OK ] Listening on D-Bus System Message Bus Socket.[ 8.764301] CAN device driver interface
[ 8.778895] omap-aes 4b500000.aes: will run requests pump with realtime priority
[ 8.779015] net eth0: initializing cpsw version 1.15 (0)
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activati[ 8.803041] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
on Socket.
[ 8.814187] omap-aes 4b700000.aes: will run requests pump with realtime priority
[ 8.912580] Micrel KSZ9031 Gigabit PHY 48485000.mdio:00: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=48485000.mdio:00, irq=POLL)
[ 8.929285] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 9.047175] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=aa6f9af0, irq=89)
[[ 9.059585] vip 48990000.vip: loading firmware vpdma-1b8.bin
OK ] Listening on dropbear.socket.
[[ 9.092181] vip 48990000.vip: VPDMA firmware loaded
OK ] Started Daily Cleanup of Temporary Directories.
Starting Reboot and dump vmcore via kexec...
[ 9.149817] ahci 4a140000.sata: controller can't do 64bit DMA, forcing 32bit
[ 9.160427] ahci 4a140000.sata: forcing port_map 0x0 -> 0x1
[ 9.167140] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ OK ] Listening on RPCbind Server Activation Socket[ 9.178379] ahci 4a140000.sata: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
.
[ OK ] Reached target Sockets.
[ 9.204138] scsi host0: ahci
[ 9.207513] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 81
[ OK ] Reached target Basic System.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started Job spooling tools.
Starting Login Service...
[ OK ] Started D-Bus System Message Bus.
Starting TI IPC Daemon...
[ 9.542270] ata1: SATA link down (SStatus 0 SControl 300)
Starting Print notice about GPLv3 packages...
Starting rc.pvr.service...
Starting TI MultiCore Tools Daemon...
[ 9.620114] remoteproc remoteproc2: powering up 40800000.dsp
[ 9.626717] remoteproc remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 20483260
[ 9.640900] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[ 9.646818] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[ 9.654719] virtio_rpmsg_bus virtio0: msg received with no recipient
[ 9.672072] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 9.678551] remoteproc remoteproc2: registered virtio2 (type 7)
[ 9.685965] remoteproc remoteproc2: remote processor 40800000.dsp is now up
Starting RPC Bind Service...
[ OK ] Reached target System Time Synchronized.
[ 9.707792] virtio_rpmsg_bus virtio2: creating channel rpmsg-proto addr 0x3d
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
[ OK ] Started Network Service.
[ OK ] Started Reboot and dump vmcore via kexec.
Starting Network Name Resolution...
Starting Wait for Network to be Configured...
[ 9.870561] remoteproc remoteproc3: powering up 41000000.dsp
[ 9.919759] remoteproc remoteproc3: Booting fw image dra7-dsp2-fw.xe66, size 20483260
[ 9.987443] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
[ 9.993429] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
[ 10.069574] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1
[ 10.142522] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 10.160175] remoteproc remoteproc3: registered virtio3 (type 7)
[ 10.181775] remoteproc remoteproc3: remote processor 41000000.dsp is now up
[ 10.245954] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
[ 10.256410] virtio_rpmsg_bus virtio3: creating channel rpmsg-proto addr 0x3d
[ 10.275877] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
[ 10.289098] omap-hdmi-audio omap-hdmi-audio.0.auto: ASoC: no DMI vendor name!
[ 10.461631] davinci_mdio 4b2b2400.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 10.479779] libphy: 4b2b2400.mdio: probed
[ OK ] Started Login Service.
[ OK ] Started Network Name Resolution.
[ OK ] Started TI IPC Daemon.
[ OK ] Started rc.pvr.service.
[ OK ] Started TI MultiCore Tools Daemon.
[ OK ] Started RPC Bind Service.
[ 10.544549] davinci_mdio 4b2b2400.mdio: phy[0]: device 4b2b2400.mdio:00, driver TI TLK10X 10/100 Mbps PHY
[ 10.562819] davinci_mdio 4b2b2400.mdio: phy[1]: device 4b2b2400.mdio:01, driver TI TLK10X 10/100 Mbps PHY
[ 10.597132] remoteproc remoteproc4: 4b234000.pru is available
[ 10.612828] pru-rproc 4b234000.pru: PRU rproc node pru@4b234000 probed successfully
[ 10.620173] virtio_rpmsg_bus virtio0: msg received with no recipient
[ 10.631441] remoteproc remoteproc5: 4b238000.pru is available
[ 10.650310] pru-rproc 4b238000.pru: PRU rproc node pru@4b238000 probed successfully
[ 10.674761] remoteproc remoteproc6: 4b2b4000.pru is available
[ 10.694980] pru-rproc 4b2b4000.pru: PRU rproc node pru@4b2b4000 probed successfully
[ 10.724115] remoteproc remoteproc7: 4b2b8000.pru is available
[ 10.743355] pru-rproc 4b2b8000.pru: PRU rproc node pru@4b2b8000 probed successfully
[ 11.030134] prueth pruss2_eth: pruss_fw_drop_untagged_vlan 0
[ 11.041232] prueth pruss2_eth: pruss MC Mask (Port 0) ff:ff:ff:ff:ff:ff
[ 11.087800] prueth pruss2_eth: pruss MC Mask (Port 1) ff:ff:ff:ff:ff:ff
[ 11.137953] prueth pruss2_eth: TI PRU ethernet (type 0) driver initialized
[ 11.989801] dwc3 48890000.usb: Failed to get clk 'ref': -2
[ 12.002456] rpmsg_rpc virtio1.rpmsg-rpc.-1.101: probing service dce-callback with src 1024 dst 101
[ 12.005956] dwc3 488d0000.usb: Failed to get clk 'ref': -2
[ 12.020982] NET: Registered protocol family 45
[ 12.050831] rpmsg_rpc virtio1.rpmsg-rpc.-1.102: probing service rpmsg-dce with src 1025 dst 102
[ 12.051166] rpmsg_rpc virtio1.rpmsg-rpc.-1.101: published functions = 4
[ 12.107980] rpmsg_rpc virtio1.rpmsg-rpc.-1.102: published functions = 9
[ 12.242372] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 12.271336] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 12.301503] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x0000000002010010
[ 12.320165] xhci-hcd xhci-hcd.1.auto: irq 181, io mem 0x48890000
[ 12.335574] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[ 12.355026] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 12.363102] pruss_intc_irq_set_affinity: event 21 not configured: ch = -1, host = -1
[ 12.370261] usb usb1: Product: xHCI Host Controller
[ 12.376381] usb usb1: Manufacturer: Linux 4.19.79-g77dfab56c6 xhci-hcd
[ 12.380794] pruss_intc_irq_set_affinity: event 23 not configured: ch = -1, host = -1
[ 12.386857] usb usb1: SerialNumber: xhci-hcd.1.auto
[ 12.399717] pruss_intc_irq_set_affinity: event 27 not configured: ch = -1, host = -1
[ 12.408514] hub 1-0:1.0: USB hub found
[ 12.412637] hub 1-0:1.0: 1 port detected
[ 12.418469] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 12.427461] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 12.435748] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 12.442967] iep ptp bc clkid -1
[ 12.446534] remoteproc remoteproc7: powering up 4b2b8000.pru
[ 12.454603] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 12.463293] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
[ 12.471669] remoteproc remoteproc7: Booting fw image ti-pruss/am57xx-pru1-prueth-fw.elf, size 7152
[ 12.482593] pruss 4b280000.pruss: configured system_events[63-0] = 00600000,08a00000
[ 12.490375] pruss 4b280000.pruss: configured intr_channels = 0x0000032a host_intr = 0x000002aa
[ 12.500130] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 12.509283] usb usb2: Product: xHCI Host Controller
[ 12.514830] remoteproc remoteproc7: remote processor 4b2b8000.pru is now up
[ 12.522655] usb usb2: Manufacturer: Linux 4.19.79-g77dfab56c6 xhci-hcd
[ 12.529214] usb usb2: SerialNumber: xhci-hcd.1.auto
[ 12.534655] net eth3: started
[ 12.538410] IPv6: ADDRCONF(NETDEV_UP): eth3: link is not ready
[ 12.545770] hub 2-0:1.0: USB hub found
[ 12.550269] hub 2-0:1.0: 1 port detected
[ 12.577900] pruss_intc_irq_set_affinity: event 20 not configured: ch = -1, host = -1
[ 12.586062] pruss_intc_irq_set_affinity: event 22 not configured: ch = -1, host = -1
[ 12.594911] pruss_intc_irq_set_affinity: event 26 not configured: ch = -1, host = -1
[ 12.602977] remoteproc remoteproc6: powering up 4b2b4000.pru
[ 12.635034] remoteproc remoteproc6: Booting fw image ti-pruss/am57xx-pru0-prueth-fw.elf, size 7124
[ 12.648656] pruss 4b280000.pruss: configured system_events[63-0] = 00000600,04500000
[ 12.673139] pruss 4b280000.pruss: configured intr_channels = 0x000000d5 host_intr = 0x00000155
[ 12.689633] remoteproc remoteproc6: remote processor 4b2b4000.pru is now up
[ 12.697471] net eth2: started
[ 12.701270] IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
bc
binutils-dev
binutils
bison-dev
bison
cifs-utils
cpio
cpp-symlinks
cpp
dosfstools
elfutils-dev
elfutils
findutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbc6x
gdbserver
gettext
glmark2
gstreamer1.0-libav
gzip
hidapi
libasm1
libbfd
libcairo-perf-utils
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmavconn
libmpc3
libmpfr6
libreadline-dev
libreadline7
libunistring2
m4-dev
m4
make
mavlink
mavros-extras
mavros-msgs
mavros
nettle
parted
pdm-anomaly-detection
socketcan-interface
swig-dev
swig
which
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
Starting Save/Restore Sound Card State...
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Created slice system-systemd\x2dfsck.slice.
Starting File System Check on /dev/mmcblk0p1...
Starting weston.service...
[ OK ] Reached target Network.
Starting Enable and configure wl18xx bluetooth stack...
Starting Lightning Fast Webserver With Light System Requirements...
[ OK ] Started Redis In-Memory Data Store.
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Permit User Sessions...
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started Save/Restore Sound Card State.
[ OK ] Reached target Sound Card.
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Started Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started File System Check on /dev/mmcblk0p1.
Mounting /run/media/mmcblk0p1...
[ OK ] Mounted /run/media/mmcblk0p1.
[ OK ] Started Simple Network Management Protocol (SNMP) Daemon..
[ OK ] Started weston.service.
Starting Matrix GUI...
Starting telnetd.service...
[ OK ] Started Matrix GUI.
[ OK ] Started telnetd.service.
Starting thttpd.service...
[ OK ] Started thttpd.service.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am57xx-evm ttyS2
Arago 2019.11 am57xx-evm ttyS2
am57xx-evm login:
The image is for Arago Project http://arago-project.org am57xx-evm ttyS2, Arago 2019.11 am57xx-evm ttyS2.
I tried following the Linux SD card creation in SDK Linux create SD card using custom images but it still doesn't boot up like before.
I also tried the Arago Project setup in Building the SDK, but I don't know which config.txt aligns with the above bootup.