Part Number: PROCESSOR-SDK-AM62X
Tool/software:
Based on my experience using the NXP stress test tool, the following is true.
When the CPU powers on, the ROM Code can choose to load a DDR script file via USB Boot. Based on the calibration settings in the DDR script,
the DDR isinitialized.
This tool allows you to fine-tune the DDR clock frequency based on these calibration values for testing. As shown in the image.

you can set the Start Frequency and End Frequency to select the range where the DDR clock frequency will dynamically change.
By clicking the Stress Test Button, the tool performs a frequency sweep test on the DDR within this range by incrementally changing
the frequency.
For example, if the DDR's base frequency is set to 1600MHz, you can set the Start Frequency to 1550MHz and the End Frequency to 1650MHz for testing.
You want to know if TI currently has a similar testing tool that allows for dynamic fine-tuning of the DDR clock frequency for testing?