Tool/software:
Hi TI experts,
HW: custom board
SDK: j721s2, 9.2
I am currently facing rendering issues when I ported my code from rtos SDK 8.6 to rtos SDK 9.2. On SDK9.2 when I render a 3D car model using the GPU, the PVR reports an error and the program gets stuck for a few seconds and then recovers, whereas SDK8.6 doesn't have this problem.
I also run into this problem when I change the program to run on the EVM board.
The following is the log run on the EVM:
pvrlogdump_j721s2-evm_2204282011.txt.gz
Thanks
Regards
quanfeng