Hi, We have recently moved a large existing code base to ccs5 and switched from COFF to ELF. We also use SYS/BIOS. We now have to configure the linker using a .bld and .cfg file which is processed during the bios build phase. This produces bios_pe66_x.xdl which is to all intents and purposes a linker command file. 82e9ace0 82e9ace0 00000001 00000001 r-- .const.1139 A similarly large number of .far and .fardata also. Our sections configuration (via xdctools and the .cfg file) is: ...