This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to read EMIFA Ctrl registers on OMAPL138



Hello,

 I am new to linux as well as OMAP.

I am trying to write a Linux driver for accessing the FPGA  through the EMIFA bus.

I am unable to access the EMIFA control registers at 0x68000000.

 

I wrote the following the code:

 

     resrc=request_mem_region(0x68000000,64,"fpga");  
   
    if (resrc== NULL)
    {
        printk("resource not allocated\n");
        return -1;
       }
   
    location = (unsigned int *)ioremap_nocache(0x68000000,64);
   
    if (!location)
    {
        printk("AEMIFA CTL BASE NOT AVAILABLE\n");
        return 1;
    }
      regval = readl(location);
    printk("Regval %x\n",regval);
    regval = ioread32(location);
    printk("Regval %x\n",regval);

 

I have tried to use both ioread32 as well as readl functions but I always get 0 as return values.

The value expected is 0x4000 0205h. Its a read only location so there is no question of something else overwriting the register.

I get the correct value when I access the same register in u-boot.

 

With regards

Pankaj