Hi,
I want to put my AM1808 based board in low power mode (suspend to RAM mode.)
But I can not configure the wakeup event on any GPIO based IRQ. It is also not documented any where in the Reference manual.
So can I implement the some GPIO based wake up signal or I must have to use the hardware DEEPSLEEP signal ?
For our system we need the board to wake up on keypad interrupts, UART, SPI interrupts etc.
Any help will be appreciated.