Hello,
I have compiled u-boot from TI SDK 05.02 for LogicPD AM3517 SOM, using the am3517_evem_config option. Following that, the boards does boot from SD card, but I keep getting these messages from u-boot:
NAND: HW ECC [Kernel/FS layout] selected
nand_get_flash_type: second ID read did not match 54,40 against 00,40
No NAND device found!!!
0 MiB
*** Warning - bad CRC or NAND, using default environment
The installed nand chip is from Micron. Is there any ways to have NAND support from u-Boot?
Thanks,
Yves McDonald
ymcdonald@leapmedical.ca