This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6422: Reading on-board EEPROM at 0x51 failed -1

Part Number: AM6422

Tool/software:

Hi,

We use our own hardware, using SDK 8.6,AM6422. When the system starts, the following message is printed in uboot, and it is found that it will be restarted several times in uboot and then enter the system。 

////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

U-Boot SPL 2021.01-g2ee8efd654 (Feb 27 2023 - 13:51:27 +0000)
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
Resetting on cold boot to workaround ErrataID:i2331
resetting ...

U-Boot SPL 2021.01-g2ee8efd654 (Feb 27 2023 - 13:51:27 +0000)
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from MMC1
Authentication passed
Authentication passed
Authentication passed
Authentication passed
init_env from device 9 not supported!
Starting ATF on ARM64 core...

NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 13:46:23, Feb 27 2023
I/TC:
I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Mon Feb 27 13:47:09 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2021.01-g2ee8efd654 (Feb 27 2023 - 13:49:29 +0000)
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
Trying to boot from MMC1
Authentication passed
Authentication passed


U-Boot 2021.01-00001-g7e12ed6f28-dirty (Aug 20 2024 - 09:21:31 +0800)

SoC: AM64X SR2.0 HS-FS
Model: Texas Instruments AM642 EVM
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
DRAM: 2 GiB
NAND: 0 MiB
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from MMC... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
Net: eth0: ethernet@8000000port@1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
Failed to load 'boot.scr'
** Unrecognized filesystem type **
19147264 bytes read in 95 ms (192.2 MiB/s)
39808 bytes read in 3 ms (12.7 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 000000008fef3000, end 000000008fffffff ... OK

Starting kernel ...

//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

I hope you can help analyze it,and thank you!