Hi,
I'm using Hyperlynx to simulate the DDR2 interface of my design using DMVA2. I downloaded the .ibis model file for the TMS320DM368. Could you confirm this is the appropriate model for the DMVA2 part?
Also, when selecting a model for drivers in the DDR controller module, there are basically four options for 1.8V logic.
NOSR0_NOTERM_1P8 Cell operated at 1.8(nom)
|NOSR0_NOTERM_1P8
|BUFFER OPERATING AT FAST MODE WITH 1.8V SUPPLY WITH +/-10% VARIATION
SR0_NOTERM_1P8 Cell operated at 1.8(nom)
|SR0_NOTERM_1P8
|BUFFER OPERATING AT SLOW MODE WITH 1.8V SUPPLY WITH +/-10% VARIATION
NOSR0_NOTERM_0.1_1P8 Cell operated at 1.8(nom)
|NOSR0_NOTERM_0.1_1P8
|BUFFER OPERATING AT FAST MODE WITH 1.8V SUPPLY WITH +/-0.1V VARIATION
SR0_NOTERM_0.1_1P8 Cell operated at 1.8(nom)
|SR0_NOTERM_0.1_1P8
|BUFFER OPERATING AT SLOW MODE WITH 1.8V SUPPLY WITH +/-0.1V VARIATION
Since I'm relatively new to simulations using IBIS models, I would like to understand the differences between SR0 vs NOSR0, and also the differences between FAST and SLOW modes.
I want to understand how these options can affect my simulation.
Regards,
Elvis