This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

After installed new 3.10_00_19 dvsdk tools, cannot compile DMEO program dsplink



After installed a new version of dvsdk tool, I cannot event make simple demo working, reported the error is: the directory is not existed, what I missed here, any suggestion ?

-------------  output from the console --------------

gmake[3]: Entering directory `/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen'
[GEN                 ] ------- DIRS ------------------ DEBUG --------------
[GEN                 ] ------- OBJECT ---------------- DEBUG --------------
/usr//bin/perl /home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/make/bin/runif.pl LINUX "exist /home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen" "/home/jimx/dvsdk/dvsdk_3_10_00_19/xdctools_3_16_01_27/gmake -C /home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen -f  /home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/make/DspBios/C64XX/compile.mk objdeb VERBOSE=0" ""
gmake[4]: Entering directory `/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen'
echo Compiling failure.c...
Compiling failure.c...
/home/jimx/dvsdk/dvsdk_3_10_00_19/cgt6x_6_1_12/bin/cl6x -g -d"_DEBUG" --no_compress -dMAX_DSPS=1 -dMAX_PROCESSORS=2 -dID_GPP=1 -dDAVINCIHD -dPROC_COMPONENT -dPOOL_COMPONENT -dNOTIFY_COMPONENT -dMPCS_COMPONENT -dRINGIO_COMPONENT -dMPLIST_COMPONENT -dMSGQ_COMPONENT -dMSGQ_ZCPY_LINK -dZCPY_LINK -dPROCID=0 -dDM6467GEM -dDM6467GEM_INTERFACE=SHMEM_INTERFACE -dPHYINTERFACE=SHMEM_INTERFACE -dDSP_SWI_MODE -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/inc -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/inc/DspBios -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/inc/DspBios/5.XX -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/inc/DspBios/5.XX/DM6467GEM -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/inc/DM6467GEM -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/inc/C64XX -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen/DspBios -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen/DspBios/ -I/home/jimx/dvsdk/dvsdk_3_10_00_19/bios_5_41_00_06/packages/ti/bios/include -I/home/jimx/dvsdk/dvsdk_3_10_00_19/cgt6x_6_1_12/include -I/home/jimx/dvsdk/dvsdk_3_10_00_19/bios_5_41_00_06/packages/ti/rtdx/include/c6000 -I/home/jimx/dvsdk/dvsdk_3_10_00_19/bios_5_41_00_06/packages/ti/psl/include -I/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/BUILD/DM6467GEM_0/INCLUDE -q -pdr -pdv -pden -ml3 -mv6400+ --disable:sploop     -fr"/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/BUILD/DM6467GEM_0/GEN/OBJ/DEBUG" failure.c
/bin/sh: /home/jimx/dvsdk/dvsdk_3_10_00_19/cgt6x_6_1_12/bin/cl6x: not found
gmake[4]: *** [failure.c.deb] Error 127
gmake[4]: Leaving directory `/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen'
gmake[3]: *** [objdeb] Error 2
gmake[3]: Leaving directory `/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base/gen'
gmake[2]: *** [gen.objdeb] Error 2
gmake[2]: Leaving directory `/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src/base'
gmake[1]: *** [base.objdeb] Error 2
gmake[1]: Leaving directory `/home/jimx/dvsdk/dvsdk_3_10_00_19/dsplink_linux_1_64/dsplink/dsp/src'
make: *** [dsplink_dsp] Error 2