/******************************************************************************/
/* Copyright 2004 by SEED Electronic Technology LTD. */
/* All rights reserved. SEED Electronic Technology LTD. */
/* Restricted rights to use, duplicate or disclose this code are */
/* granted through contract. */
/* */
/* */
/******************************************************************************/
/*----------------------------------------------------------------------------*/
/* MODULE NAME... SFRAM */
/* FILENAME...... 5502_SDRAM.c */
/* DATE CREATED.. Wed 6/11/2004 */
/* PROJECT....... write and read data between the CPU and SDRAM */
/* COMPONENT..... */
/* PREREQUISITS.. */
/*----------------------------------------------------------------------------*/
/*----------------------------------------------------------------------------*/
/* DESCRIPTION: */
/* */
/* This is an example of writting and reading SDRAM */
/*----------------------------------------------------------------------------*/
#include <csl.h>
#include <csl_pll.h>
#include <csl_emif.h>
#include <csl_chip.h>
#include <csl_emifBhal.h>
#include <stdio.h>
#define DataLength 1000
Uint16 i;
#pragma DATA_SECTION (SourData,".sourdata")
Uint32 SourData[DataLength];
EMIF_Config MyEmifConfig = {
EMIF_GBLCTL1_RMK( // EMIF Global Control Register 1
EMIF_GBLCTL1_NOHOLD_HOLD_ENABLED, // Hold enable
EMIF_GBLCTL1_EK1HZ_EK1EN, // High-Z control
EMIF_GBLCTL1_EK1EN_ENABLED // ECLKOUT1 Enable
),
EMIF_GBLCTL2_RMK( // EMIF Global Control Register 2
EMIF_GBLCTL2_EK2RATE_1XCLK, // ECLKOUT2 Rate
EMIF_GBLCTL2_EK2HZ_HIGHZ,
EMIF_GBLCTL2_EK2EN_DISABLED // ECLKOUT2 DISABLED
),
EMIF_CE1CTL1_RMK( // CE1 Space Control Register 1
EMIF_CE1CTL1_TA_DEFAULT,
EMIF_CE1CTL1_READ_STROBE_DEFAULT,
EMIF_CE1CTL1_MTYPE_DEFAULT,
EMIF_CE1CTL1_WRITE_HOLD_MSB_DEFAULT,
EMIF_CE1CTL1_READ_HOLD_DEFAULT
),
EMIF_CE1CTL2_RMK( // CE1 Space Control Register 2
EMIF_CE1CTL2_WRITE_SETUP_DEFAULT,
EMIF_CE1CTL2_WRITE_STROBE_DEFAULT,
EMIF_CE1CTL2_WRITE_HOLD_DEFAULT,
EMIF_CE1CTL2_READ_SETUP_DEFAULT
),
EMIF_CE0CTL1_RMK( // CE0 Space Control Register 1
EMIF_CE0CTL1_TA_DEFAULT,
EMIF_CE0CTL1_READ_STROBE_DEFAULT,
EMIF_CE0CTL1_MTYPE_16BIT_SDRAM, // we use the CE0
EMIF_CE0CTL1_WRITE_HOLD_MSB_DEFAULT,
EMIF_CE0CTL1_READ_HOLD_DEFAULT
),
EMIF_CE0CTL2_RMK( // CE0 Space Control Register 2
EMIF_CE0CTL2_WRITE_SETUP_DEFAULT,
EMIF_CE0CTL2_WRITE_STROBE_DEFAULT,
EMIF_CE0CTL2_WRITE_HOLD_DEFAULT,
EMIF_CE0CTL2_READ_SETUP_DEFAULT
),
EMIF_CE2CTL1_RMK( // CE2 Space Control Register 1
EMIF_CE2CTL1_TA_DEFAULT, // Not use for SDRAM (asynchronous memory types only)
EMIF_CE2CTL1_READ_STROBE_DEFAULT, // Read strobe width
EMIF_CE2CTL1_MTYPE_DEFAULT, //
EMIF_CE2CTL1_WRITE_HOLD_DEFAULT, // Write hold width
EMIF_CE2CTL1_READ_HOLD_DEFAULT // Read hold width
),
EMIF_CE2CTL2_RMK( // CE2 Space Control Register 2
EMIF_CE2CTL2_WRITE_SETUP_DEFAULT, // Write setup width
EMIF_CE2CTL2_WRITE_STROBE_DEFAULT, // Write strobe width
EMIF_CE2CTL2_WRITE_HOLD_DEFAUL // Write hold width
EMIF_CE2CTL2_READ_SETUP_DEFAULT // Read setup width
),
EMIF_CE3CTL1_RMK( // CE3 Space Control Register 1
EMIF_CE3CTL1_TA_DEFAULT, // Not use for SDRAM (asynchronous memory types only)
EMIF_CE3CTL1_READ_STROBE_DEFAULT, // Read strobe width
EMIF_CE2CTL1_MTYPE_DEFAULT,
EMIF_CE3CTL1_WRITE_HOLD_DEFAULT, // Write hold width
EMIF_CE3CTL1_READ_HOLD_DEFAULT // Read hold width
),
EMIF_CE3CTL2_RMK( // CE3 Space Control Register 2
EMIF_CE3CTL2_WRITE_SETUP_DEFAULT, // Write setup width
EMIF_CE3CTL2_WRITE_STROBE_DEFAULT, // Write strobe width
EMIF_CE3CTL2_WRITE_HOLD_DEFAULT, // Write hold width
EMIF_CE3CTL2_READ_SETUP_DEFAULT // Read setup width
),
EMIF_SDCTL1_RMK( // SDRAM Control Register 1
EMIF_SDCTL1_TRC_OF(5), // Specifies tRC value of the SDRAM in EMIF clock cycles.
EMIF_SDCTL1_SLFRFR_DISABLED // Self-refresh mode disabled
),
EMIF_SDCTL2_RMK( // SDRAM Control Register 2
0x11, // 4 banks,11 row address, 8 column address, I don't kown why ,how to congfig this SDWTH[4:0]:(Determines the size of the SDRAM that are placed on the bus. The width of the
data bus for a given CE space is determined by the MTYPE field in the CE control
registers)
EMIF_SDCTL2_RFEN_ENABLED, // Refresh enabled
EMIF_SDCTL2_INIT_INIT_SDRAM,
EMIF_SDCTL2_TRCD_OF(1), // Specifies tRCD value of the SDRAM in EMIF clock cycles
EMIF_SDCTL2_TRP_OF(1) // Specifies tRP value of the SDRAM in EMIF clock cycles
),
0x618, // SDRAM Refresh Control Register 1
0x0300, // SDRAM Refresh Control Register 2
EMIF_SDEXT1_RMK( // SDRAM Extension Register 1
EMIF_SDEXT1_R2WDQM_1CYCLE,
EMIF_SDEXT1_RD2WR_4CYCLES,
EMIF_SDEXT1_RD2DEAC_1CYCLE,
EMIF_SDEXT1_RD2RD_1CYCLE,
EMIF_SDEXT1_THZP_OF(1), // tPROZ2=2
EMIF_SDEXT1_TWR_OF(0),
EMIF_SDEXT1_TRRD_2CYCLES,
EMIF_SDEXT1_TRAS_OF(4),
EMIF_SDEXT1_TCL_2CYCLES
),
EMIF_SDEXT2_RMK( // SDRAM Extension Register 2
EMIF_SDEXT2_WR2RD_0CYCLES,
EMIF_SDEXT2_WR2DEAC_1CYCLE,
0,
EMIF_SDEXT2_R2WDQM_1CYCLE
),
EMIF_CE1SEC1_DEFAULT, // CE1 Secondary Control Register 1
EMIF_CE0SEC1_DEFAULT, // CE0 Secondary Control Register 1
EMIF_CE2SEC1_DEFAULT, // CE2 Secondary Control Register 1
EMIF_CE3SEC1_DEFAULT, // CE3 Secondary Control Register 1
EMIF_CESCR_DEFAULT // CE Size Control Register
};
/******************************************************************************\
* End of 5502_SDRAM.c
\******************************************************************************/